<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32DS for ARM v2.2 installation issue in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-for-ARM-v2-2-installation-issue/m-p/2356528#M14229</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Due to various reasons, I am currently reinstalling S32DS for ARM v2.2. After double-clicking the exe installer, the installation interface does not pop up. Instead, only a folder named I1777285553 is extracted in the Temp folder. Inside I1777285553\Windows, there is an S32DS_arm_v2.2.exe. I tried double-clicking it, but it shows the error: "Failed to load Java VM: error 2". However, there is a java.exe under I1777285553\Windows\resource\jre\bin. I also tried running S32DS_arm_v2.2.exe from the command line and specifying the location of java.exe, but there is no response. What should I do in this situation? Do I need to re-download Java?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 27 Apr 2026 10:49:03 GMT</pubDate>
    <dc:creator>duosahnyu</dc:creator>
    <dc:date>2026-04-27T10:49:03Z</dc:date>
    <item>
      <title>S32DS for ARM v2.2 installation issue</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-for-ARM-v2-2-installation-issue/m-p/2356528#M14229</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Due to various reasons, I am currently reinstalling S32DS for ARM v2.2. After double-clicking the exe installer, the installation interface does not pop up. Instead, only a folder named I1777285553 is extracted in the Temp folder. Inside I1777285553\Windows, there is an S32DS_arm_v2.2.exe. I tried double-clicking it, but it shows the error: "Failed to load Java VM: error 2". However, there is a java.exe under I1777285553\Windows\resource\jre\bin. I also tried running S32DS_arm_v2.2.exe from the command line and specifying the location of java.exe, but there is no response. What should I do in this situation? Do I need to re-download Java?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 27 Apr 2026 10:49:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-for-ARM-v2-2-installation-issue/m-p/2356528#M14229</guid>
      <dc:creator>duosahnyu</dc:creator>
      <dc:date>2026-04-27T10:49:03Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS for ARM v2.2 installation issue</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-for-ARM-v2-2-installation-issue/m-p/2356680#M14230</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/261964"&gt;@duosahnyu&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Thanks for reaching out to us. I just downloaded and installed S32DS for ARM v2.2 on a Windows 11 machine without problems, so we can discard issues with the installer. Can you try running the installer with administrator privileges? Also, please check if you see a txt file in&amp;nbsp;&lt;EM&gt;C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\Logs&lt;/EM&gt;, if so, please share it in your next reply.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Mon, 27 Apr 2026 17:10:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-for-ARM-v2-2-installation-issue/m-p/2356680#M14230</guid>
      <dc:creator>alejandro_e</dc:creator>
      <dc:date>2026-04-27T17:10:45Z</dc:date>
    </item>
  </channel>
</rss>