<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Problems using BMS GEN1 SDK 4.4 and R21-11 Version 1.0.3 in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Problems-using-BMS-GEN1-SDK-4-4-and-R21-11-Version-1-0-3/m-p/2337223#M14130</link>
    <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/57959"&gt;@Robin_Shen&lt;/a&gt;&amp;nbsp;&amp;nbsp;:&lt;/P&gt;&lt;P&gt;I have the same problem, so that me confirm again, I can't use install &lt;SPAN&gt;S32K3 BMS SDK AUTOSAR 4.4 R21-11 Version 1.0.2 based on&amp;nbsp;&lt;/SPAN&gt;S32DS3.6 version? Because there are MC33772 &amp;amp; MC33774 MCAL driver inside it, there are not inside BMS SDK GEN2, it's necessary for our project.&lt;/P&gt;&lt;P&gt;Do you have any idea or suggestion?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;BR, BillWen&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 23 Mar 2026 00:16:29 GMT</pubDate>
    <dc:creator>BillWen</dc:creator>
    <dc:date>2026-03-23T00:16:29Z</dc:date>
    <item>
      <title>Problems using BMS GEN1 SDK 4.4 and R21-11 Version 1.0.3</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Problems-using-BMS-GEN1-SDK-4-4-and-R21-11-Version-1-0-3/m-p/2170462#M13761</link>
      <description>&lt;P&gt;Dear Sir or Madam,&lt;/P&gt;&lt;P&gt;we have troubles using the driver „S32K3 BMS GEN1 SDK 4.4 and R21-11 Version 1.0.3“ in S32 Design Studio with S32K358.&lt;/P&gt;&lt;P&gt;In the Release Notes of the BMS SDK, in section 2.2.2 Installation Design Studio, the following steps are written:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Install S32 Design Studio IDE v3.5 Service Pack 1 EAR4 Build 23030&lt;/LI&gt;&lt;LI&gt;Install the Update Site for S32K3 Real Time Drivers AUTOSAR 4.4 and R21-11 Version 3.0.0:&amp;nbsp;&lt;EM&gt;SW32K3_RTD_4.4_R21-11_3.0.0_D2303_DS_updatesite.zip&lt;/EM&gt;&lt;/LI&gt;&lt;LI&gt;Install this BMS GEN1 SDK SW package using the Update site installer:&amp;nbsp;&lt;EM&gt;SW32K3_BMS_GEN1_SDK_4.4_R21-11_1.0.3_updatesite_D2407.zip&lt;/EM&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Until now, we worked with S32 DS v3.6.3 and &lt;EM&gt;SW32K3_S32M27x_RTD_R21-11_6.0.0_D2506_DesignStudio_updatesite.zip&lt;/EM&gt;.&lt;/P&gt;&lt;P&gt;Installing &lt;EM&gt;SW32K3_BMS_GEN1_SDK_4.4_R21-11_1.0.3_updatesite_D2407.zip &lt;/EM&gt;with RTD 6.0.0 in S32 DS v3.6.3 fails with an error message [1].&lt;/P&gt;&lt;P&gt;A downgrade from RTD 6.0.0 to 3.0.0 leads to error messages upon opening our project file that we created using RTD 6.0.0 [2].&lt;/P&gt;&lt;P&gt;I created a blank project using S32 DS v3.5 (I could not find the exact Service Pack 1 EAR4 Build 2030). I could install RTD 3.0.0 and the BMS SDK according to the release notes above. However, the generated code did not compile because standardTypes.h was not found.&lt;/P&gt;&lt;P&gt;My questions:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Is there a way to import, configure and compile the BMS Drivers using the BMS SDK, RTD 6.0.0 and S32 DS v3.6.3?&lt;/LI&gt;&lt;LI&gt;If not, do all developers that use S32 DS need to downgrade their installation and RTD to comply with the steps from the release notes? We all work on a common configuration of which the BMS driver is part of.&lt;/LI&gt;&lt;LI&gt;How do we generate code that compiles?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Philipp&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;[1]:&lt;/P&gt;&lt;P&gt;S32DS v3.6.3&lt;/P&gt;&lt;P&gt;Installation of BMS-SDK mit RTD 6.0.0:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Operation details Software being installed:
com.nxp.BMS_GEN1_SDK.S32K3XX.root.1.0.3.feature.feature.group 1.0.3.202408021227 Missing requirement:
com.nxp.BMS_GEN1_SDK.S32K3XX.root.1.0.3.feature.feature.group 1.0.3.202408021227 requires
'org.eclipse.equinox.p2.iu; com.nxp.RTD.S32K3.root.feature.feature.group 3.0.0' but it could not be found&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;[2]:&lt;/P&gt;&lt;P&gt;S32DS v3.6.3&lt;/P&gt;&lt;P&gt;Loading our S32DS Project with RTD 3.0.0:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;An error has occurred. See error log for more details.

PeripheralExpressionException[
Description: Feature FEATURE_PORT_PINSWITHIF not defined for the part number S32K358, core M7_0_0 and peripheral null
Function: getFeature(valid)
Contexts:
ExpressionContext[ child_context = ChildContext[
 $this = Siul2_Port.PortConfigSet.PortContainer.0.PortPin.0.PortPinIfe
 component = Siul2_Port
 $instance = Siul2_Port
 $group = BOARD_InitPeripherals]]

ExpressionContext[ child_context = ChildContext[
 $this = Siul2_Port.PortConfigSet.PortContainer.0.PortPin.0.PortPinIfe
 component = Siul2_Port
 $instance = Siul2_Port
 $group = BOARD_InitPeripherals]]

ExpressionContext[ child_context = ChildContext[
 $this = Siul2_Port.PortConfigSet.PortContainer.0.PortPin.0.PortPinIfe
 component = Siul2_Port
 $instance = Siul2_Port
 $group = BOARD_InitPeripherals]]
]&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 16 Sep 2025 13:03:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Problems-using-BMS-GEN1-SDK-4-4-and-R21-11-Version-1-0-3/m-p/2170462#M13761</guid>
      <dc:creator>PhilippH</dc:creator>
      <dc:date>2025-09-16T13:03:19Z</dc:date>
    </item>
    <item>
      <title>Re: Problems using BMS GEN1 SDK 4.4 and R21-11 Version 1.0.3</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Problems-using-BMS-GEN1-SDK-4-4-and-R21-11-Version-1-0-3/m-p/2171491#M13763</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Philipp,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Sorry, I checked the latest HVBMS for the S32K358 and it still uses S32DS v3.5 and RTD 3.0.0.&lt;BR /&gt;At this stage, I'm afraid you'll have to refer to section &lt;STRONG&gt;4 BMS Software installation procedure&lt;/STRONG&gt; in the &lt;STRONG&gt;BMS_SWInstalationGuide_Bring-up_2024.10.pdf&lt;/STRONG&gt; to install these software.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="BMS_SWInstalationGuide_Bring-up_2024.10.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/357397iCB571D45124B358E/image-size/large?v=v2&amp;amp;px=999" role="button" title="BMS_SWInstalationGuide_Bring-up_2024.10.png" alt="BMS_SWInstalationGuide_Bring-up_2024.10.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;It is not recommended to install these software in S32DS v3.6.3.&amp;nbsp;Unless the HVBMS team releases a new version of the software package, those examples will not work in S32DS v3.6.3 + RTD 6.0.0 environment.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 18 Sep 2025 01:28:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Problems-using-BMS-GEN1-SDK-4-4-and-R21-11-Version-1-0-3/m-p/2171491#M13763</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2025-09-18T01:28:39Z</dc:date>
    </item>
    <item>
      <title>Re: Problems using BMS GEN1 SDK 4.4 and R21-11 Version 1.0.3</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Problems-using-BMS-GEN1-SDK-4-4-and-R21-11-Version-1-0-3/m-p/2175847#M13780</link>
      <description>&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;we managed to install a working environment with the detailled installation guide and downgraded our project.&lt;/P&gt;&lt;P&gt;Despite using the S32K358, some of us develop on EvalBoards using the S32K396 (&lt;A href="https://www.nxp.com/part/S32K396BMS-EVB" target="_blank"&gt;https://www.nxp.com/part/S32K396BMS-EVB&lt;/A&gt;).&lt;/P&gt;&lt;P&gt;I tried installing the S32K396 SDK in my environment, however S32DS now crashes upon opening it. Is there a way to use the HVBMS environment with S32K396?&lt;/P&gt;</description>
      <pubDate>Thu, 25 Sep 2025 13:38:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Problems-using-BMS-GEN1-SDK-4-4-and-R21-11-Version-1-0-3/m-p/2175847#M13780</guid>
      <dc:creator>PhilippH</dc:creator>
      <dc:date>2025-09-25T13:38:38Z</dc:date>
    </item>
    <item>
      <title>Re: Problems using BMS GEN1 SDK 4.4 and R21-11 Version 1.0.3</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Problems-using-BMS-GEN1-SDK-4-4-and-R21-11-Version-1-0-3/m-p/2176156#M13786</link>
      <description>&lt;P&gt;I noticed that the two packages are different in the&lt;A href="https://www.nxp.com/app-autopackagemgr/automotive-software-package-manager:AUTO-SW-PACKAGE-MANAGER?currentTab=0" target="_self"&gt; Automotive Software Package Manager&lt;/A&gt;.&lt;BR /&gt;I recommend reinstalling S32DS v3.5 in a different directory, such as C:\NXP\S32DS.3.5_S32K396BMS.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="S32K396BMS BMS&amp;amp;VCU PoC.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/358624i8CF60CBFCAFC875D/image-size/large?v=v2&amp;amp;px=999" role="button" title="S32K396BMS BMS&amp;amp;VCU PoC.png" alt="S32K396BMS BMS&amp;amp;VCU PoC.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 26 Sep 2025 00:57:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Problems-using-BMS-GEN1-SDK-4-4-and-R21-11-Version-1-0-3/m-p/2176156#M13786</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2025-09-26T00:57:50Z</dc:date>
    </item>
    <item>
      <title>Re: Problems using BMS GEN1 SDK 4.4 and R21-11 Version 1.0.3</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Problems-using-BMS-GEN1-SDK-4-4-and-R21-11-Version-1-0-3/m-p/2337223#M14130</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/57959"&gt;@Robin_Shen&lt;/a&gt;&amp;nbsp;&amp;nbsp;:&lt;/P&gt;&lt;P&gt;I have the same problem, so that me confirm again, I can't use install &lt;SPAN&gt;S32K3 BMS SDK AUTOSAR 4.4 R21-11 Version 1.0.2 based on&amp;nbsp;&lt;/SPAN&gt;S32DS3.6 version? Because there are MC33772 &amp;amp; MC33774 MCAL driver inside it, there are not inside BMS SDK GEN2, it's necessary for our project.&lt;/P&gt;&lt;P&gt;Do you have any idea or suggestion?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;BR, BillWen&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 23 Mar 2026 00:16:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Problems-using-BMS-GEN1-SDK-4-4-and-R21-11-Version-1-0-3/m-p/2337223#M14130</guid>
      <dc:creator>BillWen</dc:creator>
      <dc:date>2026-03-23T00:16:29Z</dc:date>
    </item>
  </channel>
</rss>