<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Standalone NXP GCC Toolchain for S32K in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Standalone-NXP-GCC-Toolchain-for-S32K/m-p/2196194#M13855</link>
    <description>&lt;P&gt;I found the location to download the toolchains. It looks as if the one I want is:&lt;/P&gt;&lt;H4&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;NXP_GCC11-4_eARMv7&lt;/SPAN&gt;_gf703eb2-LINUX&lt;/SPAN&gt;&lt;/H4&gt;&lt;P&gt;But it says that it's a .bin but when I run it either with "bash file.bin" or "chmod +x file.bin; ./file.bin" I get the error below.&lt;/P&gt;&lt;P&gt;Why would Java be in the mix? Is there tarball version of these tool. There is a tarball for the GCC tools but I assume this not the NXP adapted compiler (which I need to build the RTD).&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;Preparing to install&lt;BR /&gt;Extracting the installation resources from the installer archive...&lt;BR /&gt;Configuring the installer for this system's environment...&lt;BR /&gt;No Java virtual machine could be found from your PATH&lt;BR /&gt;environment variable. You must install a VM prior to&lt;BR /&gt;running this program.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 31 Oct 2025 00:50:10 GMT</pubDate>
    <dc:creator>greenwichmeanie</dc:creator>
    <dc:date>2025-10-31T00:50:10Z</dc:date>
    <item>
      <title>Standalone NXP GCC Toolchain for S32K</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Standalone-NXP-GCC-Toolchain-for-S32K/m-p/2196194#M13855</link>
      <description>&lt;P&gt;I found the location to download the toolchains. It looks as if the one I want is:&lt;/P&gt;&lt;H4&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;NXP_GCC11-4_eARMv7&lt;/SPAN&gt;_gf703eb2-LINUX&lt;/SPAN&gt;&lt;/H4&gt;&lt;P&gt;But it says that it's a .bin but when I run it either with "bash file.bin" or "chmod +x file.bin; ./file.bin" I get the error below.&lt;/P&gt;&lt;P&gt;Why would Java be in the mix? Is there tarball version of these tool. There is a tarball for the GCC tools but I assume this not the NXP adapted compiler (which I need to build the RTD).&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;Preparing to install&lt;BR /&gt;Extracting the installation resources from the installer archive...&lt;BR /&gt;Configuring the installer for this system's environment...&lt;BR /&gt;No Java virtual machine could be found from your PATH&lt;BR /&gt;environment variable. You must install a VM prior to&lt;BR /&gt;running this program.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 31 Oct 2025 00:50:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Standalone-NXP-GCC-Toolchain-for-S32K/m-p/2196194#M13855</guid>
      <dc:creator>greenwichmeanie</dc:creator>
      <dc:date>2025-10-31T00:50:10Z</dc:date>
    </item>
  </channel>
</rss>