<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: Program &amp;quot;arm-none-eabi-g++&amp;quot; not found in PATH</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Program-quot-arm-none-eabi-g-quot-not-found-in-PATH/m-p/2119710#M13553</link>
    <description>&lt;P&gt;Thank you for your answer.&lt;BR /&gt;I got an error when I imported a project created in V3.5.&lt;BR /&gt;I'll study more using the example projects and then ask a question.&lt;/P&gt;</description>
    <pubDate>Thu, 19 Jun 2025 22:37:27 GMT</pubDate>
    <dc:creator>batch202563</dc:creator>
    <dc:date>2025-06-19T22:37:27Z</dc:date>
    <item>
      <title>Program "arm-none-eabi-g++" not found in PATH</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Program-quot-arm-none-eabi-g-quot-not-found-in-PATH/m-p/2118244#M13547</link>
      <description>&lt;P&gt;Hello there,&lt;/P&gt;&lt;P&gt;When starting S32DS (V3.6.2), the following error occurs.&lt;/P&gt;&lt;P&gt;Description Resource Path Location Type&lt;BR /&gt;Program "arm-none-eabi-g++" not found in PATH T1_powersupply_test Project Properties, C++ Preprocessor Include.../Providers, [CDT S32DS Built-in Compiler Settings] options C/C++ Scanner Discovery Problem&lt;BR /&gt;Program "arm-none-eabi-gcc" not found in PATH T1_powersupply_test Project Properties, C++ Preprocessor Include.../Providers, [CDT S32DS Built-in Compiler Settings] options C/C++ Scanner Discovery Problem&lt;/P&gt;&lt;P&gt;However, the build itself completes successfully.&lt;/P&gt;</description>
      <pubDate>Wed, 18 Jun 2025 05:30:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Program-quot-arm-none-eabi-g-quot-not-found-in-PATH/m-p/2118244#M13547</guid>
      <dc:creator>batch202563</dc:creator>
      <dc:date>2025-06-18T05:30:01Z</dc:date>
    </item>
    <item>
      <title>Re: Program "arm-none-eabi-g++" not found in PATH</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Program-quot-arm-none-eabi-g-quot-not-found-in-PATH/m-p/2119498#M13552</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/251648"&gt;@batch202563&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Could you share which RTD package and product you are using? Also, are you creating an example from scratch and modifying the toolchain settings, or is does this happen with example projects as well?&lt;/P&gt;
&lt;P&gt;I can compile projects correctly in S32DS v3.6.2, however, this seems to be an old issue with eclipse:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;A href="https://www.openstm32.org/forumthread1112" target="_blank"&gt;OpenSTM32 Community Site | Program "arm-none-eabi-g++" not found in PATH&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://forum.arduino.cc/t/arm-none-eabi-g-file-does-not-exist-solved/1288661" target="_blank"&gt;Arm-none-eabi-g++ file does not exist [SOLVED] - Other Hardware / 3rd Party Boards - Arduino Forum&lt;/A&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&lt;SPAN&gt;If it’s working, this is a known bug due the Eclipse indexer synchronization. If you delete the errors or relaunch Eclipse, it should not appear, the error message should not appear.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Julián&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 19 Jun 2025 17:10:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Program-quot-arm-none-eabi-g-quot-not-found-in-PATH/m-p/2119498#M13552</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2025-06-19T17:10:06Z</dc:date>
    </item>
    <item>
      <title>Re: Program "arm-none-eabi-g++" not found in PATH</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Program-quot-arm-none-eabi-g-quot-not-found-in-PATH/m-p/2119710#M13553</link>
      <description>&lt;P&gt;Thank you for your answer.&lt;BR /&gt;I got an error when I imported a project created in V3.5.&lt;BR /&gt;I'll study more using the example projects and then ask a question.&lt;/P&gt;</description>
      <pubDate>Thu, 19 Jun 2025 22:37:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Program-quot-arm-none-eabi-g-quot-not-found-in-PATH/m-p/2119710#M13553</guid>
      <dc:creator>batch202563</dc:creator>
      <dc:date>2025-06-19T22:37:27Z</dc:date>
    </item>
  </channel>
</rss>