<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: Install SDK/RTD into S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Install-SDK-RTD-into-S32-Design-Studio/m-p/2090076#M13370</link>
    <description>hello,I have installed S32 Design Studio 3.6.1 and S32K1_S32M24X Real Time Drivers AUTOSAR 4.4 &amp;amp; R21-11 Version 2.0.0, but when I try and create a new S32K116 project, there are no SDK's to choose from . The S32K1_S32M24X Real Time Drivers AUTOSAR 4.4 &amp;amp; R21-11 Version 2.0.0 seems just have S32K118、S32K144、S32K144W、S32K148 example project. Where can i find the S32k166 example project?</description>
    <pubDate>Wed, 30 Apr 2025 09:01:18 GMT</pubDate>
    <dc:creator>Alan_7z</dc:creator>
    <dc:date>2025-04-30T09:01:18Z</dc:date>
    <item>
      <title>Install SDK/RTD into S32 Design Studio</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Install-SDK-RTD-into-S32-Design-Studio/m-p/1779464#M11619</link>
      <description>&lt;P&gt;I have installed S32 Design Studio 3.5 but when I try and create a new S32K144 project, there are no SDK's to choose from !&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ArkAndyFraser_0-1703458157123.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/255729i37CEDDE7A59DCCC8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ArkAndyFraser_0-1703458157123.png" alt="ArkAndyFraser_0-1703458157123.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ArkAndyFraser_0-1703458157123.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is the correct mechanism to install SDKs and what is the difference between SDK and RTD?&lt;/P&gt;&lt;P&gt;I downloaded and installed&amp;nbsp;S32K1 Real Time Drivers AUTOSAR 4.4 Version 1.0.0 but still there are no SDK's listed.&lt;/P&gt;&lt;P&gt;Andy&lt;/P&gt;</description>
      <pubDate>Sun, 24 Dec 2023 22:51:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Install-SDK-RTD-into-S32-Design-Studio/m-p/1779464#M11619</guid>
      <dc:creator>ArkAndyFraser</dc:creator>
      <dc:date>2023-12-24T22:51:31Z</dc:date>
    </item>
    <item>
      <title>Re: Install SDK/RTD into S32 Design Studio</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Install-SDK-RTD-into-S32-Design-Studio/m-p/1780135#M11627</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/222282"&gt;@ArkAndyFraser&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The S32 Software Development Kit (SDK) for S32K1&amp;nbsp; is an extensive suite of peripheral abstraction layers, peripheral drivers, RTOS, stacks, and middleware.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;NOTE: S32DS v3.5 only has support for SDK v4.0.1. The last release of this software is supported by S32DS v3.4.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;On the other hand, the&amp;nbsp;Real-Time Drivers (RTD) are a set supporting real-time software on AUTOSAR and non-AUTOSAR applications targeting Arm® Cortex®-M cores and ISO 26262 compliance for all software layers.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regarding the RTD package installation, firstly, we recommend using the latest release. This can be downloaded from&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K1-RTD44-D" target="_blank" rel="noopener"&gt;Real-Time Drivers for S32K1&lt;/A&gt;&amp;nbsp;-&amp;gt;&amp;nbsp;Automotive SW - S32K1_S32M24x - Real-Time Drivers for Cortex-M -&amp;gt;&amp;nbsp;S32K1_S32M24X Real Time Drivers AUTOSAR 4.4 &amp;amp; R21-11 Version 2.0.0. Download the update site package that can be installed in S32DS through S32 Design Studio Extensions and Updates -&amp;gt; Add Update Sites and select the archive file containing the S32 RTD software.&lt;/P&gt;
&lt;P&gt;Also, check the following&amp;nbsp;S32DS HOWTOs. It might be useful for you.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32DS-Extensions-Updates-Explanation-and-How-To-Use/ta-p/1128543" target="_blank" rel="noopener"&gt;S32DS Extensions &amp;amp; Updates: Explanation and How To Use&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-S32-Design-Studio-Create-a-New-Application-Project/ta-p/1126018" target="_blank" rel="noopener"&gt;HOWTO: S32 Design Studio - Create a New Application Project&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-a-Blinking-LED-example-project-using-S32K1xx-RTD/ta-p/1471695" target="_blank" rel="noopener"&gt;HOWTO: Create a Blinking LED example project using S32K1xx RTD with AUTOSAR&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-a-Blinking-LED-example-project-using-S32K1xx-RTD/ta-p/1471810" target="_blank" rel="noopener"&gt;HOWTO: Create a Blinking LED example project using S32K1xx RTD without AUTOSAR&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R.&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;</description>
      <pubDate>Tue, 26 Dec 2023 19:40:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Install-SDK-RTD-into-S32-Design-Studio/m-p/1780135#M11627</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-12-26T19:40:39Z</dc:date>
    </item>
    <item>
      <title>Re: Install SDK/RTD into S32 Design Studio</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Install-SDK-RTD-into-S32-Design-Studio/m-p/1780589#M11633</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201913"&gt;@VaneB&lt;/a&gt;&amp;nbsp;I am trying to keep S32DS up to date so am trying to migrate away from the SDK and onto RTD.&lt;/P&gt;&lt;P&gt;I think what was confusing me is that I have twelve AUTOSAR RTD packages listed but none of them supported the S32K144 device I am using. However, having downloaded the package you referenced; I can now see the module I need to install.&lt;/P&gt;&lt;P&gt;Many thanks for your help.&lt;/P&gt;&lt;P&gt;Andy&lt;/P&gt;</description>
      <pubDate>Wed, 27 Dec 2023 16:12:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Install-SDK-RTD-into-S32-Design-Studio/m-p/1780589#M11633</guid>
      <dc:creator>ArkAndyFraser</dc:creator>
      <dc:date>2023-12-27T16:12:31Z</dc:date>
    </item>
    <item>
      <title>Re: Install SDK/RTD into S32 Design Studio</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Install-SDK-RTD-into-S32-Design-Studio/m-p/2090076#M13370</link>
      <description>hello,I have installed S32 Design Studio 3.6.1 and S32K1_S32M24X Real Time Drivers AUTOSAR 4.4 &amp;amp; R21-11 Version 2.0.0, but when I try and create a new S32K116 project, there are no SDK's to choose from . The S32K1_S32M24X Real Time Drivers AUTOSAR 4.4 &amp;amp; R21-11 Version 2.0.0 seems just have S32K118、S32K144、S32K144W、S32K148 example project. Where can i find the S32k166 example project?</description>
      <pubDate>Wed, 30 Apr 2025 09:01:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Install-SDK-RTD-into-S32-Design-Studio/m-p/2090076#M13370</guid>
      <dc:creator>Alan_7z</dc:creator>
      <dc:date>2025-04-30T09:01:18Z</dc:date>
    </item>
  </channel>
</rss>