<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design Studioのトピックi can not see example poject pin map</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/i-can-not-see-example-poject-pin-map/m-p/2080315#M13310</link>
    <description>&lt;P&gt;i am using s32ds 3.6.1version. rtd 4.0.0 , s32k344.&lt;/P&gt;&lt;P&gt;after i download rtd 4.0.0 and i open the porject.&amp;nbsp;&lt;/P&gt;&lt;P&gt;but i can not see example project pinmap.&amp;nbsp;&lt;/P&gt;&lt;P&gt;i got a message that project is old version.,&amp;nbsp;&lt;/P&gt;&lt;P&gt;so i installed s32ds 3.5 version. but i get same issue.&amp;nbsp;&lt;/P&gt;&lt;P&gt;and i failed install s32ds 3.4 version.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. how i can see that project well? pin, driver, clock and so on.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="화면 캡처 2025-04-15 105527.png" style="width: 459px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/333006i8C4BCAD9A00327AA/image-size/large?v=v2&amp;amp;px=999" role="button" title="화면 캡처 2025-04-15 105527.png" alt="화면 캡처 2025-04-15 105527.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. i got a activation code for 3.4 version. but it is not work.&amp;nbsp;&lt;/P&gt;&lt;P&gt;how i can install s32ds 3.4 version ?&lt;/P&gt;&lt;P&gt;i already have install file s32ds 3.4version. i download in nxp.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks for regards.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 15 Apr 2025 02:03:14 GMT</pubDate>
    <dc:creator>rlaxortn</dc:creator>
    <dc:date>2025-04-15T02:03:14Z</dc:date>
    <item>
      <title>i can not see example poject pin map</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/i-can-not-see-example-poject-pin-map/m-p/2080315#M13310</link>
      <description>&lt;P&gt;i am using s32ds 3.6.1version. rtd 4.0.0 , s32k344.&lt;/P&gt;&lt;P&gt;after i download rtd 4.0.0 and i open the porject.&amp;nbsp;&lt;/P&gt;&lt;P&gt;but i can not see example project pinmap.&amp;nbsp;&lt;/P&gt;&lt;P&gt;i got a message that project is old version.,&amp;nbsp;&lt;/P&gt;&lt;P&gt;so i installed s32ds 3.5 version. but i get same issue.&amp;nbsp;&lt;/P&gt;&lt;P&gt;and i failed install s32ds 3.4 version.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. how i can see that project well? pin, driver, clock and so on.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="화면 캡처 2025-04-15 105527.png" style="width: 459px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/333006i8C4BCAD9A00327AA/image-size/large?v=v2&amp;amp;px=999" role="button" title="화면 캡처 2025-04-15 105527.png" alt="화면 캡처 2025-04-15 105527.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. i got a activation code for 3.4 version. but it is not work.&amp;nbsp;&lt;/P&gt;&lt;P&gt;how i can install s32ds 3.4 version ?&lt;/P&gt;&lt;P&gt;i already have install file s32ds 3.4version. i download in nxp.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks for regards.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Apr 2025 02:03:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/i-can-not-see-example-poject-pin-map/m-p/2080315#M13310</guid>
      <dc:creator>rlaxortn</dc:creator>
      <dc:date>2025-04-15T02:03:14Z</dc:date>
    </item>
    <item>
      <title>Re: i can not see example poject pin map</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/i-can-not-see-example-poject-pin-map/m-p/2080530#M13314</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;If it is a new project, it is recommended to use the latest S32K3 RTD &lt;STRONG&gt;5.0.0&lt;/STRONG&gt; + S32DS &lt;STRONG&gt;v3.6&lt;/STRONG&gt;.&lt;/P&gt;
&lt;P&gt;Or refer to &lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-offline-install-S32K3-RTD-4-0-0-in-S32DS-v3-5/ta-p/1968014" target="_self"&gt;HOWTO: offline install S32K3 RTD 4.0.0 in S32DS v3.5&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 15 Apr 2025 06:50:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/i-can-not-see-example-poject-pin-map/m-p/2080530#M13314</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2025-04-15T06:50:16Z</dc:date>
    </item>
  </channel>
</rss>