<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: Install S32DS on Windows without using built-in Java</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Install-S32DS-on-Windows-without-using-built-in-Java/m-p/2071068#M13271</link>
    <description>&lt;P&gt;I'm searching for an option to have a (Windows 11 -) installer for S32DS without JRE (similar to the one for Linux). Maybe some of the NXP-staff?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance&lt;/P&gt;</description>
    <pubDate>Mon, 31 Mar 2025 10:30:44 GMT</pubDate>
    <dc:creator>Manuel314</dc:creator>
    <dc:date>2025-03-31T10:30:44Z</dc:date>
    <item>
      <title>Install S32DS on Windows without using built-in Java</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Install-S32DS-on-Windows-without-using-built-in-Java/m-p/2067301#M13260</link>
      <description>&lt;P&gt;Hello cummulity,&lt;/P&gt;&lt;P&gt;In my company the IT is blocking the use of Oracle Java for security reasons. They have provided us all with an alternative build of Java that is installed on all our computers.&lt;/P&gt;&lt;P&gt;I now want to install S32DS on my windows 11 machine, but want to use the JRE that is already available on the computer.&lt;/P&gt;&lt;P&gt;I have found that the S32DS installer always tries to run the JRE that is included in the installer package and is then blocked by our firewall and I can't install it.&lt;/P&gt;&lt;P&gt;Since the installer package for Linux does not include a JRE, is there such an option for windows as well?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Mon, 24 Mar 2025 13:50:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Install-S32DS-on-Windows-without-using-built-in-Java/m-p/2067301#M13260</guid>
      <dc:creator>Manuel314</dc:creator>
      <dc:date>2025-03-24T13:50:22Z</dc:date>
    </item>
    <item>
      <title>Re: Install S32DS on Windows without using built-in Java</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Install-S32DS-on-Windows-without-using-built-in-Java/m-p/2071068#M13271</link>
      <description>&lt;P&gt;I'm searching for an option to have a (Windows 11 -) installer for S32DS without JRE (similar to the one for Linux). Maybe some of the NXP-staff?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance&lt;/P&gt;</description>
      <pubDate>Mon, 31 Mar 2025 10:30:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Install-S32DS-on-Windows-without-using-built-in-Java/m-p/2071068#M13271</guid>
      <dc:creator>Manuel314</dc:creator>
      <dc:date>2025-03-31T10:30:44Z</dc:date>
    </item>
    <item>
      <title>Re: Install S32DS on Windows without using built-in Java</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Install-S32DS-on-Windows-without-using-built-in-Java/m-p/2071938#M13280</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;you can specify java vm in s32ds.ini file (located in c:\NXP\S32DS.3.6.0\eclipse\&amp;nbsp; folder) once S32DS is installed. But windows installer itself uses build in java vm.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 01 Apr 2025 09:42:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Install-S32DS-on-Windows-without-using-built-in-Java/m-p/2071938#M13280</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2025-04-01T09:42:58Z</dc:date>
    </item>
    <item>
      <title>Re: Install S32DS on Windows without using built-in Java</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Install-S32DS-on-Windows-without-using-built-in-Java/m-p/2071956#M13281</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;that is the very problem I'm facing. I can't run the installer, because it uses the build-in java vm.&lt;/P&gt;&lt;P&gt;Since the installer for Linux does not, I asked myself, if something similar would be available for windows.&lt;/P&gt;</description>
      <pubDate>Tue, 01 Apr 2025 10:15:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Install-S32DS-on-Windows-without-using-built-in-Java/m-p/2071956#M13281</guid>
      <dc:creator>Manuel314</dc:creator>
      <dc:date>2025-04-01T10:15:29Z</dc:date>
    </item>
    <item>
      <title>Re: Install S32DS on Windows without using built-in Java</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Install-S32DS-on-Windows-without-using-built-in-Java/m-p/2102947#M13448</link>
      <description>&lt;P&gt;Has there been any update to this? I am facing the same issue.&lt;/P&gt;</description>
      <pubDate>Thu, 22 May 2025 20:06:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Install-S32DS-on-Windows-without-using-built-in-Java/m-p/2102947#M13448</guid>
      <dc:creator>scallaway21</dc:creator>
      <dc:date>2025-05-22T20:06:40Z</dc:date>
    </item>
    <item>
      <title>Re: Install S32DS on Windows without using built-in Java</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Install-S32DS-on-Windows-without-using-built-in-Java/m-p/2103145#M13450</link>
      <description>&lt;P&gt;I have found sort-of a solution together with our IT-department. My issue exactly is, that only Oracle-Java is blocked. The newer versions of S32DS don't use Oracle Java (like 3.4, which we are using) anymore but OpenJDK. A solution would be to simply update to the newest version.&lt;/P&gt;&lt;P&gt;In our particular case that is not an easy option since our project relies on features that 3.4 has and 3.5up does not support anymore.&lt;/P&gt;</description>
      <pubDate>Fri, 23 May 2025 05:13:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Install-S32DS-on-Windows-without-using-built-in-Java/m-p/2103145#M13450</guid>
      <dc:creator>Manuel314</dc:creator>
      <dc:date>2025-05-23T05:13:18Z</dc:date>
    </item>
  </channel>
</rss>