<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: Debug probe ethernet connection</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Debug-probe-ethernet-connection/m-p/2051241#M13119</link>
    <description>&lt;P&gt;&lt;SPAN&gt;"with older probes on some PCs is issue with the USB - the USB on older probes acts as Ethernet over USB and in some cases OS can't handle it. " --Is there any methods to solve this problem?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 26 Feb 2025 02:20:28 GMT</pubDate>
    <dc:creator>Catherine</dc:creator>
    <dc:date>2025-02-26T02:20:28Z</dc:date>
    <item>
      <title>Debug probe ethernet connection</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Debug-probe-ethernet-connection/m-p/2049515#M13107</link>
      <description>&lt;P&gt;Hi expert,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; Customer is using S32DS on physical ubuntu 22.04, and found problems on connecting the debug probe. Here is the screenshot.&lt;/P&gt;
&lt;DIV id="tinyMceEditorCatherine_0" class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image (2).png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/325255iC98BF6C0C2C7000A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="image (2).png" alt="image (2).png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;image (2).png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt; &lt;/P&gt;
&lt;P&gt;It seems that there is something error in connecting by the usb. So my question is&lt;/P&gt;
&lt;P&gt;(1) Is it an issue of connecting usb? If yes, how to solve this issue?&lt;/P&gt;
&lt;P&gt;(2)Is there any hands-on tutorial of connecting debug probe by ethernet?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 24 Feb 2025 01:59:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Debug-probe-ethernet-connection/m-p/2049515#M13107</guid>
      <dc:creator>Catherine</dc:creator>
      <dc:date>2025-02-24T01:59:07Z</dc:date>
    </item>
    <item>
      <title>Re: Debug probe ethernet connection</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Debug-probe-ethernet-connection/m-p/2050910#M13114</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;with older probes on some PCs is issue with the USB - the USB on older probes acts as Ethernet over USB and in some cases OS can't handle it.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;To use debug probe with Ethernet connection you can simply connect probe to network with DHCP server and use probe's domain name (or assigned IP address).&amp;nbsp; If you need static IP for probe (for example with missing DHCP server) you can use this HOWTO document -&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Setup-static-IP-address-for-S32-debug-probe/ta-p/1103006" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Setup-static-IP-address-for-S32-debug-probe/ta-p/1103006&lt;/A&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 25 Feb 2025 15:00:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Debug-probe-ethernet-connection/m-p/2050910#M13114</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2025-02-25T15:00:14Z</dc:date>
    </item>
    <item>
      <title>Re: Debug probe ethernet connection</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Debug-probe-ethernet-connection/m-p/2051241#M13119</link>
      <description>&lt;P&gt;&lt;SPAN&gt;"with older probes on some PCs is issue with the USB - the USB on older probes acts as Ethernet over USB and in some cases OS can't handle it. " --Is there any methods to solve this problem?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 26 Feb 2025 02:20:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Debug-probe-ethernet-connection/m-p/2051241#M13119</guid>
      <dc:creator>Catherine</dc:creator>
      <dc:date>2025-02-26T02:20:28Z</dc:date>
    </item>
    <item>
      <title>Re: Debug probe ethernet connection</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Debug-probe-ethernet-connection/m-p/2051756#M13121</link>
      <description>&lt;P&gt;It depends what's the cause. Most usually is the reason that OS security settings (like our NXP PC Image) allows only one ethernet connection and OS disable second Eth - which is Debug Probe's Ethernet over USB interface.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;It may be also some driver issue (but in this case it looks that driver is okay), user privileges issue - can user access /dev/ttyACM0 device?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I suggest to focus on OS settings.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 26 Feb 2025 12:14:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Debug-probe-ethernet-connection/m-p/2051756#M13121</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2025-02-26T12:14:58Z</dc:date>
    </item>
  </channel>
</rss>