<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックIssue with CAN0 Communication on Custom S32K144 Board</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Issue-with-CAN0-Communication-on-Custom-S32K144-Board/m-p/2042517#M13076</link>
    <description>&lt;P&gt;Hello team,&lt;/P&gt;&lt;P&gt;We are working with a custom board using the S32K144 (LQFP64 64-pin package) and S32 Design Studio v2.2. Using&amp;nbsp;processor expert we have generated code.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Working Configuration:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;CAN1 (CANpal component) is configured with PTC6 and PTC7.&lt;/LI&gt;&lt;LI&gt;CAN communication (send/receive) is working as expected.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;STRONG&gt;Non-working Configuration:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;CAN0 (CANpal component) is configured with PTC2 and PTC3.&lt;/LI&gt;&lt;LI&gt;CAN communication (send/receive) is not functioning.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Could you please advise on steps to resolve this issue?&lt;/P&gt;</description>
    <pubDate>Wed, 12 Feb 2025 09:59:16 GMT</pubDate>
    <dc:creator>stark21</dc:creator>
    <dc:date>2025-02-12T09:59:16Z</dc:date>
    <item>
      <title>Issue with CAN0 Communication on Custom S32K144 Board</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Issue-with-CAN0-Communication-on-Custom-S32K144-Board/m-p/2042517#M13076</link>
      <description>&lt;P&gt;Hello team,&lt;/P&gt;&lt;P&gt;We are working with a custom board using the S32K144 (LQFP64 64-pin package) and S32 Design Studio v2.2. Using&amp;nbsp;processor expert we have generated code.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Working Configuration:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;CAN1 (CANpal component) is configured with PTC6 and PTC7.&lt;/LI&gt;&lt;LI&gt;CAN communication (send/receive) is working as expected.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;STRONG&gt;Non-working Configuration:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;CAN0 (CANpal component) is configured with PTC2 and PTC3.&lt;/LI&gt;&lt;LI&gt;CAN communication (send/receive) is not functioning.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Could you please advise on steps to resolve this issue?&lt;/P&gt;</description>
      <pubDate>Wed, 12 Feb 2025 09:59:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Issue-with-CAN0-Communication-on-Custom-S32K144-Board/m-p/2042517#M13076</guid>
      <dc:creator>stark21</dc:creator>
      <dc:date>2025-02-12T09:59:16Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with CAN0 Communication on Custom S32K144 Board</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Issue-with-CAN0-Communication-on-Custom-S32K144-Board/m-p/2042818#M13080</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I assume there is no hardware conflict on your custom board (CAN0 interface) so the CAN_H and CAN_L pins are routed and treated similarly as in case of CAN1 interface.&amp;nbsp; If you are using higer baudrate please also double-check the presense of termination resistor 120 Ohm.&lt;/P&gt;
&lt;P&gt;I'd also validate Sending a data from your board over CAN0 - measure CAN_TX&amp;nbsp; (TTL) signal using logic analyzer to see the output is present on pin.&amp;nbsp; You can hook the signal e.g on CAN trancevier (TTL Tx pin).&lt;/P&gt;
&lt;P&gt;If you do not see any activity on pin, after sending a data I'd suggest you to run the debug ession with Non-Working Configuration, execute code and stop right after CAN initialization.&lt;/P&gt;
&lt;P&gt;Then please check GPIO pinmux registers - so GPIO PTC2 and PTC3 are set to alt 3.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="stanish_0-1739387404538.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/323679iC19355E1F2210200/image-size/medium?v=v2&amp;amp;px=400" role="button" title="stanish_0-1739387404538.png" alt="stanish_0-1739387404538.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;stanish_0-1739387404538.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="stanish_1-1739387527860.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/323680i9AFDF395F7CEC329/image-size/medium?v=v2&amp;amp;px=400" role="button" title="stanish_1-1739387527860.png" alt="stanish_1-1739387527860.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;stanish_1-1739387527860.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;If it does not help please send us more information about the issue you observe.&lt;/P&gt;
&lt;P&gt;Hope it helps.&lt;/P&gt;
&lt;P&gt;Stan&lt;/P&gt;</description>
      <pubDate>Wed, 12 Feb 2025 19:13:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Issue-with-CAN0-Communication-on-Custom-S32K144-Board/m-p/2042818#M13080</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2025-02-12T19:13:04Z</dc:date>
    </item>
  </channel>
</rss>