<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design Studio中的主题 Re: having a single elf for multiple projects(application, bootloader , bootmanager)</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/having-a-single-elf-for-multiple-projects-application-bootloader/m-p/2041707#M13068</link>
    <description>&lt;P&gt;&lt;A href="https://community.nxp.com/t5/MPC5xxx/linking-single-elf-file-for-multiple-bootloader-and-applicationn/m-p/2041706/highlight/true#M27260" target="_blank"&gt;https://community.nxp.com/t5/MPC5xxx/linking-single-elf-file-for-multiple-bootloader-and-applicationn/m-p/2041706/highlight/true#M27260&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 11 Feb 2025 10:38:33 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2025-02-11T10:38:33Z</dc:date>
    <item>
      <title>having a single elf for multiple projects(application, bootloader , bootmanager)</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/having-a-single-elf-for-multiple-projects-application-bootloader/m-p/2041328#M13065</link>
      <description>&lt;P&gt;I'm currently trying to get a boot-manager/ bootloader/application to be linked as a single .elf file for the MPC5748G.&lt;/P&gt;&lt;P&gt;There are some issues that I'm a little confused about, and I would be very grateful if you could provide any guidance with regard to them.&lt;/P&gt;&lt;P&gt;The plan is to always boot the boot-manager and then jump to the application or the application according to the value of some flag. How to combine all 3 software entities into one instead of flashing each one on its own and if I manage to do that, would I be able to access the code of bootloader or application after jumping?&lt;/P&gt;&lt;P&gt;I have already defined different start and end addresses of each entity in the linker file and developed the jumping mechanism&lt;/P&gt;</description>
      <pubDate>Tue, 11 Feb 2025 02:31:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/having-a-single-elf-for-multiple-projects-application-bootloader/m-p/2041328#M13065</guid>
      <dc:creator>Tarek72</dc:creator>
      <dc:date>2025-02-11T02:31:46Z</dc:date>
    </item>
    <item>
      <title>Re: having a single elf for multiple projects(application, bootloader , bootmanager)</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/having-a-single-elf-for-multiple-projects-application-bootloader/m-p/2041707#M13068</link>
      <description>&lt;P&gt;&lt;A href="https://community.nxp.com/t5/MPC5xxx/linking-single-elf-file-for-multiple-bootloader-and-applicationn/m-p/2041706/highlight/true#M27260" target="_blank"&gt;https://community.nxp.com/t5/MPC5xxx/linking-single-elf-file-for-multiple-bootloader-and-applicationn/m-p/2041706/highlight/true#M27260&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 11 Feb 2025 10:38:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/having-a-single-elf-for-multiple-projects-application-bootloader/m-p/2041707#M13068</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2025-02-11T10:38:33Z</dc:date>
    </item>
  </channel>
</rss>