<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FreeRTOS extension on S32 Design Studio 3.6 in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/FreeRTOS-extension-on-S32-Design-Studio-3-6/m-p/2036544#M13026</link>
    <description>&lt;P&gt;Hello everyone. I'm trying to use the latest FreeRTOS extension (SW32K3_FreeRTOS_11.1.0_5.0.0_CD1_D2409_DesignStudio_updatesite.zip) with S32 Design Studio 3.6, but every time that I add it to the source list nothing happens.&lt;/P&gt;&lt;P&gt;With S32 Design Studio I don't have this issue, I can easily import the .zip file and then immediately install the extension. I would use version 3.5 if I could, but for some reason I can only set it up on Windows, on Linux I can't get past the license check.&lt;/P&gt;&lt;P&gt;Given that I have to work on a Linux host and so&amp;nbsp;S32 Design Studio 3.6 is my only available choice, how do I install the FreeRTOS extension?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
    <pubDate>Fri, 31 Jan 2025 11:14:40 GMT</pubDate>
    <dc:creator>Wolver</dc:creator>
    <dc:date>2025-01-31T11:14:40Z</dc:date>
    <item>
      <title>FreeRTOS extension on S32 Design Studio 3.6</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/FreeRTOS-extension-on-S32-Design-Studio-3-6/m-p/2036544#M13026</link>
      <description>&lt;P&gt;Hello everyone. I'm trying to use the latest FreeRTOS extension (SW32K3_FreeRTOS_11.1.0_5.0.0_CD1_D2409_DesignStudio_updatesite.zip) with S32 Design Studio 3.6, but every time that I add it to the source list nothing happens.&lt;/P&gt;&lt;P&gt;With S32 Design Studio I don't have this issue, I can easily import the .zip file and then immediately install the extension. I would use version 3.5 if I could, but for some reason I can only set it up on Windows, on Linux I can't get past the license check.&lt;/P&gt;&lt;P&gt;Given that I have to work on a Linux host and so&amp;nbsp;S32 Design Studio 3.6 is my only available choice, how do I install the FreeRTOS extension?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Fri, 31 Jan 2025 11:14:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/FreeRTOS-extension-on-S32-Design-Studio-3-6/m-p/2036544#M13026</guid>
      <dc:creator>Wolver</dc:creator>
      <dc:date>2025-01-31T11:14:40Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS extension on S32 Design Studio 3.6</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/FreeRTOS-extension-on-S32-Design-Studio-3-6/m-p/2036713#M13030</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/246231"&gt;@Wolver&lt;/a&gt;.&lt;/P&gt;
&lt;P&gt;Unfortunately, RTDs are not supported on a Linux host. The reason for this is that Linux is a case sensitive operative system which can cause conflicts within some filenames, although RTDs can be used, a proper functionality is not guaranteed.&lt;/P&gt;
&lt;P&gt;This same topic is treated in the following post: "&lt;A href="https://community.nxp.com/t5/S32-Design-Studio/S32K3-SDK-Re-Attach-RTD-SDK-from-command-line/m-p/1463363/highlight/true#M8614" target="_blank" rel="noopener"&gt;S32K3 SDK: Re-Attach RTD-SDK from command line&lt;/A&gt;", please let me know if the information is useful and we're sorry for the inconveniences.&lt;/P&gt;
&lt;P&gt;- RomanVR.&lt;/P&gt;</description>
      <pubDate>Fri, 31 Jan 2025 18:30:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/FreeRTOS-extension-on-S32-Design-Studio-3-6/m-p/2036713#M13030</guid>
      <dc:creator>RomanVR</dc:creator>
      <dc:date>2025-01-31T18:30:47Z</dc:date>
    </item>
  </channel>
</rss>