<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32DS install S32M24x_RTD got error in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-install-S32M24x-RTD-got-error/m-p/2009587#M12854</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;如果在线安装RTD失败，请尝试离线安装RTD的方法：&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-offline-install-S32K1-RTD-2-0-0-in-S32DS-v3-5/ta-p/1927845" target="_self"&gt;HOWTO: offline install S32K1 RTD 2.0.0 in S32DS v3.5&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Mon, 09 Dec 2024 01:07:22 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2024-12-09T01:07:22Z</dc:date>
    <item>
      <title>S32DS install S32M24x_RTD got error</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-install-S32M24x-RTD-got-error/m-p/2009484#M12852</link>
      <description>&lt;P&gt;我正在尝试安装 SW32K1_S32M24x_RTD_R21-11_2.0.0_QLP1_DS_updatesite_D2408，但它失败了，并附加了日志错误文件。&lt;/P&gt;&lt;P&gt;您能帮忙检查一下吗？&lt;/P&gt;</description>
      <pubDate>Sat, 07 Dec 2024 11:17:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-install-S32M24x-RTD-got-error/m-p/2009484#M12852</guid>
      <dc:creator>yuan28149</dc:creator>
      <dc:date>2024-12-07T11:17:23Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS install S32M24x_RTD got error</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-install-S32M24x-RTD-got-error/m-p/2009528#M12853</link>
      <description>&lt;P&gt;By the way, the version is 3.5.14.&lt;/P&gt;&lt;P&gt;The suggestion is using 3.5.12, but now the extension can not find this one.&lt;/P&gt;</description>
      <pubDate>Sun, 08 Dec 2024 06:09:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-install-S32M24x-RTD-got-error/m-p/2009528#M12853</guid>
      <dc:creator>yuan28149</dc:creator>
      <dc:date>2024-12-08T06:09:25Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS install S32M24x_RTD got error</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-install-S32M24x-RTD-got-error/m-p/2009587#M12854</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;如果在线安装RTD失败，请尝试离线安装RTD的方法：&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-offline-install-S32K1-RTD-2-0-0-in-S32DS-v3-5/ta-p/1927845" target="_self"&gt;HOWTO: offline install S32K1 RTD 2.0.0 in S32DS v3.5&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 09 Dec 2024 01:07:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-install-S32M24x-RTD-got-error/m-p/2009587#M12854</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-12-09T01:07:22Z</dc:date>
    </item>
  </channel>
</rss>