<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic laxcc help in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/laxcc-help/m-p/1971277#M12702</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm trying to work on a customer issue. They are using the S32 Design suite which is launching the laxcc compiler. I've downloaded a copy and I can run laxcc but I can't find any documentation on it. When I run it with -help, it claims to be a compiler called it3a-cc.&lt;/P&gt;&lt;P&gt;Specifically, what does the -env option do? The help says&amp;nbsp;&lt;/P&gt;&lt;P&gt;" -env # specify a non-standard environment path"&lt;BR /&gt;&lt;BR /&gt;What is an environment path and what would a standard one be?&lt;BR /&gt;&lt;BR /&gt;Thanks.&lt;BR /&gt;&lt;BR /&gt;Peter&lt;/P&gt;</description>
    <pubDate>Thu, 10 Oct 2024 10:19:53 GMT</pubDate>
    <dc:creator>PeterSmithson</dc:creator>
    <dc:date>2024-10-10T10:19:53Z</dc:date>
    <item>
      <title>laxcc help</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/laxcc-help/m-p/1971277#M12702</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm trying to work on a customer issue. They are using the S32 Design suite which is launching the laxcc compiler. I've downloaded a copy and I can run laxcc but I can't find any documentation on it. When I run it with -help, it claims to be a compiler called it3a-cc.&lt;/P&gt;&lt;P&gt;Specifically, what does the -env option do? The help says&amp;nbsp;&lt;/P&gt;&lt;P&gt;" -env # specify a non-standard environment path"&lt;BR /&gt;&lt;BR /&gt;What is an environment path and what would a standard one be?&lt;BR /&gt;&lt;BR /&gt;Thanks.&lt;BR /&gt;&lt;BR /&gt;Peter&lt;/P&gt;</description>
      <pubDate>Thu, 10 Oct 2024 10:19:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/laxcc-help/m-p/1971277#M12702</guid>
      <dc:creator>PeterSmithson</dc:creator>
      <dc:date>2024-10-10T10:19:53Z</dc:date>
    </item>
  </channel>
</rss>