<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: S32K344 Example Not working, Unresolved inclusions</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32K344-Example-Not-working-Unresolved-inclusions/m-p/1917813#M12567</link>
    <description>&lt;P&gt;Found the issue, when trying to remake the example for the K342, the peripherals by default only had siul2 port by default which made only some of the headers valid after code generation which confused me, using the Siul2_dio_ip_Example_S32k344 example and manually adding the siul2_dio peripheral and then code generating let it work.&lt;/P&gt;</description>
    <pubDate>Fri, 26 Jul 2024 05:54:26 GMT</pubDate>
    <dc:creator>pb632146</dc:creator>
    <dc:date>2024-07-26T05:54:26Z</dc:date>
    <item>
      <title>S32K344 Example Not working, Unresolved inclusions</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32K344-Example-Not-working-Unresolved-inclusions/m-p/1916640#M12563</link>
      <description>&lt;P&gt;I am trying to use the Emios_Icu_Ip_BlinkLED and DIO_Example_S32K344&amp;nbsp; examples fond in S32K3xx AUTOSAR 4.4 - R21-11 RTD 3.0.0 D23 for really simple led blinking, but I am running into the issue of unresolved inclusions for the libraries within.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="pb632146_1-1721857242713.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/290191iA7FA113D2E95A462/image-size/medium?v=v2&amp;amp;px=400" role="button" title="pb632146_1-1721857242713.png" alt="pb632146_1-1721857242713.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;pb632146_1-1721857242713.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="pb632146_0-1721856680035.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/290188i07FD1DD4F0C18F68/image-size/medium?v=v2&amp;amp;px=400" role="button" title="pb632146_0-1721856680035.png" alt="pb632146_0-1721856680035.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;pb632146_0-1721856680035.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I can see the files in \NXP\S32DS.3.5\eclipse\mcu_data\components\PlatformSDK_S32K3\ but they just do not seem to be including after code generation, what should I do?&lt;/P&gt;</description>
      <pubDate>Wed, 24 Jul 2024 21:41:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32K344-Example-Not-working-Unresolved-inclusions/m-p/1916640#M12563</guid>
      <dc:creator>pb632146</dc:creator>
      <dc:date>2024-07-24T21:41:03Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 Example Not working, Unresolved inclusions</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32K344-Example-Not-working-Unresolved-inclusions/m-p/1917325#M12564</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/230291"&gt;@pb632146&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Before running the example is required to generate some configurations. Select the "S32 Configuration Tool" menu then click on the desired configuration tool (Pins, Cocks, Peripherals etc...) and select the current project. Make the desired changes(if any) then click on the S32 Configuration Tool &amp;gt; "Update Code" button.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
      <pubDate>Thu, 25 Jul 2024 16:25:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32K344-Example-Not-working-Unresolved-inclusions/m-p/1917325#M12564</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2024-07-25T16:25:22Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 Example Not working, Unresolved inclusions</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32K344-Example-Not-working-Unresolved-inclusions/m-p/1917586#M12565</link>
      <description>&lt;P&gt;The Code generation is not doing anything for me and I do not understand why.&lt;/P&gt;&lt;P&gt;I can see where I presume the headers would be pulling from, is there a place I need to add the file path to to fix this or something?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="pb632146_0-1721942770265.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/290422i928E475F7BE9B804/image-size/medium?v=v2&amp;amp;px=400" role="button" title="pb632146_0-1721942770265.png" alt="pb632146_0-1721942770265.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;pb632146_0-1721942770265.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I've set a pin to be a digital output and the code generation updated but the code does not run, I think I am missing something fundamental on this.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="pb632146_1-1721942859241.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/290423iC5881B946C73C733/image-size/medium?v=v2&amp;amp;px=400" role="button" title="pb632146_1-1721942859241.png" alt="pb632146_1-1721942859241.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;pb632146_1-1721942859241.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 25 Jul 2024 21:27:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32K344-Example-Not-working-Unresolved-inclusions/m-p/1917586#M12565</guid>
      <dc:creator>pb632146</dc:creator>
      <dc:date>2024-07-25T21:27:46Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 Example Not working, Unresolved inclusions</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32K344-Example-Not-working-Unresolved-inclusions/m-p/1917602#M12566</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/230291"&gt;@pb632146&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The sample codes are provided ready to run out of the box, with no modifications required beyond generating configurations as mentioned above.&lt;/P&gt;</description>
      <pubDate>Thu, 25 Jul 2024 22:28:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32K344-Example-Not-working-Unresolved-inclusions/m-p/1917602#M12566</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2024-07-25T22:28:41Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 Example Not working, Unresolved inclusions</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32K344-Example-Not-working-Unresolved-inclusions/m-p/1917813#M12567</link>
      <description>&lt;P&gt;Found the issue, when trying to remake the example for the K342, the peripherals by default only had siul2 port by default which made only some of the headers valid after code generation which confused me, using the Siul2_dio_ip_Example_S32k344 example and manually adding the siul2_dio peripheral and then code generating let it work.&lt;/P&gt;</description>
      <pubDate>Fri, 26 Jul 2024 05:54:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32K344-Example-Not-working-Unresolved-inclusions/m-p/1917813#M12567</guid>
      <dc:creator>pb632146</dc:creator>
      <dc:date>2024-07-26T05:54:26Z</dc:date>
    </item>
  </channel>
</rss>