<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: S32DS Force re-generation of all code</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Force-re-generation-of-all-code/m-p/1910692#M12530</link>
    <description>&lt;P&gt;Thank you Jiri,&lt;/P&gt;&lt;P&gt;I've moved the generated files to another folder, but still S32DS was smart enough to relocate them in the new place - this is the reason why they have not been re-generated on my side. I've now moved the folder outside the workspace scope and it seems to re-generate the files...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 17 Jul 2024 16:22:01 GMT</pubDate>
    <dc:creator>soerenh</dc:creator>
    <dc:date>2024-07-17T16:22:01Z</dc:date>
    <item>
      <title>S32DS Force re-generation of all code</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Force-re-generation-of-all-code/m-p/1904662#M12513</link>
      <description>&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;Is there a way to force re-generation of all code in the generated/ folder of a S32DS workspace project?&lt;/P&gt;&lt;P&gt;It seems that S32DS somehow memorizes files that it has generated and only re-generates them when the underlying configuration has changed. This is not very practical for collaborative develoment and can create differences among different S32DS installations. I'd like to forcefully re-generate all code in generate/ in order to have a consistent status.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tried:&lt;/P&gt;&lt;P&gt;1) to reload the SDK (Manage SDKs -&amp;gt; reload), but that did only overwrite some, but not all files. Siul2_Port_Ip_BOARD_InitPeripherals_PBcfg.h is one example, which isn't re-generated after that&lt;/P&gt;&lt;P&gt;2) deleting the generated/ folder. S32DS dosn't seem to care, but keeps on creating only files if I change the module configuration&lt;/P&gt;&lt;P&gt;3) cleaning the project&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm desperately lost. I believe I have tried every button and setting... any help is much appreciated!&lt;/P&gt;&lt;P&gt;SDK I'm using is PlatformSDK_S32XX_4_0_0_S32G399A_M7_0&lt;/P&gt;&lt;P&gt;S32DS version: 3.5, Build id: 240529 (Update 12)&lt;/P&gt;</description>
      <pubDate>Tue, 09 Jul 2024 17:54:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Force-re-generation-of-all-code/m-p/1904662#M12513</guid>
      <dc:creator>soerenh</dc:creator>
      <dc:date>2024-07-09T17:54:22Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS Force re-generation of all code</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Force-re-generation-of-all-code/m-p/1905320#M12516</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;deleting the generated and RTD folder should work. In project explorer right click on folder name and delete. Then go back into Config Tool and generate code again.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If it still doesn't work, try to create new workspace and import your project into it.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 10 Jul 2024 13:55:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Force-re-generation-of-all-code/m-p/1905320#M12516</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2024-07-10T13:55:29Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS Force re-generation of all code</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Force-re-generation-of-all-code/m-p/1910692#M12530</link>
      <description>&lt;P&gt;Thank you Jiri,&lt;/P&gt;&lt;P&gt;I've moved the generated files to another folder, but still S32DS was smart enough to relocate them in the new place - this is the reason why they have not been re-generated on my side. I've now moved the folder outside the workspace scope and it seems to re-generate the files...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jul 2024 16:22:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Force-re-generation-of-all-code/m-p/1910692#M12530</guid>
      <dc:creator>soerenh</dc:creator>
      <dc:date>2024-07-17T16:22:01Z</dc:date>
    </item>
  </channel>
</rss>