<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: When debugging the &amp;quot;LINFlexD_UART_MPC5744P&amp;quot; example documentation, the following error in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/When-debugging-the-quot-LINFlexD-UART-MPC5744P-quot-example/m-p/1896430#M12477</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;check project setting for Path and Source locations.&lt;BR /&gt;But if you create new project from&amp;nbsp;LINFlexD_UART_MPC5744P demo, it is compiled normally in S32DS.&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Mon, 01 Jul 2024 06:47:24 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2024-07-01T06:47:24Z</dc:date>
    <item>
      <title>When debugging the "LINFlexD_UART_MPC5744P" example documentation, the following error occurred:</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/When-debugging-the-quot-LINFlexD-UART-MPC5744P-quot-example/m-p/1894538#M12464</link>
      <description>&lt;P&gt;**** Incremental Build of configuration Debug for project LINFlexD_UART_MPC5744P ****&lt;BR /&gt;make -j24 all&lt;BR /&gt;Building file: ../src/MPC57xx__Interrupt_Init.c&lt;BR /&gt;Building file: ../src/Vector.c&lt;BR /&gt;Building file: ../src/flashrchw.c&lt;BR /&gt;Building file: ../src/gpio.c&lt;BR /&gt;Building file: ../src/intc_SW_mode_isr_vectors_MPC5744P.c&lt;BR /&gt;Invoking: Standard S32DS C Compiler&lt;BR /&gt;Building file: ../src/intc_sw_handlers.S&lt;BR /&gt;Building file: ../src/linflexd_uart.c&lt;BR /&gt;Building file: ../src/main.c&lt;BR /&gt;Invoking: Standard S32DS C Compiler&lt;BR /&gt;Invoking: Standard S32DS C Compiler&lt;BR /&gt;Building file: ../src/mode_entry.c&lt;BR /&gt;Building file: ../Project_Settings/Startup_Code/startup.S&lt;BR /&gt;powerpc-eabivle-gcc "@src/MPC57xx__Interrupt_Init.args" -MMD -MP -MF"src/flashrchw.d" -MT"src/flashrchw.o" -o "src/flashrchw.o" "../src/flashrchw.c"&lt;BR /&gt;Invoking: Standard S32DS C Compiler&lt;BR /&gt;Invoking: Standard S32DS C Compiler&lt;BR /&gt;Invoking: Standard S32DS Assembler&lt;BR /&gt;Invoking: Standard S32DS C Compiler&lt;BR /&gt;powerpc-eabivle-gcc "@src/MPC57xx__Interrupt_Init.args" -MMD -MP -MF"src/MPC57xx__Interrupt_Init.d" -MT"src/MPC57xx__Interrupt_Init.o" -o "src/MPC57xx__Interrupt_Init.o" "../src/MPC57xx__Interrupt_Init.c"&lt;BR /&gt;powerpc-eabivle-gcc.exe: error: ewl_c9x.specs: No such file or directory&lt;BR /&gt;Invoking: Standard S32DS Assembler&lt;BR /&gt;powerpc-eabivle-gcc "@src/MPC57xx__Interrupt_Init.args" -MMD -MP -MF"src/Vector.d" -MT"src/Vector.o" -o "src/Vector.o" "../src/Vector.c"&lt;BR /&gt;Invoking: Standard S32DS C Compiler&lt;BR /&gt;powerpc-eabivle-gcc "@src/MPC57xx__Interrupt_Init.args" -MMD -MP -MF"src/linflexd_uart.d" -MT"src/linflexd_uart.o" -o "src/linflexd_uart.o" "../src/linflexd_uart.c"&lt;BR /&gt;powerpc-eabivle-gcc "@src/MPC57xx__Interrupt_Init.args" -MMD -MP -MF"src/intc_SW_mode_isr_vectors_MPC5744P.d" -MT"src/intc_SW_mode_isr_vectors_MPC5744P.o" -o "src/intc_SW_mode_isr_vectors_MPC5744P.o" "../src/intc_SW_mode_isr_vectors_MPC5744P.c"&lt;BR /&gt;powerpc-eabivle-gcc.exe: error: ewl_c9x.specs: No such file or directory&lt;BR /&gt;Invoking: Standard S32DS C Compiler&lt;BR /&gt;powerpc-eabivle-gcc "@src/MPC57xx__Interrupt_Init.args" -MMD -MP -MF"src/gpio.d" -MT"src/gpio.o" -o "src/gpio.o" "../src/gpio.c"&lt;BR /&gt;powerpc-eabivle-gcc.exe: error: ewl_c9x.specs: No such file or directory&lt;BR /&gt;powerpc-eabivle-gcc "@src/intc_sw_handlers.args" -o "src/intc_sw_handlers.o" "../src/intc_sw_handlers.S"&lt;BR /&gt;powerpc-eabivle-gcc "@src/MPC57xx__Interrupt_Init.args" -MMD -MP -MF"src/mode_entry.d" -MT"src/mode_entry.o" -o "src/mode_entry.o" "../src/mode_entry.c"&lt;BR /&gt;powerpc-eabivle-gcc.exe: error: ewl_c9x.specs: No such file or directory&lt;BR /&gt;powerpc-eabivle-gcc "@Project_Settings/Startup_Code/startup.args" -o "Project_Settings/Startup_Code/startup.o" "../Project_Settings/Startup_Code/startup.S"&lt;BR /&gt;powerpc-eabivle-gcc.exe: error: ewl_c9x.specs: No such file or directory&lt;BR /&gt;powerpc-eabivle-gcc "@src/MPC57xx__Interrupt_Init.args" -MMD -MP -MF"src/main.d" -MT"src/main.o" -o "src/main.o" "../src/main.c"&lt;BR /&gt;powerpc-eabivle-gcc.exe: error: ewl_c9x.specs: No such file or directory&lt;BR /&gt;make: *** [src/subdir.mk:45: src/flashrchw.o] Error 1&lt;BR /&gt;make: *** Waiting for unfinished jobs....&lt;BR /&gt;powerpc-eabivle-gcc.exe: error: ewl_c9x.specs: No such file or directory&lt;BR /&gt;make: *** [src/subdir.mk:45: src/linflexd_uart.o] Error 1&lt;BR /&gt;make: *** [src/subdir.mk:45: src/Vector.o] Error 1&lt;BR /&gt;make: *** [src/subdir.mk:45: src/MPC57xx__Interrupt_Init.o] Error 1&lt;BR /&gt;powerpc-eabivle-gcc.exe: error: ewl_c9x.specs: No such file or directory&lt;BR /&gt;powerpc-eabivle-gcc.exe: error: ewl_c9x.specs: No such file or directory&lt;BR /&gt;powerpc-eabivle-gcc.exe: error: ewl_c9x.specs: No such file or directory&lt;BR /&gt;make: *** [src/subdir.mk:45: src/mode_entry.o] Error 1&lt;BR /&gt;make: *** [src/subdir.mk:45: src/main.o] Error 1&lt;BR /&gt;make: *** [src/subdir.mk:45: src/gpio.o] Error 1&lt;BR /&gt;make: *** [src/subdir.mk:45: src/intc_SW_mode_isr_vectors_MPC5744P.o] Error 1&lt;BR /&gt;make: *** [src/subdir.mk:52: src/intc_sw_handlers.o] Error 1&lt;BR /&gt;make: *** [Project_Settings/Startup_Code/subdir.mk:17: Project_Settings/Startup_Code/startup.o] Error 1&lt;/P&gt;&lt;P&gt;23:14:03 Build Finished (took 207ms)&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jun 2024 15:25:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/When-debugging-the-quot-LINFlexD-UART-MPC5744P-quot-example/m-p/1894538#M12464</guid>
      <dc:creator>xingzhenlei</dc:creator>
      <dc:date>2024-06-26T15:25:57Z</dc:date>
    </item>
    <item>
      <title>Re: When debugging the "LINFlexD_UART_MPC5744P" example documentation, the following error</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/When-debugging-the-quot-LINFlexD-UART-MPC5744P-quot-example/m-p/1896430#M12477</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;check project setting for Path and Source locations.&lt;BR /&gt;But if you create new project from&amp;nbsp;LINFlexD_UART_MPC5744P demo, it is compiled normally in S32DS.&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Mon, 01 Jul 2024 06:47:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/When-debugging-the-quot-LINFlexD-UART-MPC5744P-quot-example/m-p/1896430#M12477</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-07-01T06:47:24Z</dc:date>
    </item>
  </channel>
</rss>