<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design Studio中的主题 Installing new SDK causes automation project migration</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Installing-new-SDK-causes-automation-project-migration/m-p/1891676#M12447</link>
    <description>&lt;P&gt;I have S32 DS 3.5 and S32K344 micro.&lt;/P&gt;&lt;P&gt;It was originally set with SDK/RTD V2.0.0&lt;/P&gt;&lt;P&gt;It became necessary to add SDK 4.0.0, so that one project would migrate to 4.0.0 and another project stays at 2.0.0&lt;/P&gt;&lt;P&gt;SDK 4.0.0 gets installed properly and both SDKs appear under project settings.&lt;/P&gt;&lt;P&gt;I was expecting that by attaching/detaching SDK I can control which SDK current project would use.&lt;/P&gt;&lt;P&gt;However those "attached/detached" check-boxes seems to have no effect.&lt;/P&gt;&lt;P&gt;Regardless of that all projects would use 4.0.0 and it is was not possible to keep one project with 2.0.0&lt;/P&gt;&lt;P&gt;Is there a way to avoid that?&lt;/P&gt;</description>
    <pubDate>Thu, 20 Jun 2024 21:14:04 GMT</pubDate>
    <dc:creator>sstelmak</dc:creator>
    <dc:date>2024-06-20T21:14:04Z</dc:date>
    <item>
      <title>Installing new SDK causes automation project migration</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Installing-new-SDK-causes-automation-project-migration/m-p/1891676#M12447</link>
      <description>&lt;P&gt;I have S32 DS 3.5 and S32K344 micro.&lt;/P&gt;&lt;P&gt;It was originally set with SDK/RTD V2.0.0&lt;/P&gt;&lt;P&gt;It became necessary to add SDK 4.0.0, so that one project would migrate to 4.0.0 and another project stays at 2.0.0&lt;/P&gt;&lt;P&gt;SDK 4.0.0 gets installed properly and both SDKs appear under project settings.&lt;/P&gt;&lt;P&gt;I was expecting that by attaching/detaching SDK I can control which SDK current project would use.&lt;/P&gt;&lt;P&gt;However those "attached/detached" check-boxes seems to have no effect.&lt;/P&gt;&lt;P&gt;Regardless of that all projects would use 4.0.0 and it is was not possible to keep one project with 2.0.0&lt;/P&gt;&lt;P&gt;Is there a way to avoid that?&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jun 2024 21:14:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Installing-new-SDK-causes-automation-project-migration/m-p/1891676#M12447</guid>
      <dc:creator>sstelmak</dc:creator>
      <dc:date>2024-06-20T21:14:04Z</dc:date>
    </item>
    <item>
      <title>Re: Installing new SDK causes automation project migration</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Installing-new-SDK-causes-automation-project-migration/m-p/1891887#M12449</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/233204"&gt;@sstelmak&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;S32DS 3.5 can keep one RTD version only (plus additional extensions packages/stacks).&lt;/P&gt;
&lt;P&gt;The solution is to install more S32DS instances. Just use different folder name of S32DS like:&lt;/P&gt;
&lt;P&gt;c:\NXP\S32DS.3.5_RTD_200\&lt;/P&gt;
&lt;P&gt;c:\NXP\S32DS.3.5_RTD_400\&lt;/P&gt;
&lt;P&gt;And install corresponding RTD package to those instances.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Fri, 21 Jun 2024 06:07:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Installing-new-SDK-causes-automation-project-migration/m-p/1891887#M12449</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2024-06-21T06:07:55Z</dc:date>
    </item>
    <item>
      <title>Re: Installing new SDK causes automation project migration</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Installing-new-SDK-causes-automation-project-migration/m-p/1892974#M12457</link>
      <description>&lt;P&gt;That works, thank you&lt;/P&gt;</description>
      <pubDate>Mon, 24 Jun 2024 15:16:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Installing-new-SDK-causes-automation-project-migration/m-p/1892974#M12457</guid>
      <dc:creator>sstelmak</dc:creator>
      <dc:date>2024-06-24T15:16:32Z</dc:date>
    </item>
  </channel>
</rss>