<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: runtime error at 216 at 0328A5D6 is issue in software or hardware?? in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/runtime-error-at-216-at-0328A5D6-is-issue-in-software-or/m-p/1868466#M12299</link>
    <description>&lt;P&gt;unfortunately we used s32 118k custom board. do u say another comments?&lt;/P&gt;</description>
    <pubDate>Sun, 19 May 2024 23:15:32 GMT</pubDate>
    <dc:creator>seokhyeonwang</dc:creator>
    <dc:date>2024-05-19T23:15:32Z</dc:date>
    <item>
      <title>runtime error at 216 at 0328A5D6 is issue in software or hardware??</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/runtime-error-at-216-at-0328A5D6-is-issue-in-software-or/m-p/1614023#M9871</link>
      <description>&lt;P&gt;When I am flashing program in microcontroller using PE micro debugger we get the following error i.e.runtime error at 216 and GDB is terminated so we can't flash the program in controller.Please solve the issue&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="sheetalk_0-1678706599457.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/214290iBF080A23B1AA6FC9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="sheetalk_0-1678706599457.png" alt="sheetalk_0-1678706599457.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 13 Mar 2023 11:24:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/runtime-error-at-216-at-0328A5D6-is-issue-in-software-or/m-p/1614023#M9871</guid>
      <dc:creator>sheetalk</dc:creator>
      <dc:date>2023-03-13T11:24:34Z</dc:date>
    </item>
    <item>
      <title>Re: runtime error at 216 at 0328A5D6 is issue in software or hardware??</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/runtime-error-at-216-at-0328A5D6-is-issue-in-software-or/m-p/1614173#M9873</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/212603"&gt;@sheetalk&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Which NXP EVB are you using? Is it the&amp;nbsp;&lt;A class="dtmcustomrulelink" href="https://www.nxp.com/part/S32K142EVB-Q100" data-dtmaction="Buy Options - Section Click" data-dtmsubaction="S32K142EVB-Q100" target="_blank"&gt;S32K142EVB-Q100&lt;/A&gt;? If so, this device is 100-pin package. From the image you attached, it appears you are trying to program with a project for the 64-pin package device.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Mon, 13 Mar 2023 15:03:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/runtime-error-at-216-at-0328A5D6-is-issue-in-software-or/m-p/1614173#M9873</guid>
      <dc:creator>mikedoidge</dc:creator>
      <dc:date>2023-03-13T15:03:03Z</dc:date>
    </item>
    <item>
      <title>Re: runtime error at 216 at 0328A5D6 is issue in software or hardware??</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/runtime-error-at-216-at-0328A5D6-is-issue-in-software-or/m-p/1860869#M12256</link>
      <description>&lt;P&gt;i also have same problem i use flash driver setting process flash init -&amp;gt; erase -&amp;gt; programming -&amp;gt; read process that access after dont work flash debugging another board can do.&lt;BR /&gt;another board can use. i want to enforce flash reset and setting it will be fine. but i also, custom board, so i dont find how to reset this flash. flash tool dosen`t match com port i want to help too.&lt;/P&gt;</description>
      <pubDate>Tue, 07 May 2024 23:27:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/runtime-error-at-216-at-0328A5D6-is-issue-in-software-or/m-p/1860869#M12256</guid>
      <dc:creator>seokhyeonwang</dc:creator>
      <dc:date>2024-05-07T23:27:01Z</dc:date>
    </item>
    <item>
      <title>Re: runtime error at 216 at 0328A5D6 is issue in software or hardware??</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/runtime-error-at-216-at-0328A5D6-is-issue-in-software-or/m-p/1868466#M12299</link>
      <description>&lt;P&gt;unfortunately we used s32 118k custom board. do u say another comments?&lt;/P&gt;</description>
      <pubDate>Sun, 19 May 2024 23:15:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/runtime-error-at-216-at-0328A5D6-is-issue-in-software-or/m-p/1868466#M12299</guid>
      <dc:creator>seokhyeonwang</dc:creator>
      <dc:date>2024-05-19T23:15:32Z</dc:date>
    </item>
  </channel>
</rss>