<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design Studio中的主题 Re: How the project is configured when referencing the lib library</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/How-the-project-is-configured-when-referencing-the-lib-library/m-p/1848575#M12158</link>
    <description>Hello, I follow the normal methods of generating and adding static libraries. When I added static libraries, the following error appeared. May I ask what caused it?&lt;BR /&gt;&lt;BR /&gt;Building target: BMS_2_2.elf&lt;BR /&gt;Invoking: Standard S32DS C Linker&lt;BR /&gt;arm-none-eabi-gcc -o "BMS_2_2.elf" "@BMS_2_2.args"&lt;BR /&gt;arm-none-eabi-gcc.exe: error: : No such file or directory&lt;BR /&gt;make: *** [makefile:86: BMS_2_2.elf] Error 1&lt;BR /&gt;"make -j16 all" terminated with exit code 2. Build might be incomplete.</description>
    <pubDate>Wed, 17 Apr 2024 01:35:01 GMT</pubDate>
    <dc:creator>NXP2</dc:creator>
    <dc:date>2024-04-17T01:35:01Z</dc:date>
    <item>
      <title>How the project is configured when referencing the lib library</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/How-the-project-is-configured-when-referencing-the-lib-library/m-p/1504420#M8935</link>
      <description>&lt;P&gt;We are using the chip of S32K314 for development.&lt;/P&gt;&lt;P&gt;When we need to reference the lib library, we don't know how to configure the name of the library in the following configuration to ensure that the compilation passes (C/C++ Build→Settings→Libraries).&lt;/P&gt;&lt;P&gt;For example, the name of the library is libe2e.a, and we cannot configure it as "e2e" or "libe2e".&lt;/P&gt;&lt;P&gt;Please help confirm how this part should be configured, thank you.&lt;/P&gt;</description>
      <pubDate>Thu, 11 Aug 2022 02:36:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/How-the-project-is-configured-when-referencing-the-lib-library/m-p/1504420#M8935</guid>
      <dc:creator>LiuJie_Joynext</dc:creator>
      <dc:date>2022-08-11T02:36:27Z</dc:date>
    </item>
    <item>
      <title>Re: How the project is configured when referencing the lib library</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/How-the-project-is-configured-when-referencing-the-lib-library/m-p/1505664#M8936</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/204746"&gt;@LiuJie_Joynext&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;We have an article which you may find useful for this topic:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Add-a-static-library-file-into-S32DS-GCC-project/ta-p/1110308" target="_self"&gt; HOWTO: Add a static library file into S32DS GCC project&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope it helps,&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Fri, 12 Aug 2022 15:21:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/How-the-project-is-configured-when-referencing-the-lib-library/m-p/1505664#M8936</guid>
      <dc:creator>mikedoidge</dc:creator>
      <dc:date>2022-08-12T15:21:32Z</dc:date>
    </item>
    <item>
      <title>Re: How the project is configured when referencing the lib library</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/How-the-project-is-configured-when-referencing-the-lib-library/m-p/1848575#M12158</link>
      <description>Hello, I follow the normal methods of generating and adding static libraries. When I added static libraries, the following error appeared. May I ask what caused it?&lt;BR /&gt;&lt;BR /&gt;Building target: BMS_2_2.elf&lt;BR /&gt;Invoking: Standard S32DS C Linker&lt;BR /&gt;arm-none-eabi-gcc -o "BMS_2_2.elf" "@BMS_2_2.args"&lt;BR /&gt;arm-none-eabi-gcc.exe: error: : No such file or directory&lt;BR /&gt;make: *** [makefile:86: BMS_2_2.elf] Error 1&lt;BR /&gt;"make -j16 all" terminated with exit code 2. Build might be incomplete.</description>
      <pubDate>Wed, 17 Apr 2024 01:35:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/How-the-project-is-configured-when-referencing-the-lib-library/m-p/1848575#M12158</guid>
      <dc:creator>NXP2</dc:creator>
      <dc:date>2024-04-17T01:35:01Z</dc:date>
    </item>
  </channel>
</rss>