<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design Studio中的主题 RTC example code</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/RTC-example-code/m-p/1842963#M12132</link>
    <description>&lt;LI-SPOILER&gt;&amp;nbsp;&lt;/LI-SPOILER&gt;&lt;P&gt;Hi, I am trying S32K312&amp;nbsp; microcontroller with external RTC (DS1307) through I2C communication. Is there any examples related to it?&lt;/P&gt;</description>
    <pubDate>Tue, 09 Apr 2024 07:10:13 GMT</pubDate>
    <dc:creator>JIBIN_7</dc:creator>
    <dc:date>2024-04-09T07:10:13Z</dc:date>
    <item>
      <title>RTC example code</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/RTC-example-code/m-p/1842963#M12132</link>
      <description>&lt;LI-SPOILER&gt;&amp;nbsp;&lt;/LI-SPOILER&gt;&lt;P&gt;Hi, I am trying S32K312&amp;nbsp; microcontroller with external RTC (DS1307) through I2C communication. Is there any examples related to it?&lt;/P&gt;</description>
      <pubDate>Tue, 09 Apr 2024 07:10:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/RTC-example-code/m-p/1842963#M12132</guid>
      <dc:creator>JIBIN_7</dc:creator>
      <dc:date>2024-04-09T07:10:13Z</dc:date>
    </item>
    <item>
      <title>Re: RTC example code</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/RTC-example-code/m-p/1847790#M12153</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;I saw from your previous &lt;A href="https://community.nxp.com/t5/S32-SDK/Issue-with-I2C-Code-in-S32K312/td-p/1831703" target="_self"&gt;question&lt;/A&gt; that you were referring to &lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-I2C-Transmit-amp-Receive-Using-DMA-DS3-5-RTD300/ta-p/1801357" target="_self"&gt;Example S32K312 I2C Transmit &amp;amp; Receive Using DMA DS3.5 RTD300&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;DS1307 is not an NXP product, so there is no project for this device. 0x68 is the I2C address for DS1307. Did you change the &lt;STRONG&gt;Slave address&lt;/STRONG&gt; in &lt;EM&gt;S32 Configuration Tool&lt;/EM&gt;?&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="DS1307 0x68 S32K312_I2C_LPI2C_DMA_working.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/273941iDA1AE47BAAD55227/image-size/large?v=v2&amp;amp;px=999" role="button" title="DS1307 0x68 S32K312_I2C_LPI2C_DMA_working.png" alt="DS1307 0x68 S32K312_I2C_LPI2C_DMA_working.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 16 Apr 2024 06:49:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/RTC-example-code/m-p/1847790#M12153</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-04-16T06:49:56Z</dc:date>
    </item>
    <item>
      <title>Re: RTC example code</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/RTC-example-code/m-p/1856712#M12221</link>
      <description>&lt;P&gt;I updated the slave address to 0x68 and tested the same, it is not working. Can you please suggest?&lt;/P&gt;</description>
      <pubDate>Mon, 29 Apr 2024 11:17:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/RTC-example-code/m-p/1856712#M12221</guid>
      <dc:creator>Mithulesh23</dc:creator>
      <dc:date>2024-04-29T11:17:55Z</dc:date>
    </item>
    <item>
      <title>Re: RTC example code</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/RTC-example-code/m-p/1857193#M12225</link>
      <description>&lt;P&gt;Please don't just tell me this doesn't work, I need more information in order to help you faster.&lt;BR /&gt;For example, sending the I2C waveform captured by the logic analyzer allows us to check whether S32K3 sends the correct slave address.&lt;/P&gt;</description>
      <pubDate>Tue, 30 Apr 2024 04:46:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/RTC-example-code/m-p/1857193#M12225</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-04-30T04:46:57Z</dc:date>
    </item>
  </channel>
</rss>