<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックI2C-AsyncTransmit with DMA has some problems.</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/I2C-AsyncTransmit-with-DMA-has-some-problems/m-p/1819331#M11951</link>
    <description>&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;DMA is used for asynchronous transfers, after which the state remains in the sent state.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt; According to the observation of the logic analyzer, there has been data transmission on the SDA line.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt; I would like to ask if there is any relevant examples&amp;nbsp; can refer to.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt; I'm using version 4.3.1 of MCAL,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 01 Mar 2024 07:23:55 GMT</pubDate>
    <dc:creator>xc1234</dc:creator>
    <dc:date>2024-03-01T07:23:55Z</dc:date>
    <item>
      <title>I2C-AsyncTransmit with DMA has some problems.</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/I2C-AsyncTransmit-with-DMA-has-some-problems/m-p/1819331#M11951</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;DMA is used for asynchronous transfers, after which the state remains in the sent state.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt; According to the observation of the logic analyzer, there has been data transmission on the SDA line.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt; I would like to ask if there is any relevant examples&amp;nbsp; can refer to.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt; I'm using version 4.3.1 of MCAL,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 01 Mar 2024 07:23:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/I2C-AsyncTransmit-with-DMA-has-some-problems/m-p/1819331#M11951</guid>
      <dc:creator>xc1234</dc:creator>
      <dc:date>2024-03-01T07:23:55Z</dc:date>
    </item>
  </channel>
</rss>