<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32DS Missing platform/devices folder after generating code in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Missing-platform-devices-folder-after-generating-code/m-p/1802745#M11829</link>
    <description>&lt;P&gt;Hi Aitor,&lt;/P&gt;&lt;P&gt;In the end I gave up on creating a new blank project and directly created a project from example (hello_world) and started from there using SDK Configuration Tool.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Laura.&lt;/P&gt;</description>
    <pubDate>Tue, 06 Feb 2024 14:39:25 GMT</pubDate>
    <dc:creator>l_sanz</dc:creator>
    <dc:date>2024-02-06T14:39:25Z</dc:date>
    <item>
      <title>S32DS Missing platform/devices folder after generating code</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Missing-platform-devices-folder-after-generating-code/m-p/1573231#M9566</link>
      <description>&lt;P&gt;Hello everybody,&lt;/P&gt;&lt;P&gt;I'm creating a new S32DS application project and I'm having some issues with the base project.&lt;/P&gt;&lt;P&gt;Note that I have installed the correct Device pack and the 4.0.3 SDK beforehand.&lt;/P&gt;&lt;P&gt;First of all I create a new project and check that it compiles. Then I create a new board configuration with the code generator tool and configure the UART pins and peripheral. I click on Update Code button and generate the new code.&lt;/P&gt;&lt;P&gt;When I compile the new code it throws an error about missing header files (status.h)&lt;/P&gt;&lt;P&gt;I have checked other example projects and I have seen that they include a folder named "device" in &amp;lt;project_root&amp;gt;/SDK/platform/ that is not found in my project. I only have the "drivers" folder inside /platform/&lt;/P&gt;&lt;P&gt;Any idea why my project configurator is not adding these files to my project?&lt;/P&gt;&lt;P&gt;Thank you in advance!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 21 Dec 2022 16:37:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Missing-platform-devices-folder-after-generating-code/m-p/1573231#M9566</guid>
      <dc:creator>l_sanz</dc:creator>
      <dc:date>2022-12-21T16:37:54Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS Missing platform/devices folder after generating code</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Missing-platform-devices-folder-after-generating-code/m-p/1573250#M9569</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210329"&gt;@l_sanz&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Can you tell us the MCU that you are using?&lt;/P&gt;</description>
      <pubDate>Wed, 21 Dec 2022 17:29:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Missing-platform-devices-folder-after-generating-code/m-p/1573250#M9569</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2022-12-21T17:29:26Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS Missing platform/devices folder after generating code</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Missing-platform-devices-folder-after-generating-code/m-p/1573303#M9570</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210329"&gt;@l_sanz&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Since I don't know which device you are working with, I can't be more specific. However, I believe you are missing some step which sets up the device data in the S32 Configuraton Tools. Most likely this is not happening so the 'device' folder is not created when you perform 'Update Code'. Please review one of the following HOWTO articles to see if you can identify what step you missed. They are all very similar, so please select the one which matches or is closest to the device you are using for the most relevant details. Each one walks through the steps to create a new application project and use the SDK to blink an LED on the EVB.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-a-Blinking-LED-example-project-using-S32K1xx-RTD/ta-p/1471695" target="_self"&gt;HOWTO: Create a Blinking LED example project using S32K1xx RTD with AUTOSAR&lt;/A&gt;&lt;SPAN&gt;&lt;STRONG&gt;&amp;nbsp;&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-a-Blinking-LED-example-project-using-S32K1xx-RTD/ta-p/1471810" target="_self"&gt;HOWTO: Create a Blinking LED example project using S32K1xx RTD without AUTOSAR&lt;/A&gt;&lt;SPAN&gt;&lt;STRONG&gt;&amp;nbsp;&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-a-Blinking-LED-application-project-for-S32G-using/ta-p/1562381" target="_self"&gt;HOWTO: Create a Blinking LED application project for S32G using S32 RTD No AUTOSAR&lt;/A&gt;&lt;SPAN&gt;&lt;STRONG&gt;&amp;nbsp;&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-a-Blinking-LED-application-project-for-S32G-using/ta-p/1563066" target="_self"&gt;HOWTO: Create a Blinking LED application project for S32G using S32 RTD with AUTOSAR&lt;/A&gt;&lt;SPAN&gt;&lt;STRONG&gt;&amp;nbsp;&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-a-Blinking-LED-application-project-for-S32R45-using/ta-p/1563699" target="_self"&gt;HOWTO: Create a Blinking LED application project for S32R45 using S32 RTD No AUTOSAR&lt;/A&gt;&lt;SPAN&gt;&lt;STRONG&gt;&amp;nbsp;&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-a-Blinking-LED-application-project-for-S32R45-using/ta-p/1563798" target="_self"&gt;HOWTO: Create a Blinking LED application project for S32R45 using S32 RTD with AUTOSAR&lt;/A&gt;&lt;SPAN&gt;&lt;STRONG&gt;&amp;nbsp;&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-a-Blinking-LED-application-project-for-S32R41-using/ta-p/1564626" target="_self"&gt;HOWTO: Create a Blinking LED application project for S32R41 using S32 RTD No AUTOSAR&lt;/A&gt;&lt;SPAN&gt;&lt;STRONG&gt;&amp;nbsp;&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-a-Blinking-LED-application-project-for-S32R41-using/ta-p/1564758" target="_self"&gt;HOWTO: Create a Blinking LED application project for S32R41 using S32 RTD AUTOSAR&lt;/A&gt;&lt;SPAN&gt;&lt;STRONG&gt;&amp;nbsp;&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Wed, 21 Dec 2022 20:04:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Missing-platform-devices-folder-after-generating-code/m-p/1573303#M9570</guid>
      <dc:creator>mikedoidge</dc:creator>
      <dc:date>2022-12-21T20:04:54Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS Missing platform/devices folder after generating code</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Missing-platform-devices-folder-after-generating-code/m-p/1573647#M9571</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201913"&gt;@VaneB&lt;/a&gt;&amp;nbsp;and&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/83694"&gt;@mikedoidge&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using a S32K118 MCU for development. I have installed everything related to my MCU. There was no option to install&amp;nbsp;&lt;SPAN&gt;S32K1 RTD AUTOSAR 4.4.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Captura.JPG" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/205232i6800DF19A0F738E8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Captura.JPG" alt="Captura.JPG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Captura.JPG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;When creating the project if I select the the GCC9.2 then in the SDK selection menu I don't have&amp;nbsp;&lt;SPAN&gt;PlatformSDK_S32K1_2022_02_S32K118_M4F like specified in step 7.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Everything else I do like the tutorial says. Could it be that I need to download and install something more?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for the help!&lt;/P&gt;</description>
      <pubDate>Thu, 22 Dec 2022 09:34:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Missing-platform-devices-folder-after-generating-code/m-p/1573647#M9571</guid>
      <dc:creator>l_sanz</dc:creator>
      <dc:date>2022-12-22T09:34:01Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS Missing platform/devices folder after generating code</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Missing-platform-devices-folder-after-generating-code/m-p/1574957#M9576</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210329"&gt;@l_sanz&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Which version of S32DS are you using? &lt;BR /&gt;Regarding the S32K1 RTD AUTOSAR 4.4. you can download it from this link:&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K1-RTD44-D" target="_blank" rel="noopener"&gt;Real-Time Drivers for S32K1&lt;/A&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 27 Dec 2022 15:48:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Missing-platform-devices-folder-after-generating-code/m-p/1574957#M9576</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2022-12-27T15:48:15Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS Missing platform/devices folder after generating code</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Missing-platform-devices-folder-after-generating-code/m-p/1802742#M11828</link>
      <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;I have found the same issue, I am working with the family S32K1 (S32K144). I have just downloaded&lt;STRONG&gt;&amp;nbsp;S32 Design Studio for S32 Platform&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Version: 3.5.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I follow the link:&amp;nbsp;HOWTO: Create a Blinking LED example project using S32K1xx RTD without AUTOSAR&amp;nbsp;and I can see that I have all the necesary firmware installed for the correct working of the IDE.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;S32K1 RTD AUTOSAR 4.4&lt;/STRONG&gt;&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;S32K1xxx development packages&lt;/STRONG&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;when I take an&lt;STRONG&gt; example from the SDK&lt;/STRONG&gt; (this project is correctly generated and takes into account the folder &lt;STRONG&gt;platform/devices&lt;/STRONG&gt;) and worked as expected when I built it. But when I create a &lt;STRONG&gt;new project (S32DS Application Project)&lt;/STRONG&gt;, I can't attach the SDK in the configuration of the proyect and the final result when I finish the process is that the project doesn't have this folder generated.&lt;/P&gt;&lt;P&gt;Any idea that what could be happening in my IDE?.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Aitor&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Feb 2024 14:33:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Missing-platform-devices-folder-after-generating-code/m-p/1802742#M11828</guid>
      <dc:creator>aurrutia</dc:creator>
      <dc:date>2024-02-06T14:33:19Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS Missing platform/devices folder after generating code</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Missing-platform-devices-folder-after-generating-code/m-p/1802745#M11829</link>
      <description>&lt;P&gt;Hi Aitor,&lt;/P&gt;&lt;P&gt;In the end I gave up on creating a new blank project and directly created a project from example (hello_world) and started from there using SDK Configuration Tool.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Laura.&lt;/P&gt;</description>
      <pubDate>Tue, 06 Feb 2024 14:39:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Missing-platform-devices-folder-after-generating-code/m-p/1802745#M11829</guid>
      <dc:creator>l_sanz</dc:creator>
      <dc:date>2024-02-06T14:39:25Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS Missing platform/devices folder after generating code</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Missing-platform-devices-folder-after-generating-code/m-p/1802748#M11830</link>
      <description>&lt;P&gt;Hi Laura,&lt;/P&gt;&lt;P&gt;I think that I have the response for our problems. In my case the SDK 4.0 RTM for my microcontroler needed the gcc 6.3 for the correct generation of the code. So in the rest of the cases gcc 9.x AND 10.X doesn't work in my case.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Aitor&lt;/P&gt;</description>
      <pubDate>Tue, 06 Feb 2024 14:50:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Missing-platform-devices-folder-after-generating-code/m-p/1802748#M11830</guid>
      <dc:creator>aurrutia</dc:creator>
      <dc:date>2024-02-06T14:50:13Z</dc:date>
    </item>
  </channel>
</rss>