<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: Update Potentiometer value in run time</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Update-Potentiometer-value-in-run-time/m-p/1798572#M11799</link>
    <description>&lt;P&gt;I am new to nxp s32k144 . I have successfully tested the read and write functions but now i want to use ADC module and write code for reading the value from potentiometer and then displaying it on semihosting console .&amp;nbsp;&lt;BR /&gt;If possible please provide me the code and also give me step by step instructions to run that code and view the output&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 31 Jan 2024 09:53:57 GMT</pubDate>
    <dc:creator>chandanmohanty</dc:creator>
    <dc:date>2024-01-31T09:53:57Z</dc:date>
    <item>
      <title>Update Potentiometer value in run time</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Update-Potentiometer-value-in-run-time/m-p/1019779#M5945</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using S32K144 evaluation board and trying to use the potentiometer (ADC0_SE12)to change the light intensity of LED.My problem is how I can update the potentiometer value in run time and see an immediate change of the light intensity?&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD width="200"&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Dec 2019 00:04:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Update-Potentiometer-value-in-run-time/m-p/1019779#M5945</guid>
      <dc:creator>huda_abdalla</dc:creator>
      <dc:date>2019-12-09T00:04:52Z</dc:date>
    </item>
    <item>
      <title>Re: Update Potentiometer value in run time</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Update-Potentiometer-value-in-run-time/m-p/1019780#M5946</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;unfortunately this feature is not supported by S32DS. In runtime you can only see values in PE Micro Real Time Expressions:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/95999iF12995CDDA7FA714/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can use FreeMaster for that. There is an example in S32DS:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/96000i5E315D3906B9AC46/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Dec 2019 08:13:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Update-Potentiometer-value-in-run-time/m-p/1019780#M5946</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2019-12-09T08:13:19Z</dc:date>
    </item>
    <item>
      <title>Re: Update Potentiometer value in run time</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Update-Potentiometer-value-in-run-time/m-p/1019781#M5947</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for fast reply,Unfortunately "ftm_pwm_s32k144" is not useful ,since I'm not using SDK. Actually I want to acquire the potentiometer value to ADC and generate PWM to change the RGB light intensity?...I used&amp;nbsp;&lt;/P&gt;&lt;P&gt;PE Micro Real Time Expressions,if I changed the potentiometer and I have to run the code every time so that I can see the value changing also the intensity..What I need is to see the intensity changing with potentiometer changing without the need to run the code each time !!&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope it is clear&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Dec 2019 10:59:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Update-Potentiometer-value-in-run-time/m-p/1019781#M5947</guid>
      <dc:creator>huda_abdalla</dc:creator>
      <dc:date>2019-12-09T10:59:49Z</dc:date>
    </item>
    <item>
      <title>Re: Update Potentiometer value in run time</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Update-Potentiometer-value-in-run-time/m-p/1019782#M5948</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sorry, I don't get it. If I understand it correctly - you like to simulate potentiometer output voltage by Debugger in real time, Am I correct?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PE Micro allows only reading values in real time. Value can't be written in real time (you need to stop program, change value, and run it again).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Dec 2019 12:45:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Update-Potentiometer-value-in-run-time/m-p/1019782#M5948</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2019-12-09T12:45:20Z</dc:date>
    </item>
    <item>
      <title>Re: Update Potentiometer value in run time</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Update-Potentiometer-value-in-run-time/m-p/1019783#M5949</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;yes that's right,I get it now ....I have another question :I would like to update the pwm compare register from the ADC0&amp;nbsp; to control the the duty cycle of the pwm using the adc,,I'm using FTM0_ch0 for the pwm output&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Dec 2019 20:57:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Update-Potentiometer-value-in-run-time/m-p/1019783#M5949</guid>
      <dc:creator>huda_abdalla</dc:creator>
      <dc:date>2019-12-09T20:57:21Z</dc:date>
    </item>
    <item>
      <title>Re: Update Potentiometer value in run time</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Update-Potentiometer-value-in-run-time/m-p/1798572#M11799</link>
      <description>&lt;P&gt;I am new to nxp s32k144 . I have successfully tested the read and write functions but now i want to use ADC module and write code for reading the value from potentiometer and then displaying it on semihosting console .&amp;nbsp;&lt;BR /&gt;If possible please provide me the code and also give me step by step instructions to run that code and view the output&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 31 Jan 2024 09:53:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Update-Potentiometer-value-in-run-time/m-p/1798572#M11799</guid>
      <dc:creator>chandanmohanty</dc:creator>
      <dc:date>2024-01-31T09:53:57Z</dc:date>
    </item>
  </channel>
</rss>