<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Gtest Running Issue in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Gtest-Running-Issue/m-p/1797440#M11792</link>
    <description>&lt;P&gt;Thanks for the solution but I tried same but still its not working.&lt;/P&gt;&lt;P&gt;Can yo please suggest any solution to run gtest in S32Ds.3.5 for c code.&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Rajshri&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 30 Jan 2024 06:19:57 GMT</pubDate>
    <dc:creator>Rajshri</dc:creator>
    <dc:date>2024-01-30T06:19:57Z</dc:date>
    <item>
      <title>Gtest Running Issue</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Gtest-Running-Issue/m-p/1795135#M11773</link>
      <description>&lt;P&gt;I tried running gtest on S32 Design Studio with S32DS application project with processor "CPU_S32K144HFT0VLLT" but when I add "lgtest_main" it is throwing an error "libgtest_main.a file format is not recognised".&lt;/P&gt;&lt;P&gt;Please provide solution on this or suggest any other to run gtest on S32DS.&lt;/P&gt;</description>
      <pubDate>Thu, 25 Jan 2024 06:22:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Gtest-Running-Issue/m-p/1795135#M11773</guid>
      <dc:creator>Rajshri</dc:creator>
      <dc:date>2024-01-25T06:22:22Z</dc:date>
    </item>
    <item>
      <title>Re: Gtest Running Issue</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Gtest-Running-Issue/m-p/1795650#M11780</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/228657"&gt;@Rajshri&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;It seems this is a problem linked with the static library (.a extension). Here is a community post explaining how to add a static library:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Add-a-static-library-file-into-S32DS-GCC-project/ta-p/1110308" target="_blank"&gt;HOWTO: Add a static library file into S32DS GCC pr... - NXP Community&lt;/A&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&lt;SPAN&gt;Please, try to perform the suggested procedure from above. If you are not able to get the project working let us know to provide further support.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Julián.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 25 Jan 2024 21:18:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Gtest-Running-Issue/m-p/1795650#M11780</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-01-25T21:18:06Z</dc:date>
    </item>
    <item>
      <title>Re: Gtest Running Issue</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Gtest-Running-Issue/m-p/1797440#M11792</link>
      <description>&lt;P&gt;Thanks for the solution but I tried same but still its not working.&lt;/P&gt;&lt;P&gt;Can yo please suggest any solution to run gtest in S32Ds.3.5 for c code.&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Rajshri&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 30 Jan 2024 06:19:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Gtest-Running-Issue/m-p/1797440#M11792</guid>
      <dc:creator>Rajshri</dc:creator>
      <dc:date>2024-01-30T06:19:57Z</dc:date>
    </item>
    <item>
      <title>Re: Gtest Running Issue</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Gtest-Running-Issue/m-p/1798021#M11795</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/228657"&gt;@Rajshri&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Is DS displaying the same error?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 30 Jan 2024 20:21:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Gtest-Running-Issue/m-p/1798021#M11795</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-01-30T20:21:30Z</dc:date>
    </item>
    <item>
      <title>Re: Gtest Running Issue</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Gtest-Running-Issue/m-p/1798270#M11797</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200831"&gt;@Julián_AragónM&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Yes, It is displaying same error.&lt;/P&gt;&lt;P&gt;Can you please provide me steps to integrate gtest with S32DS for C Code ?&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Rajshri&lt;/P&gt;</description>
      <pubDate>Wed, 31 Jan 2024 05:15:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Gtest-Running-Issue/m-p/1798270#M11797</guid>
      <dc:creator>Rajshri</dc:creator>
      <dc:date>2024-01-31T05:15:34Z</dc:date>
    </item>
    <item>
      <title>Re: Gtest Running Issue</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Gtest-Running-Issue/m-p/1799071#M11805</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/228657"&gt;@Rajshri&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;This seems to be an importing problem.&lt;/P&gt;
&lt;P&gt;I would recommend to instead create an application project from this community post:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-S32-Design-Studio-Create-a-New-Application-Project/ta-p/1126018" target="_self"&gt;HOWTO: S32 Design Studio - Create a New Application Project&lt;/A&gt;, and a&lt;SPAN&gt;dd your content to this base project, adding the static library from the previous example I shared and trying to compile it.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Custom implementation should come from customer's side, as it is out of this community's scope of help. I apologize for any inconveniences this may cause.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Julián&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 31 Jan 2024 21:35:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Gtest-Running-Issue/m-p/1799071#M11805</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-01-31T21:35:28Z</dc:date>
    </item>
  </channel>
</rss>