<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K3 Linux development with gcc without S32DS in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32K3-Linux-development-with-gcc-without-S32DS/m-p/1791431#M11747</link>
    <description>&lt;P&gt;Is the version of gcc used with S32 Design Studio 3.5 the same as the ARM GNU toolchain from github, or are there NXP specific patches applied to it?&lt;/P&gt;&lt;P&gt;Are the RTDs still not supported when building with Linux? It looks like the only issue is a case sensitivity mismatch between the include files and the actual filenames.&amp;nbsp;&lt;/P&gt;&lt;P&gt;We would like to only use S32DS for the configurator.&lt;BR /&gt;All builds would be done from the Linux command line as part of our CI/CD process.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 19 Jan 2024 00:39:37 GMT</pubDate>
    <dc:creator>hns80</dc:creator>
    <dc:date>2024-01-19T00:39:37Z</dc:date>
    <item>
      <title>S32K3 Linux development with gcc without S32DS</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32K3-Linux-development-with-gcc-without-S32DS/m-p/1791431#M11747</link>
      <description>&lt;P&gt;Is the version of gcc used with S32 Design Studio 3.5 the same as the ARM GNU toolchain from github, or are there NXP specific patches applied to it?&lt;/P&gt;&lt;P&gt;Are the RTDs still not supported when building with Linux? It looks like the only issue is a case sensitivity mismatch between the include files and the actual filenames.&amp;nbsp;&lt;/P&gt;&lt;P&gt;We would like to only use S32DS for the configurator.&lt;BR /&gt;All builds would be done from the Linux command line as part of our CI/CD process.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 19 Jan 2024 00:39:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32K3-Linux-development-with-gcc-without-S32DS/m-p/1791431#M11747</guid>
      <dc:creator>hns80</dc:creator>
      <dc:date>2024-01-19T00:39:37Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 Linux development with gcc without S32DS</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32K3-Linux-development-with-gcc-without-S32DS/m-p/1793774#M11762</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;the NXP gcc version is slightly different. You can download standalone version for Linux here -&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/sps/download/license.jsp?colCode=NXP_GCC10_2_eARMv7_b1728_g5963bc8-bin&amp;amp;appType=file1&amp;amp;DOWNLOAD_ID=null" target="_blank"&gt;https://www.nxp.com/webapp/sps/download/license.jsp?colCode=NXP_GCC10_2_eARMv7_b1728_g5963bc8-bin&amp;amp;appType=file1&amp;amp;DOWNLOAD_ID=null&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Unfortunately the RTD is still not supported on Linux platform. If the project is not very large, you can modify filenames manually.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 23 Jan 2024 11:27:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32K3-Linux-development-with-gcc-without-S32DS/m-p/1793774#M11762</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2024-01-23T11:27:47Z</dc:date>
    </item>
  </channel>
</rss>