<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I2C configuration in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/I2C-configuration/m-p/1790854#M11737</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/225259"&gt;@LavanyaR&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;only one master configuration structure can be used at a time. Let me copy here from the user manual:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lukaszadrapa_0-1705564695387.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/258753i19AD8973ABC1F63D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="lukaszadrapa_0-1705564695387.png" alt="lukaszadrapa_0-1705564695387.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;lukaszadrapa_0-1705564695387.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;So, there are two options if more slave devices with different settings are used - either deinit and init the driver each time when you need to switch the configuration or set the baud rate and address in runtime as mentioned in the manual.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you have the slave devices connected to different pins, it will be even more complicated - you need to change also GPIO configuration. So, deinit and init makes more sense here.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 18 Jan 2024 08:02:37 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2024-01-18T08:02:37Z</dc:date>
    <item>
      <title>I2C configuration</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/I2C-configuration/m-p/1790009#M11722</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In our project I2C1 (PTD9 &amp;amp; PTD6) used for EEPROM communication. I2C1 (PTC6 &amp;amp;PTC7) used for RTC&amp;nbsp;communication. Is it possible to configure the same instance twice in single master?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jan 2024 06:19:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/I2C-configuration/m-p/1790009#M11722</guid>
      <dc:creator>LavanyaR</dc:creator>
      <dc:date>2024-01-17T06:19:10Z</dc:date>
    </item>
    <item>
      <title>Re: I2C configuration</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/I2C-configuration/m-p/1790854#M11737</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/225259"&gt;@LavanyaR&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;only one master configuration structure can be used at a time. Let me copy here from the user manual:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lukaszadrapa_0-1705564695387.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/258753i19AD8973ABC1F63D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="lukaszadrapa_0-1705564695387.png" alt="lukaszadrapa_0-1705564695387.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;lukaszadrapa_0-1705564695387.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;So, there are two options if more slave devices with different settings are used - either deinit and init the driver each time when you need to switch the configuration or set the baud rate and address in runtime as mentioned in the manual.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you have the slave devices connected to different pins, it will be even more complicated - you need to change also GPIO configuration. So, deinit and init makes more sense here.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Jan 2024 08:02:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/I2C-configuration/m-p/1790854#M11737</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2024-01-18T08:02:37Z</dc:date>
    </item>
  </channel>
</rss>