<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: Driver configuration for S32K322</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Driver-configuration-for-S32K322/m-p/1786566#M11688</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/225259"&gt;@LavanyaR&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1. In the Linker file, ensure that the size of ITCM and DTCM are as shown in the following code. Also, the Linker file is already provided when you create a new application project with the desired MCU.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;LI-CODE lang="c"&gt;int_itcm                : ORIGIN = 0x00000000, LENGTH = 0x00008000    /* 32K */
int_dtcm                : ORIGIN = 0x20000000, LENGTH = 0x00010000    /* 64K */&lt;/LI-CODE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;2. For S32K322 the most viable option is to generate a new project with the corresponding MCU and then copy the application source files from your pre-existing project as well as any customizations you made to the project properties.&lt;/P&gt;</description>
    <pubDate>Wed, 10 Jan 2024 22:18:15 GMT</pubDate>
    <dc:creator>VaneB</dc:creator>
    <dc:date>2024-01-10T22:18:15Z</dc:date>
    <item>
      <title>Driver configuration for S32K322</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Driver-configuration-for-S32K322/m-p/1784438#M11664</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Shall we use s32k344 example driver code for s32k322 microcontroller? or Do you have driver code for s32k322 microcontroller?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks in advance&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 08 Jan 2024 12:22:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Driver-configuration-for-S32K322/m-p/1784438#M11664</guid>
      <dc:creator>LavanyaR</dc:creator>
      <dc:date>2024-01-08T12:22:44Z</dc:date>
    </item>
    <item>
      <title>Re: Driver configuration for S32K322</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Driver-configuration-for-S32K322/m-p/1784583#M11670</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;can please share more info? Which particular driver are you looking for? Or you men all Real Time Drivers set for S32K322? Assuming that your S32DS version is v3.5.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 08 Jan 2024 18:11:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Driver-configuration-for-S32K322/m-p/1784583#M11670</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2024-01-08T18:11:02Z</dc:date>
    </item>
    <item>
      <title>Re: Driver configuration for S32K322</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Driver-configuration-for-S32K322/m-p/1784827#M11674</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Yes i need RTD set for S32k322. Here we are using&amp;nbsp;&lt;SPAN&gt;S32DS v3.5 and RTD version are 2.0.3 and 3.0.0.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Kindly provide me the which RTD version i have to use for S32k322?. We require FreeRTOS also&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 09 Jan 2024 03:43:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Driver-configuration-for-S32K322/m-p/1784827#M11674</guid>
      <dc:creator>LavanyaR</dc:creator>
      <dc:date>2024-01-09T03:43:18Z</dc:date>
    </item>
    <item>
      <title>Re: Driver configuration for S32K322</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Driver-configuration-for-S32K322/m-p/1785491#M11678</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/225259"&gt;@LavanyaR&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;As you know, S32K3 has many derivatives, so to reduce effort, in the most recent RTD releases we only provide examples for K344, K358, and K396. Examples of other derivatives can be created based on these existing examples. Also, as you are using RTD version 2.0.3, all S32K342 examples will work for S32K322&amp;nbsp;as long as you modify the DTCM and ITCM size in the linker script.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="VaneB_1-1704830066285.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/257368i8E49769E94BC7064/image-size/medium?v=v2&amp;amp;px=400" role="button" title="VaneB_1-1704830066285.png" alt="VaneB_1-1704830066285.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;VaneB_1-1704830066285.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;The S32K322 devices are supported by RTD 2.0.x, 3.0.0 and 4.0.0. You can find a list of supported derivatives in ReleaseNotes.pdf (Chapter 2.3 Supported Derivatives).&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R.&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;</description>
      <pubDate>Tue, 09 Jan 2024 19:55:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Driver-configuration-for-S32K322/m-p/1785491#M11678</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2024-01-09T19:55:22Z</dc:date>
    </item>
    <item>
      <title>Re: Driver configuration for S32K322</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Driver-configuration-for-S32K322/m-p/1785709#M11679</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201913"&gt;@VaneB&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. Can you tell me procedure to modify the linker script?&lt;/P&gt;&lt;P&gt;2. We are having ADC, SPI, CAN, I2C, timer and RTC driver code for S32k324 controller. Shall we use this driver code for s32k322 controller?&lt;/P&gt;&lt;P&gt;Note : We taken s32k344 example code as reference for configuring the above drivers.&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Lavanya&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 10 Jan 2024 03:48:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Driver-configuration-for-S32K322/m-p/1785709#M11679</guid>
      <dc:creator>LavanyaR</dc:creator>
      <dc:date>2024-01-10T03:48:23Z</dc:date>
    </item>
    <item>
      <title>Re: Driver configuration for S32K322</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Driver-configuration-for-S32K322/m-p/1786566#M11688</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/225259"&gt;@LavanyaR&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1. In the Linker file, ensure that the size of ITCM and DTCM are as shown in the following code. Also, the Linker file is already provided when you create a new application project with the desired MCU.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;LI-CODE lang="c"&gt;int_itcm                : ORIGIN = 0x00000000, LENGTH = 0x00008000    /* 32K */
int_dtcm                : ORIGIN = 0x20000000, LENGTH = 0x00010000    /* 64K */&lt;/LI-CODE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;2. For S32K322 the most viable option is to generate a new project with the corresponding MCU and then copy the application source files from your pre-existing project as well as any customizations you made to the project properties.&lt;/P&gt;</description>
      <pubDate>Wed, 10 Jan 2024 22:18:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Driver-configuration-for-S32K322/m-p/1786566#M11688</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2024-01-10T22:18:15Z</dc:date>
    </item>
    <item>
      <title>Re: Driver configuration for S32K322</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Driver-configuration-for-S32K322/m-p/1787713#M11694</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201913"&gt;@VaneB&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In our project I2C1 (PTD9 &amp;amp; PTD6) used for EEPROM communication. I2C1 (PTC6 &amp;amp;PTC7) used for RTC&amp;nbsp;communication. Is it possible to configure the same instance twice in single master?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Lavanya&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 12 Jan 2024 05:18:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Driver-configuration-for-S32K322/m-p/1787713#M11694</guid>
      <dc:creator>LavanyaR</dc:creator>
      <dc:date>2024-01-12T05:18:26Z</dc:date>
    </item>
  </channel>
</rss>