<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: Issue when S32DS using Jlink to debug</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Issue-when-S32DS-using-Jlink-to-debug/m-p/1784705#M11672</link>
    <description>Hi Julian,&lt;BR /&gt;Thanks for the reply.&lt;BR /&gt;I've fixed the issue by removing the step-3 above.&lt;BR /&gt;As you can see the error report in step-4 "another server is running...". Since we have set the Jlink serverCL.exe in the setp-2 and the server will be started when do the debug, so the Step-3 should not be done.&lt;BR /&gt;&lt;BR /&gt;Hope it works for your side.&lt;BR /&gt;&lt;BR /&gt;BR,&lt;BR /&gt;Gavin&lt;BR /&gt;</description>
    <pubDate>Tue, 09 Jan 2024 01:09:17 GMT</pubDate>
    <dc:creator>GavinLi1</dc:creator>
    <dc:date>2024-01-09T01:09:17Z</dc:date>
    <item>
      <title>Issue when S32DS using Jlink to debug</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Issue-when-S32DS-using-Jlink-to-debug/m-p/1784287#M11662</link>
      <description>&lt;P&gt;Hi NXP experts,&lt;/P&gt;&lt;P&gt;I follow the&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32-Design-Studio-for-S32-Platform-V3-4-V3-5-SEGGER-J-LINK-Plus/ta-p/1635798" target="_blank" rel="noopener"&gt;S32 Design Studio for S32 Platform V3.4/V3.5 + SEG... - NXP Community&lt;/A&gt;&amp;nbsp;to using Jlink to connect S32K324(since there is no S32K324 example found in RTD, I use the S32K344 example instead) but meet issue.&lt;/P&gt;&lt;P&gt;My steps shown as follow:&lt;/P&gt;&lt;P&gt;1.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="GavinLi1_0-1704704989635.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/257043i03113AD939B2ED99/image-size/medium?v=v2&amp;amp;px=400" role="button" title="GavinLi1_0-1704704989635.png" alt="GavinLi1_0-1704704989635.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;2.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="GavinLi1_1-1704705028773.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/257044i72AEFB7DA2739D9E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="GavinLi1_1-1704705028773.png" alt="GavinLi1_1-1704705028773.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;3.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="GavinLi1_0-1704705549788.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/257047i08ACCABBD87E7C1F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="GavinLi1_0-1704705549788.png" alt="GavinLi1_0-1704705549788.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;4.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="GavinLi1_3-1704705074772.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/257046i62F787E9C14808AC/image-size/medium?v=v2&amp;amp;px=400" role="button" title="GavinLi1_3-1704705074772.png" alt="GavinLi1_3-1704705074772.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Any steps I miss?&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;Gavin&lt;/P&gt;</description>
      <pubDate>Mon, 08 Jan 2024 09:19:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Issue-when-S32DS-using-Jlink-to-debug/m-p/1784287#M11662</guid>
      <dc:creator>GavinLi1</dc:creator>
      <dc:date>2024-01-08T09:19:18Z</dc:date>
    </item>
    <item>
      <title>Re: Issue when S32DS using Jlink to debug</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Issue-when-S32DS-using-Jlink-to-debug/m-p/1784517#M11668</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;did you check with&amp;nbsp;Windows Task Manager if there is really not running another J-Link gdb server instance ?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Other possibility is that Firewall/network policy or other application is blocking port 2331.&lt;/P&gt;</description>
      <pubDate>Mon, 08 Jan 2024 15:19:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Issue-when-S32DS-using-Jlink-to-debug/m-p/1784517#M11668</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2024-01-08T15:19:13Z</dc:date>
    </item>
    <item>
      <title>Re: Issue when S32DS using Jlink to debug</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Issue-when-S32DS-using-Jlink-to-debug/m-p/1784635#M11671</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/227799"&gt;@GavinLi1&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Adding to what Jiri said, please consider porting the example from the K344 to the K324, as there are some differences between devices that may come with issues.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián.&lt;/P&gt;</description>
      <pubDate>Mon, 08 Jan 2024 20:14:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Issue-when-S32DS-using-Jlink-to-debug/m-p/1784635#M11671</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-01-08T20:14:10Z</dc:date>
    </item>
    <item>
      <title>Re: Issue when S32DS using Jlink to debug</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Issue-when-S32DS-using-Jlink-to-debug/m-p/1784705#M11672</link>
      <description>Hi Julian,&lt;BR /&gt;Thanks for the reply.&lt;BR /&gt;I've fixed the issue by removing the step-3 above.&lt;BR /&gt;As you can see the error report in step-4 "another server is running...". Since we have set the Jlink serverCL.exe in the setp-2 and the server will be started when do the debug, so the Step-3 should not be done.&lt;BR /&gt;&lt;BR /&gt;Hope it works for your side.&lt;BR /&gt;&lt;BR /&gt;BR,&lt;BR /&gt;Gavin&lt;BR /&gt;</description>
      <pubDate>Tue, 09 Jan 2024 01:09:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Issue-when-S32DS-using-Jlink-to-debug/m-p/1784705#M11672</guid>
      <dc:creator>GavinLi1</dc:creator>
      <dc:date>2024-01-09T01:09:17Z</dc:date>
    </item>
  </channel>
</rss>