<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: S32DS V3.5.4: Command Line Execution - Working With Projects</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-V3-5-4-Command-Line-Execution-Working-With-Projects/m-p/1772042#M11522</link>
    <description>&lt;P&gt;Hi jiri_kral&lt;/P&gt;&lt;P&gt;I have attached the complete log.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 11 Dec 2023 07:47:22 GMT</pubDate>
    <dc:creator>superbird</dc:creator>
    <dc:date>2023-12-11T07:47:22Z</dc:date>
    <item>
      <title>S32DS V3.5.4: Command Line Execution - Working With Projects</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-V3-5-4-Command-Line-Execution-Working-With-Projects/m-p/1770544#M11505</link>
      <description>&lt;P&gt;Hello community,&lt;/P&gt;&lt;P&gt;I am using the S32DS V3.5.4 and want to use the command line to open/import existing projects. In V3.4.x I was using the command "s32ds.exe -nosplash -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data WORKSPACE -import PROJECT" to manage this. Now, in version V3.5.4 this does not work anymore (although it should according to manual). I can see the start screen of the S32DS but then the IDE quits again immediately.&lt;/P&gt;&lt;P&gt;In ".log" I see the following lines when the error occurs:&lt;/P&gt;&lt;P&gt;"java.lang.NullPointerException&lt;BR /&gt;at com.nxp.swtools.ivt.controller.IVTController.getInstance(IVTController.java:176)&lt;BR /&gt;at com.nxp.swtools.ivt.main.IVTServiceProvider.existsPointerOfLockState(IVTServiceProvider.java:51)&lt;BR /&gt;at com.nxp.swtools.ivt.main.IVTServiceProvider.getCurrentState(IVTServiceProvider.java:40)&lt;BR /&gt;at org.eclipse.ui.internal.services.EvaluationService.addSourceProvider(EvaluationService.java:157)&lt;BR /&gt;at org.eclipse.ui.internal.Workbench$34.runWithException(Workbench.java:2291)&lt;BR /&gt;at org.eclipse.ui.internal.StartupThreading$StartupRunnable.run(StartupThreading.java:36)&lt;BR /&gt;at org.eclipse.swt.widgets.Synchronizer.syncExec(Synchronizer.java:236)&lt;BR /&gt;at org.eclipse.ui.internal.UISynchronizer.syncExec(UISynchronizer.java:133)&lt;BR /&gt;at org.eclipse.swt.widgets.Display.syncExec(Display.java:4742)&lt;BR /&gt;at org.eclipse.ui.internal.StartupThreading.runWithoutExceptions(StartupThreading.java:94)&lt;BR /&gt;at org.eclipse.ui.internal.Workbench.initializeDefaultServices(Workbench.java:2283)&lt;BR /&gt;at org.eclipse.ui.internal.Workbench.init(Workbench.java:1606)&lt;BR /&gt;at org.eclipse.ui.internal.Workbench.runUI(Workbench.java:2759)&lt;BR /&gt;at org.eclipse.ui.internal.Workbench.lambda$3(Workbench.java:637)&lt;BR /&gt;at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:338)&lt;BR /&gt;at org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:551)&lt;BR /&gt;at org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:156)&lt;BR /&gt;at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:152)&lt;BR /&gt;at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:203)&lt;BR /&gt;at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:134)&lt;BR /&gt;at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104)&lt;BR /&gt;at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:401)&lt;BR /&gt;at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:255)&lt;BR /&gt;at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke0(Native Method)&lt;BR /&gt;at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke(Unknown Source)&lt;BR /&gt;at java.base/jdk.internal.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source)&lt;BR /&gt;at java.base/java.lang.reflect.Method.invoke(Unknown Source)&lt;BR /&gt;at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:654)&lt;BR /&gt;at org.eclipse.equinox.launcher.Main.basicRun(Main.java:591)&lt;BR /&gt;at org.eclipse.equinox.launcher.Main.run(Main.java:1462)"&lt;/P&gt;&lt;P&gt;I guess this is the reason for the error. Has anyone an idea how to solve this? Thank you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 07 Dec 2023 08:18:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-V3-5-4-Command-Line-Execution-Working-With-Projects/m-p/1770544#M11505</guid>
      <dc:creator>superbird</dc:creator>
      <dc:date>2023-12-07T08:18:46Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS V3.5.4: Command Line Execution - Working With Projects</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-V3-5-4-Command-Line-Execution-Working-With-Projects/m-p/1771567#M11514</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;this is full console output or only part? If part, please share full console output.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 08 Dec 2023 13:54:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-V3-5-4-Command-Line-Execution-Working-With-Projects/m-p/1771567#M11514</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2023-12-08T13:54:09Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS V3.5.4: Command Line Execution - Working With Projects</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-V3-5-4-Command-Line-Execution-Working-With-Projects/m-p/1772042#M11522</link>
      <description>&lt;P&gt;Hi jiri_kral&lt;/P&gt;&lt;P&gt;I have attached the complete log.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 11 Dec 2023 07:47:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-V3-5-4-Command-Line-Execution-Working-With-Projects/m-p/1772042#M11522</guid>
      <dc:creator>superbird</dc:creator>
      <dc:date>2023-12-11T07:47:22Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS V3.5.4: Command Line Execution - Working With Projects</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-V3-5-4-Command-Line-Execution-Working-With-Projects/m-p/1801751#M11824</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/159987"&gt;@jiri_kral&lt;/a&gt;&amp;nbsp;: Is there any news regarding this?&lt;/P&gt;</description>
      <pubDate>Mon, 05 Feb 2024 08:40:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-V3-5-4-Command-Line-Execution-Working-With-Projects/m-p/1801751#M11824</guid>
      <dc:creator>superbird</dc:creator>
      <dc:date>2024-02-05T08:40:54Z</dc:date>
    </item>
  </channel>
</rss>