<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックI get an error when I open the project folder.</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/I-get-an-error-when-I-open-the-project-folder/m-p/1764664#M11455</link>
    <description>&lt;P&gt;I was using version 3.4 of the S32 Design studio IDE. But I changed my computer and installed version 3.5.&amp;nbsp;When I open every project folder I import, the IDE directly gives an error. There is no problem in compiling, but I get the following error;&lt;/P&gt;&lt;P&gt;"Current version of the toolchain is no longer supported. It is necessary to perform project migration to a later version."&lt;/P&gt;&lt;P&gt;As a result of this process, should I reinstall the old version IDE from scratch? Or is there another solution?&lt;/P&gt;</description>
    <pubDate>Tue, 28 Nov 2023 08:10:15 GMT</pubDate>
    <dc:creator>michelangeliousas</dc:creator>
    <dc:date>2023-11-28T08:10:15Z</dc:date>
    <item>
      <title>I get an error when I open the project folder.</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/I-get-an-error-when-I-open-the-project-folder/m-p/1764664#M11455</link>
      <description>&lt;P&gt;I was using version 3.4 of the S32 Design studio IDE. But I changed my computer and installed version 3.5.&amp;nbsp;When I open every project folder I import, the IDE directly gives an error. There is no problem in compiling, but I get the following error;&lt;/P&gt;&lt;P&gt;"Current version of the toolchain is no longer supported. It is necessary to perform project migration to a later version."&lt;/P&gt;&lt;P&gt;As a result of this process, should I reinstall the old version IDE from scratch? Or is there another solution?&lt;/P&gt;</description>
      <pubDate>Tue, 28 Nov 2023 08:10:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/I-get-an-error-when-I-open-the-project-folder/m-p/1764664#M11455</guid>
      <dc:creator>michelangeliousas</dc:creator>
      <dc:date>2023-11-28T08:10:15Z</dc:date>
    </item>
    <item>
      <title>Re: I get an error when I open the project folder.</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/I-get-an-error-when-I-open-the-project-folder/m-p/1765866#M11465</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/207667"&gt;@michelangeliousas&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Your issue seems to be the compatibility of the IDE version and the packages installed.&lt;/P&gt;
&lt;P&gt;Reinstalling the old version could be a solution, however if you can share with me the packages you use I can verify if there are available for the 3.5 version of S32 Design Studio.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please let me know.&lt;/P&gt;</description>
      <pubDate>Wed, 29 Nov 2023 17:42:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/I-get-an-error-when-I-open-the-project-folder/m-p/1765866#M11465</guid>
      <dc:creator>Miguel04</dc:creator>
      <dc:date>2023-11-29T17:42:25Z</dc:date>
    </item>
  </channel>
</rss>