<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Multiple FlexCAN Configurations in ConfigTools? in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Multiple-FlexCAN-Configurations-in-ConfigTools/m-p/1763309#M11448</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;yes, in Config tool single config struct can be defined. If needed you can create own in your code.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Fri, 24 Nov 2023 10:31:20 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2023-11-24T10:31:20Z</dc:date>
    <item>
      <title>Multiple FlexCAN Configurations in ConfigTools?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Multiple-FlexCAN-Configurations-in-ConfigTools/m-p/1762286#M11442</link>
      <description>&lt;P&gt;I'm in the process of migrating a project from S32DS v2.2 with Processor Expert to S32DS v3.5 with Config Tools.&amp;nbsp; In PE, you can define multiple CAN Configurations.&amp;nbsp; For example, one for CAN at 250 Kbps and one at 500 Kbps.&amp;nbsp; I actually have 8 CAN configurations defined in PE.&amp;nbsp; In the Peripherals Tool (Config Tools), I'm not seeing a way to define more than one configuration per CAN instance.&amp;nbsp; Am I missing something? Do I just have to create my own config structs?&lt;/P&gt;</description>
      <pubDate>Thu, 23 Nov 2023 02:24:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Multiple-FlexCAN-Configurations-in-ConfigTools/m-p/1762286#M11442</guid>
      <dc:creator>tsweaver</dc:creator>
      <dc:date>2023-11-23T02:24:04Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple FlexCAN Configurations in ConfigTools?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Multiple-FlexCAN-Configurations-in-ConfigTools/m-p/1763309#M11448</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;yes, in Config tool single config struct can be defined. If needed you can create own in your code.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Fri, 24 Nov 2023 10:31:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Multiple-FlexCAN-Configurations-in-ConfigTools/m-p/1763309#M11448</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-11-24T10:31:20Z</dc:date>
    </item>
  </channel>
</rss>