<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックS32DS Pin Tool Edited Configuration Mismatch with project's *.c/*.h files</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Pin-Tool-Edited-Configuration-Mismatch-with-project-s-c-h/m-p/1753508#M11343</link>
    <description>&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;when I create a project from a port example and change the pin configuration in Pin-Tool the resulting configurations are not reflected automatically to corresponding source/header files even if I click to update code section.&lt;/P&gt;&lt;P&gt;Does that mean already like this? Or am I missing something?&lt;/P&gt;&lt;P&gt;In the corresponding part of the help document, it refers only to see the new code in code-view and to export the new files to integrate them. So, is the automatic update of the corresponding files not possible at all?&lt;/P&gt;&lt;P&gt;One another thing is that the updated files in the Pin-Tool are the following,&lt;/P&gt;&lt;P&gt;-&amp;nbsp;Siul2_Port_Ip_Cfg.c&lt;/P&gt;&lt;P&gt;-&amp;nbsp;Siul2_Port_Ip_Cfg.h&lt;/P&gt;&lt;P&gt;- Tspc_Port_Ip_Cfg.c&lt;/P&gt;&lt;P&gt;-&amp;nbsp;Tspc_Port_Ip_Cfg.h&lt;/P&gt;&lt;P&gt;but the files in the project under generate/ are as following.&lt;/P&gt;&lt;P&gt;-&amp;nbsp;Siul2_Port_Ip_&lt;STRONG&gt;PB&lt;/STRONG&gt;cfg.c&lt;/P&gt;&lt;P&gt;- Siul2_Port_Ip_&lt;STRONG&gt;PB&lt;/STRONG&gt;cfg.h&lt;/P&gt;&lt;P&gt;-&amp;nbsp;Tspc_Port_Ip_&lt;STRONG&gt;PB&lt;/STRONG&gt;cfg.c&lt;/P&gt;&lt;P&gt;-&amp;nbsp;Tspc_Port_Ip_&lt;STRONG&gt;PB&lt;/STRONG&gt;cfg.h&lt;/P&gt;&lt;P&gt;What does this 'PB' stand for? And why is it added?&lt;/P&gt;&lt;P&gt;Last thing is, if the exported files have to be manually integrated always where do I know all files which are needed to be updated and the possible dependencies which might need to be adapted manually?&lt;/P&gt;&lt;P&gt;Does the Update-Code-Dialog-Window show always all changed files? If yes, might there be still other possible files which might need to be adapted accordingly?&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;</description>
    <pubDate>Tue, 07 Nov 2023 13:04:51 GMT</pubDate>
    <dc:creator>eronimo</dc:creator>
    <dc:date>2023-11-07T13:04:51Z</dc:date>
    <item>
      <title>S32DS Pin Tool Edited Configuration Mismatch with project's *.c/*.h files</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Pin-Tool-Edited-Configuration-Mismatch-with-project-s-c-h/m-p/1753508#M11343</link>
      <description>&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;when I create a project from a port example and change the pin configuration in Pin-Tool the resulting configurations are not reflected automatically to corresponding source/header files even if I click to update code section.&lt;/P&gt;&lt;P&gt;Does that mean already like this? Or am I missing something?&lt;/P&gt;&lt;P&gt;In the corresponding part of the help document, it refers only to see the new code in code-view and to export the new files to integrate them. So, is the automatic update of the corresponding files not possible at all?&lt;/P&gt;&lt;P&gt;One another thing is that the updated files in the Pin-Tool are the following,&lt;/P&gt;&lt;P&gt;-&amp;nbsp;Siul2_Port_Ip_Cfg.c&lt;/P&gt;&lt;P&gt;-&amp;nbsp;Siul2_Port_Ip_Cfg.h&lt;/P&gt;&lt;P&gt;- Tspc_Port_Ip_Cfg.c&lt;/P&gt;&lt;P&gt;-&amp;nbsp;Tspc_Port_Ip_Cfg.h&lt;/P&gt;&lt;P&gt;but the files in the project under generate/ are as following.&lt;/P&gt;&lt;P&gt;-&amp;nbsp;Siul2_Port_Ip_&lt;STRONG&gt;PB&lt;/STRONG&gt;cfg.c&lt;/P&gt;&lt;P&gt;- Siul2_Port_Ip_&lt;STRONG&gt;PB&lt;/STRONG&gt;cfg.h&lt;/P&gt;&lt;P&gt;-&amp;nbsp;Tspc_Port_Ip_&lt;STRONG&gt;PB&lt;/STRONG&gt;cfg.c&lt;/P&gt;&lt;P&gt;-&amp;nbsp;Tspc_Port_Ip_&lt;STRONG&gt;PB&lt;/STRONG&gt;cfg.h&lt;/P&gt;&lt;P&gt;What does this 'PB' stand for? And why is it added?&lt;/P&gt;&lt;P&gt;Last thing is, if the exported files have to be manually integrated always where do I know all files which are needed to be updated and the possible dependencies which might need to be adapted manually?&lt;/P&gt;&lt;P&gt;Does the Update-Code-Dialog-Window show always all changed files? If yes, might there be still other possible files which might need to be adapted accordingly?&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;</description>
      <pubDate>Tue, 07 Nov 2023 13:04:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Pin-Tool-Edited-Configuration-Mismatch-with-project-s-c-h/m-p/1753508#M11343</guid>
      <dc:creator>eronimo</dc:creator>
      <dc:date>2023-11-07T13:04:51Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS Pin Tool Edited Configuration Mismatch with project's *.c/*.h files</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Pin-Tool-Edited-Configuration-Mismatch-with-project-s-c-h/m-p/1756406#M11393</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/225426"&gt;@eronimo&lt;/a&gt;&amp;nbsp;,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;Answer to your last question.&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;Does the Update-Code-Dialog-Window show always all changed files? If yes, might there be still other possible files which might need to be adapted accordingly?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt; is &lt;STRONG&gt;Yes&lt;/STRONG&gt; - &lt;U&gt;Update Code dialog will show all the modified files and replace them in the project after completing the Update action.&lt;/U&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;Let me get back to you in some time for other questions.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;Thank you. Best regards,&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;-Mehul Patel&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 13 Nov 2023 16:44:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Pin-Tool-Edited-Configuration-Mismatch-with-project-s-c-h/m-p/1756406#M11393</guid>
      <dc:creator>Mehul_Patel_NXP</dc:creator>
      <dc:date>2023-11-13T16:44:43Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS Pin Tool Edited Configuration Mismatch with project's *.c/*.h files</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Pin-Tool-Edited-Configuration-Mismatch-with-project-s-c-h/m-p/1758334#M11414</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;When you change&amp;nbsp;&lt;SPAN&gt;Pin-Tool, it hasn't changed the generation files yet. You must add the Pin you change into Port module of Configurations tool also:&lt;BR /&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="cuongnguyenphu_0-1700133737957.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/250184i948583DB2957936A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="cuongnguyenphu_0-1700133737957.png" alt="cuongnguyenphu_0-1700133737957.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Then, when click on Update Code, it will update generated file.&lt;BR /&gt;Pin-Tool is where you can confige attribute for the specific pin, and to use this pin, you need to add it in Port module.&lt;BR /&gt;&lt;BR /&gt;The meaning of PB is Post-Build, which is related to the Config Variant type you use to generate these config module.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="cuongnguyenphu_1-1700133911985.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/250185iACEE570728152B23/image-size/medium?v=v2&amp;amp;px=400" role="button" title="cuongnguyenphu_1-1700133911985.png" alt="cuongnguyenphu_1-1700133911985.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;- If use Post-build variant: You must call Port_Init(&amp;amp;Port_Config);&lt;BR /&gt;- If use pre-Compile variant: You must call Port_Init(NULL);&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Last thing is, if the exported files have to be manually integrated always where do I know all files which are needed to be updated and the possible dependencies which might need to be adapted manually? -&amp;gt; I don't really understand your question, what is exported file? Can you give an example&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Nov 2023 11:28:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Pin-Tool-Edited-Configuration-Mismatch-with-project-s-c-h/m-p/1758334#M11414</guid>
      <dc:creator>cuongnguyenphu</dc:creator>
      <dc:date>2023-11-16T11:28:17Z</dc:date>
    </item>
  </channel>
</rss>