<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックS32 KEA132, Comment Bug in uart.h (library)</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32-KEA132-Comment-Bug-in-uart-h-library/m-p/652767#M1128</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The comment below are incorrect, the do not return 1 but return non-zero number such as 0x20, not 1. &amp;nbsp;Please review and correct comment, thanks.&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;/*****************************************************************************//*!&lt;BR /&gt;*&lt;BR /&gt;* @brief check whether tx is complete,i.e. data has been sent out.&lt;BR /&gt;* &lt;BR /&gt;* @param[in] pUART base of UART port&lt;BR /&gt;*&lt;BR /&gt;* @return &lt;BR /&gt;* 1, Tx complete flag is set&lt;BR /&gt;* 0, Tx complete flag is clear&lt;BR /&gt;*&lt;BR /&gt;* @ Pass/ Fail criteria: none&lt;BR /&gt;*****************************************************************************/&lt;BR /&gt;static inline uint8_t UART_IsTxComplete(UART_MemMapPtr pUART)&lt;BR /&gt;{&lt;BR /&gt; return (pUART-&amp;gt;S1 &amp;amp; UART_S1_TC_MASK);&lt;BR /&gt;}&lt;BR /&gt;/*****************************************************************************//*!&lt;BR /&gt;*&lt;BR /&gt;* @brief check whether Tx buffer is empty&lt;BR /&gt;* &lt;BR /&gt;* @param[in] pUART base of UART port&lt;BR /&gt;*&lt;BR /&gt;* @return &lt;BR /&gt;* 1, Tx buffer is empty&lt;BR /&gt;* 0, Tx buffer is not empty&lt;BR /&gt;*&lt;BR /&gt;* @ Pass/ Fail criteria: none&lt;BR /&gt;*****************************************************************************/&lt;BR /&gt;static inline uint8_t UART_IsTxBuffEmpty(UART_MemMapPtr pUART)&lt;BR /&gt;{&lt;BR /&gt; return (pUART-&amp;gt;S1 &amp;amp; UART_S1_TDRE_MASK);&lt;BR /&gt;}&lt;BR /&gt;/*****************************************************************************//*!&lt;BR /&gt;*&lt;BR /&gt;* @brief check whether Rx buffer is full, i.e. receive a character&lt;BR /&gt;* &lt;BR /&gt;* @param[in] pUART base of UART port&lt;BR /&gt;*&lt;BR /&gt;* @return &lt;BR /&gt;* 1, Rx buffer is full&lt;BR /&gt;* 0, Rx buffer is not full&lt;BR /&gt;*&lt;BR /&gt;* @ Pass/ Fail criteria: none&lt;BR /&gt;*****************************************************************************/&lt;BR /&gt;static inline uint8_t UART_IsRxBuffFull(UART_MemMapPtr pUART)&lt;BR /&gt;{&lt;BR /&gt; return (pUART-&amp;gt;S1 &amp;amp; UART_S1_RDRF_MASK);&lt;BR /&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 01 Jan 2017 11:53:14 GMT</pubDate>
    <dc:creator>richardpayne</dc:creator>
    <dc:date>2017-01-01T11:53:14Z</dc:date>
    <item>
      <title>S32 KEA132, Comment Bug in uart.h (library)</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32-KEA132-Comment-Bug-in-uart-h-library/m-p/652767#M1128</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The comment below are incorrect, the do not return 1 but return non-zero number such as 0x20, not 1. &amp;nbsp;Please review and correct comment, thanks.&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;/*****************************************************************************//*!&lt;BR /&gt;*&lt;BR /&gt;* @brief check whether tx is complete,i.e. data has been sent out.&lt;BR /&gt;* &lt;BR /&gt;* @param[in] pUART base of UART port&lt;BR /&gt;*&lt;BR /&gt;* @return &lt;BR /&gt;* 1, Tx complete flag is set&lt;BR /&gt;* 0, Tx complete flag is clear&lt;BR /&gt;*&lt;BR /&gt;* @ Pass/ Fail criteria: none&lt;BR /&gt;*****************************************************************************/&lt;BR /&gt;static inline uint8_t UART_IsTxComplete(UART_MemMapPtr pUART)&lt;BR /&gt;{&lt;BR /&gt; return (pUART-&amp;gt;S1 &amp;amp; UART_S1_TC_MASK);&lt;BR /&gt;}&lt;BR /&gt;/*****************************************************************************//*!&lt;BR /&gt;*&lt;BR /&gt;* @brief check whether Tx buffer is empty&lt;BR /&gt;* &lt;BR /&gt;* @param[in] pUART base of UART port&lt;BR /&gt;*&lt;BR /&gt;* @return &lt;BR /&gt;* 1, Tx buffer is empty&lt;BR /&gt;* 0, Tx buffer is not empty&lt;BR /&gt;*&lt;BR /&gt;* @ Pass/ Fail criteria: none&lt;BR /&gt;*****************************************************************************/&lt;BR /&gt;static inline uint8_t UART_IsTxBuffEmpty(UART_MemMapPtr pUART)&lt;BR /&gt;{&lt;BR /&gt; return (pUART-&amp;gt;S1 &amp;amp; UART_S1_TDRE_MASK);&lt;BR /&gt;}&lt;BR /&gt;/*****************************************************************************//*!&lt;BR /&gt;*&lt;BR /&gt;* @brief check whether Rx buffer is full, i.e. receive a character&lt;BR /&gt;* &lt;BR /&gt;* @param[in] pUART base of UART port&lt;BR /&gt;*&lt;BR /&gt;* @return &lt;BR /&gt;* 1, Rx buffer is full&lt;BR /&gt;* 0, Rx buffer is not full&lt;BR /&gt;*&lt;BR /&gt;* @ Pass/ Fail criteria: none&lt;BR /&gt;*****************************************************************************/&lt;BR /&gt;static inline uint8_t UART_IsRxBuffFull(UART_MemMapPtr pUART)&lt;BR /&gt;{&lt;BR /&gt; return (pUART-&amp;gt;S1 &amp;amp; UART_S1_RDRF_MASK);&lt;BR /&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 01 Jan 2017 11:53:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32-KEA132-Comment-Bug-in-uart-h-library/m-p/652767#M1128</guid>
      <dc:creator>richardpayne</dc:creator>
      <dc:date>2017-01-01T11:53:14Z</dc:date>
    </item>
  </channel>
</rss>