<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design Studio中的主题 Re: S32K_multicore_trace32_normal_multilink_hardware_fault</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32K-multicore-trace32-normal-multilink-hardware-fault/m-p/1744609#M11251</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221619"&gt;@Zhougw&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you please create a support request ticket on the PEmicro website? Please click on the "Support Requests" link&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.pemicro.com/support/index.cfm" target="_blank"&gt;https://www.pemicro.com/support/index.cfm&lt;/A&gt;&lt;/P&gt;&lt;P&gt;That way, the issue can be investigated by PEmicro engineers.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 23 Oct 2023 14:56:48 GMT</pubDate>
    <dc:creator>juan_see</dc:creator>
    <dc:date>2023-10-23T14:56:48Z</dc:date>
    <item>
      <title>S32K_multicore_trace32_normal_multilink_hardware_fault</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32K-multicore-trace32-normal-multilink-hardware-fault/m-p/1743293#M11234</link>
      <description>&lt;P&gt;I use core0 and core2 of S32K3, use core0 to start core2.&lt;/P&gt;&lt;P&gt;with trace32, after load elf of core0 and core2, core2 show buss error, after core0 run mcu_setmode, core2 become normal(no bus error)., run core2 mannually, LED and CAN is OK.&lt;/P&gt;&lt;P&gt;no debugger after downloaded elf, LED and CAN is OK.&lt;/P&gt;&lt;P&gt;with multilink+s32ds, after load elf of core0 and core2, core0 is in main function, core2 triggerred hardware fault. debug cann't go on.&lt;/P&gt;&lt;P&gt;with multilink+s32ds, empty project core0 and core2 start at the same time, no bus error.&lt;/P&gt;&lt;P&gt;I guess it is because when core0 is in the entry of main function, core2 haven't started, when debugger connect core2, hardware fault triggerred.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;if I want to use core0 to start core2, and i want to use multilink+s32ds to debug, how can I solve this problem. the same elf works fine with trace32 or with no debugger, so the problem is in multilink+s32ds.&lt;/P&gt;</description>
      <pubDate>Fri, 20 Oct 2023 01:42:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32K-multicore-trace32-normal-multilink-hardware-fault/m-p/1743293#M11234</guid>
      <dc:creator>Zhougw</dc:creator>
      <dc:date>2023-10-20T01:42:11Z</dc:date>
    </item>
    <item>
      <title>Re: S32K_multicore_trace32_normal_multilink_hardware_fault</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32K-multicore-trace32-normal-multilink-hardware-fault/m-p/1744609#M11251</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221619"&gt;@Zhougw&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you please create a support request ticket on the PEmicro website? Please click on the "Support Requests" link&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.pemicro.com/support/index.cfm" target="_blank"&gt;https://www.pemicro.com/support/index.cfm&lt;/A&gt;&lt;/P&gt;&lt;P&gt;That way, the issue can be investigated by PEmicro engineers.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 23 Oct 2023 14:56:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32K-multicore-trace32-normal-multilink-hardware-fault/m-p/1744609#M11251</guid>
      <dc:creator>juan_see</dc:creator>
      <dc:date>2023-10-23T14:56:48Z</dc:date>
    </item>
  </channel>
</rss>