<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Compilation in S32 design  in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Compilation-in-S32-design/m-p/652438#M1124</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yalamanda,&lt;/P&gt;&lt;P&gt;Please make sure the folder you've added is a "source folder" otherwise makefile does not touch the source files from that folder.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/13069iC5936FEDC2717CDB/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can easily "convert" generic folder into a source one:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/13109iA79330DD9BE7BEBE/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The icon will change to a Source Folder one and the source files from this folder are included to build:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/13190i95583F6E21F0E5CF/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Dec 2016 14:56:02 GMT</pubDate>
    <dc:creator>stanish</dc:creator>
    <dc:date>2016-12-06T14:56:02Z</dc:date>
    <item>
      <title>Compilation in S32 design</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Compilation-in-S32-design/m-p/652437#M1123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All, As I already have one Existing MPC5777M project , so I imported it into the S32 Design studio Power PC V1.1 Linux,So I am able to compile it, but when I included one new folder(consists some other modules code)&amp;nbsp; by copied some where and pasted it in the project, then It is failing to compile.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I checked everything in the new folder, it is&amp;nbsp; Ok.&lt;/P&gt;&lt;P&gt;I added all new folder paths in the properties-&amp;gt;c/c++ module-&amp;gt;settings-&amp;gt;c/c++ s32ds compiler -&amp;gt;includes.But it is still failing to detect the definition for some declarations.&lt;/P&gt;&lt;P&gt;So What are the things we need to take care for adding new folder into the project and make it compile .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Dec 2016 13:39:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Compilation-in-S32-design/m-p/652437#M1123</guid>
      <dc:creator>yalamandadosaky</dc:creator>
      <dc:date>2016-12-06T13:39:38Z</dc:date>
    </item>
    <item>
      <title>Re: Compilation in S32 design</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Compilation-in-S32-design/m-p/652438#M1124</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yalamanda,&lt;/P&gt;&lt;P&gt;Please make sure the folder you've added is a "source folder" otherwise makefile does not touch the source files from that folder.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/13069iC5936FEDC2717CDB/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can easily "convert" generic folder into a source one:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/13109iA79330DD9BE7BEBE/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The icon will change to a Source Folder one and the source files from this folder are included to build:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/13190i95583F6E21F0E5CF/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Dec 2016 14:56:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Compilation-in-S32-design/m-p/652438#M1124</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2016-12-06T14:56:02Z</dc:date>
    </item>
  </channel>
</rss>