<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: What's the function of 'Generated_Code' directory?</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/What-s-the-function-of-Generated-Code-directory/m-p/1743190#M11227</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224465"&gt;@fedora&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Processor Expert has a Code Generate Codecommand, which initiates the code generation process. During this process, the source code modules containing the functionality of the project components are generated in the Generated_Code folder in the Component view. The project must be set up correctly for successful code generation. If the generation is error-free, all generated source code files are saved to the destination directory.&lt;/P&gt;
&lt;P&gt;The existence of the files can be conditional to the project or Processor Expert environment settings and their usage by the components.&lt;/P&gt;
&lt;P&gt;NOTE: the modification of the generated code may be done only at the user's own risk.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-SDK/How-to-preserve-user-modification-overwrite-with-processor/m-p/872918" target="_blank" rel="noopener"&gt;How to preserve user modification overwrite with processor expert generated code?&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R.&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;</description>
    <pubDate>Thu, 19 Oct 2023 20:02:58 GMT</pubDate>
    <dc:creator>VaneB</dc:creator>
    <dc:date>2023-10-19T20:02:58Z</dc:date>
    <item>
      <title>What's the function of 'Generated_Code' directory?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/What-s-the-function-of-Generated-Code-directory/m-p/1742745#M11221</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I'm using the S32 Design Studio for ARM IDE, and found a 'Generated_Code' directory under this project, contains many *.c and *.h files.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;Please refer to the attached image.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I want to know what is the function of 'Generated_Code' directory and those temporary code files.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;Thanks for your help!&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Fedora&lt;/P&gt;</description>
      <pubDate>Thu, 19 Oct 2023 08:07:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/What-s-the-function-of-Generated-Code-directory/m-p/1742745#M11221</guid>
      <dc:creator>fedora</dc:creator>
      <dc:date>2023-10-19T08:07:52Z</dc:date>
    </item>
    <item>
      <title>Re: What's the function of 'Generated_Code' directory?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/What-s-the-function-of-Generated-Code-directory/m-p/1743190#M11227</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224465"&gt;@fedora&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Processor Expert has a Code Generate Codecommand, which initiates the code generation process. During this process, the source code modules containing the functionality of the project components are generated in the Generated_Code folder in the Component view. The project must be set up correctly for successful code generation. If the generation is error-free, all generated source code files are saved to the destination directory.&lt;/P&gt;
&lt;P&gt;The existence of the files can be conditional to the project or Processor Expert environment settings and their usage by the components.&lt;/P&gt;
&lt;P&gt;NOTE: the modification of the generated code may be done only at the user's own risk.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-SDK/How-to-preserve-user-modification-overwrite-with-processor/m-p/872918" target="_blank" rel="noopener"&gt;How to preserve user modification overwrite with processor expert generated code?&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R.&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;</description>
      <pubDate>Thu, 19 Oct 2023 20:02:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/What-s-the-function-of-Generated-Code-directory/m-p/1743190#M11227</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-10-19T20:02:58Z</dc:date>
    </item>
    <item>
      <title>Re: What's the function of 'Generated_Code' directory?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/What-s-the-function-of-Generated-Code-directory/m-p/1743391#M11233</link>
      <description>&lt;P&gt;Hello VaneB,&lt;/P&gt;&lt;P&gt;I'll continue to study it,&amp;nbsp; thanks for reply!&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Fedora&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 20 Oct 2023 05:00:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/What-s-the-function-of-Generated-Code-directory/m-p/1743391#M11233</guid>
      <dc:creator>fedora</dc:creator>
      <dc:date>2023-10-20T05:00:22Z</dc:date>
    </item>
  </channel>
</rss>