<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Which debugging interface is better? in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Which-debugging-interface-is-better/m-p/1715951#M10914</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/222343"&gt;@srikarthik0601&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;As you are using an EVB, is not necessary to use an external debugger to flash programming unless you want it or require it.&lt;/P&gt;
&lt;P&gt;Our EVB comes with an onboard debugger with&amp;nbsp;&lt;SPAN&gt;OpenSDA, which provides a bridge between your computer (or other USB hosts) and the embedded target processor, which can be used for debugging, flash programming, and serial communication, all over a simple USB cable.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;OpenSDA is programmed with the proprietary P&amp;amp;E Micro-developed bootloader. P&amp;amp;E Micro is the default debug interface app.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;B.R.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;VaneB&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 01 Sep 2023 19:08:40 GMT</pubDate>
    <dc:creator>VaneB</dc:creator>
    <dc:date>2023-09-01T19:08:40Z</dc:date>
    <item>
      <title>Which debugging interface is better?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Which-debugging-interface-is-better/m-p/1715877#M10913</link>
      <description>&lt;P&gt;I have a S32K144-Q100 evaluation board( total newbie here). Just wanted to ask which debugging interface is better ? Segger Debugging Interface or GDB PEMicro Debugging Interface&amp;nbsp;&lt;BR /&gt;What will be the differences if I choose one over the another?&lt;/P&gt;</description>
      <pubDate>Fri, 01 Sep 2023 15:34:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Which-debugging-interface-is-better/m-p/1715877#M10913</guid>
      <dc:creator>srikarthik0601</dc:creator>
      <dc:date>2023-09-01T15:34:10Z</dc:date>
    </item>
    <item>
      <title>Re: Which debugging interface is better?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Which-debugging-interface-is-better/m-p/1715951#M10914</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/222343"&gt;@srikarthik0601&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;As you are using an EVB, is not necessary to use an external debugger to flash programming unless you want it or require it.&lt;/P&gt;
&lt;P&gt;Our EVB comes with an onboard debugger with&amp;nbsp;&lt;SPAN&gt;OpenSDA, which provides a bridge between your computer (or other USB hosts) and the embedded target processor, which can be used for debugging, flash programming, and serial communication, all over a simple USB cable.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;OpenSDA is programmed with the proprietary P&amp;amp;E Micro-developed bootloader. P&amp;amp;E Micro is the default debug interface app.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;B.R.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;VaneB&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 01 Sep 2023 19:08:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Which-debugging-interface-is-better/m-p/1715951#M10914</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-09-01T19:08:40Z</dc:date>
    </item>
    <item>
      <title>Re: Which debugging interface is better?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Which-debugging-interface-is-better/m-p/1716532#M10924</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="srikarthik0601_0-1693832633455.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/239410i4D7B2E423A8CD56F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="srikarthik0601_0-1693832633455.png" alt="srikarthik0601_0-1693832633455.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;srikarthik0601_0-1693832633455.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I just wanted to know what to choose over here, PEMicro or Segger&lt;BR /&gt;I will go with PEMicro then.&amp;nbsp;&lt;BR /&gt;And also can you tell me about I/O support, Debugger Console vs real time printf with ITM&lt;/P&gt;</description>
      <pubDate>Mon, 04 Sep 2023 13:50:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Which-debugging-interface-is-better/m-p/1716532#M10924</guid>
      <dc:creator>srikarthik0601</dc:creator>
      <dc:date>2023-09-04T13:50:24Z</dc:date>
    </item>
    <item>
      <title>Re: Which debugging interface is better?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Which-debugging-interface-is-better/m-p/1716533#M10925</link>
      <description>Thanks for the quick reply</description>
      <pubDate>Mon, 04 Sep 2023 13:51:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Which-debugging-interface-is-better/m-p/1716533#M10925</guid>
      <dc:creator>srikarthik0601</dc:creator>
      <dc:date>2023-09-04T13:51:00Z</dc:date>
    </item>
    <item>
      <title>Re: Which debugging interface is better?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Which-debugging-interface-is-better/m-p/1716636#M10926</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/222343"&gt;@srikarthik0601&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;This setting enables the semi-hosting support and configures input/output to print information to the console during debugging.&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;STRONG&gt;No I/O&lt;/STRONG&gt; - No printing will be done.&lt;/LI&gt;
&lt;LI&gt;&lt;STRONG&gt;Debugger Console&lt;/STRONG&gt; - The output will be printed out to the console provided by the debugger specified in the Debugger setting.&lt;/LI&gt;
&lt;LI&gt;&lt;STRONG&gt;Real-time printf with ITM&lt;/STRONG&gt; - The Instrumentation Trace Macrocell (ITM) block provides a mechanism for sending data from your target to the debugger via the SWO trade stream.&lt;/LI&gt;
&lt;/UL&gt;</description>
      <pubDate>Mon, 04 Sep 2023 20:52:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Which-debugging-interface-is-better/m-p/1716636#M10926</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-09-04T20:52:55Z</dc:date>
    </item>
    <item>
      <title>Re: Which debugging interface is better?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Which-debugging-interface-is-better/m-p/1730697#M11055</link>
      <description>Thank you so much!</description>
      <pubDate>Wed, 27 Sep 2023 17:13:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Which-debugging-interface-is-better/m-p/1730697#M11055</guid>
      <dc:creator>srikarthik0601</dc:creator>
      <dc:date>2023-09-27T17:13:32Z</dc:date>
    </item>
  </channel>
</rss>