<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K Chip Performance and Motor Control in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32K-Chip-Performance-and-Motor-Control/m-p/1714032#M10899</link>
    <description>&lt;P&gt;hello&lt;/P&gt;&lt;P&gt;I am currently using s32k144 to create a motor controller, but due to the performance impact of s32k144, the motor controller cannot achieve the expected state.&lt;/P&gt;&lt;P&gt;At present, I have used a system frequency of 80M in my code, with O3 as the optimization level, cache enabled, FPU enabled, and fixed-point operations used to improve code execution efficiency.&lt;/P&gt;&lt;P&gt;I want to replace a chip without changing the current code to improve performance, and choose a chip with a higher system frequency and larger cache, among other factors.&lt;/P&gt;&lt;P&gt;excuse me&lt;/P&gt;&lt;P&gt;1. Are there any other optimization plans to improve code performance&lt;/P&gt;&lt;P&gt;2. Do the s32k series chips have the same IP addresses as S32K144's FTM, TRGMUX, PDB, ADC, and have higher performance?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Wed, 30 Aug 2023 12:38:48 GMT</pubDate>
    <dc:creator>zhangchun</dc:creator>
    <dc:date>2023-08-30T12:38:48Z</dc:date>
    <item>
      <title>S32K Chip Performance and Motor Control</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32K-Chip-Performance-and-Motor-Control/m-p/1714032#M10899</link>
      <description>&lt;P&gt;hello&lt;/P&gt;&lt;P&gt;I am currently using s32k144 to create a motor controller, but due to the performance impact of s32k144, the motor controller cannot achieve the expected state.&lt;/P&gt;&lt;P&gt;At present, I have used a system frequency of 80M in my code, with O3 as the optimization level, cache enabled, FPU enabled, and fixed-point operations used to improve code execution efficiency.&lt;/P&gt;&lt;P&gt;I want to replace a chip without changing the current code to improve performance, and choose a chip with a higher system frequency and larger cache, among other factors.&lt;/P&gt;&lt;P&gt;excuse me&lt;/P&gt;&lt;P&gt;1. Are there any other optimization plans to improve code performance&lt;/P&gt;&lt;P&gt;2. Do the s32k series chips have the same IP addresses as S32K144's FTM, TRGMUX, PDB, ADC, and have higher performance?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Wed, 30 Aug 2023 12:38:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32K-Chip-Performance-and-Motor-Control/m-p/1714032#M10899</guid>
      <dc:creator>zhangchun</dc:creator>
      <dc:date>2023-08-30T12:38:48Z</dc:date>
    </item>
    <item>
      <title>Re: S32K Chip Performance and Motor Control</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32K-Chip-Performance-and-Motor-Control/m-p/1715109#M10907</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;did you tried to use AMMClib? This library is very well optimized for motor control.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jiri_kral_0-1693488234372.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/239119iA625DB9518E03D2C/image-size/large?v=v2&amp;amp;px=999" role="button" title="jiri_kral_0-1693488234372.png" alt="jiri_kral_0-1693488234372.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;jiri_kral_0-1693488234372.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 31 Aug 2023 13:24:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32K-Chip-Performance-and-Motor-Control/m-p/1715109#M10907</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2023-08-31T13:24:28Z</dc:date>
    </item>
    <item>
      <title>Re: S32K Chip Performance and Motor Control</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32K-Chip-Performance-and-Motor-Control/m-p/1715131#M10908</link>
      <description>Hi&lt;BR /&gt;Thank you very much for your reply，</description>
      <pubDate>Thu, 31 Aug 2023 14:07:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32K-Chip-Performance-and-Motor-Control/m-p/1715131#M10908</guid>
      <dc:creator>zhangchun</dc:creator>
      <dc:date>2023-08-31T14:07:20Z</dc:date>
    </item>
  </channel>
</rss>