<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: Generate a project into DLL file on S32DS</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Generate-a-project-into-DLL-file-on-S32DS/m-p/1713790#M10893</link>
    <description>&lt;P&gt;No, I have a source code run on other chips, and need to run on the new chip. But, currently, the new chip is not available, just have a simulation for the chip on the PC, so I need to bring the source code to PC, build it into DLL file, and communicate with the Chip simulation on the another PC.&lt;/P&gt;</description>
    <pubDate>Wed, 30 Aug 2023 07:06:51 GMT</pubDate>
    <dc:creator>AnhNguyenDuc</dc:creator>
    <dc:date>2023-08-30T07:06:51Z</dc:date>
    <item>
      <title>Generate a project into DLL file on S32DS</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Generate-a-project-into-DLL-file-on-S32DS/m-p/1712729#M10880</link>
      <description>&lt;P&gt;Can S32DS create a project and build into DLL file?&lt;/P&gt;
&lt;P&gt;I want to bring a embedded program to PC as a DLL file, does anyone have a document I can refer to ?&lt;/P&gt;
&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Tue, 29 Aug 2023 04:04:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Generate-a-project-into-DLL-file-on-S32DS/m-p/1712729#M10880</guid>
      <dc:creator>AnhNguyenDuc</dc:creator>
      <dc:date>2023-08-29T04:04:53Z</dc:date>
    </item>
    <item>
      <title>Re: Generate a project into DLL file on S32DS</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Generate-a-project-into-DLL-file-on-S32DS/m-p/1713083#M10885</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;unfortunately it is not possible with S32DS. S32DS uses cross platform compilers for ARM or PowerPC.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Only what can be possible is adding embedded project as a binary (the .bin or .srec file) into memory array in your PC .dll library. But you need to have some emulator which can execute such binary.&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Anyway - what's the goal?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Aug 2023 09:39:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Generate-a-project-into-DLL-file-on-S32DS/m-p/1713083#M10885</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2023-08-29T09:39:57Z</dc:date>
    </item>
    <item>
      <title>Re: Generate a project into DLL file on S32DS</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Generate-a-project-into-DLL-file-on-S32DS/m-p/1713098#M10886</link>
      <description>&lt;P&gt;Thanks Jiri Kral,&lt;/P&gt;&lt;P&gt;I have a library want to test on a chip, but the chip is not available now, just having a simulation for that on the PC. So I need to bring the library on the PC too, then communicating between two the PCs. (maybe stub some driver stuffs, build the library into a DLL files, ...).&lt;/P&gt;&lt;P&gt;If you have the experience about that, please share to me.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Tue, 29 Aug 2023 09:56:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Generate-a-project-into-DLL-file-on-S32DS/m-p/1713098#M10886</guid>
      <dc:creator>AnhNguyenDuc</dc:creator>
      <dc:date>2023-08-29T09:56:05Z</dc:date>
    </item>
    <item>
      <title>Re: Generate a project into DLL file on S32DS</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Generate-a-project-into-DLL-file-on-S32DS/m-p/1713265#M10887</link>
      <description>&lt;P&gt;Sorry, have no experience with that. As I understand it - you have some .dll which can simulate the target device? And you like to use the target code build with S32DS instead of the .dll in some simulator? If So, there is no way how to do it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Aug 2023 12:35:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Generate-a-project-into-DLL-file-on-S32DS/m-p/1713265#M10887</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2023-08-29T12:35:17Z</dc:date>
    </item>
    <item>
      <title>Re: Generate a project into DLL file on S32DS</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Generate-a-project-into-DLL-file-on-S32DS/m-p/1713790#M10893</link>
      <description>&lt;P&gt;No, I have a source code run on other chips, and need to run on the new chip. But, currently, the new chip is not available, just have a simulation for the chip on the PC, so I need to bring the source code to PC, build it into DLL file, and communicate with the Chip simulation on the another PC.&lt;/P&gt;</description>
      <pubDate>Wed, 30 Aug 2023 07:06:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Generate-a-project-into-DLL-file-on-S32DS/m-p/1713790#M10893</guid>
      <dc:creator>AnhNguyenDuc</dc:creator>
      <dc:date>2023-08-30T07:06:51Z</dc:date>
    </item>
    <item>
      <title>Re: Generate a project into DLL file on S32DS</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Generate-a-project-into-DLL-file-on-S32DS/m-p/1715098#M10906</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I wrote you email. So, such approach is not possible.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 31 Aug 2023 13:16:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Generate-a-project-into-DLL-file-on-S32DS/m-p/1715098#M10906</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2023-08-31T13:16:49Z</dc:date>
    </item>
  </channel>
</rss>