<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Build the example on S32DS with S32K144EVB in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Build-the-example-on-S32DS-with-S32K144EVB/m-p/1689061#M10592</link>
    <description>&lt;P&gt;HI friends, I am new to S32DS ide set up and use. I am trying to use S32K144EVB-Q100 to have hands on experiencing by retyping the C code in example Project HelloClocks. I have exactly copied but there is error in build as Undefined reference to SOSC_init_80MHZ. Request to solve the issue.&lt;/P&gt;&lt;P&gt;arm-none-eabi-gcc -o "S32K144_Project_HelloClocks1.elf" "@S32K144_Project_HelloClocks1.args"&lt;BR /&gt;./src/main.o: In function `main':&lt;BR /&gt;C:\Users\kapilap6\workspaceS32DS.ARM.2.2\S32K144_Project_HelloClocks1\Debug/../src/main.c:72: undefined reference to `SOSC_init_8MHZ'&lt;BR /&gt;collect2.exe: error: ld returned 1 exit status&lt;BR /&gt;make: *** [makefile:42: S32K144_Project_HelloClocks1.elf] Error 1&lt;/P&gt;</description>
    <pubDate>Thu, 20 Jul 2023 07:02:43 GMT</pubDate>
    <dc:creator>Kapila</dc:creator>
    <dc:date>2023-07-20T07:02:43Z</dc:date>
    <item>
      <title>Build the example on S32DS with S32K144EVB</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Build-the-example-on-S32DS-with-S32K144EVB/m-p/1689061#M10592</link>
      <description>&lt;P&gt;HI friends, I am new to S32DS ide set up and use. I am trying to use S32K144EVB-Q100 to have hands on experiencing by retyping the C code in example Project HelloClocks. I have exactly copied but there is error in build as Undefined reference to SOSC_init_80MHZ. Request to solve the issue.&lt;/P&gt;&lt;P&gt;arm-none-eabi-gcc -o "S32K144_Project_HelloClocks1.elf" "@S32K144_Project_HelloClocks1.args"&lt;BR /&gt;./src/main.o: In function `main':&lt;BR /&gt;C:\Users\kapilap6\workspaceS32DS.ARM.2.2\S32K144_Project_HelloClocks1\Debug/../src/main.c:72: undefined reference to `SOSC_init_8MHZ'&lt;BR /&gt;collect2.exe: error: ld returned 1 exit status&lt;BR /&gt;make: *** [makefile:42: S32K144_Project_HelloClocks1.elf] Error 1&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jul 2023 07:02:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Build-the-example-on-S32DS-with-S32K144EVB/m-p/1689061#M10592</guid>
      <dc:creator>Kapila</dc:creator>
      <dc:date>2023-07-20T07:02:43Z</dc:date>
    </item>
    <item>
      <title>Re: Build the example on S32DS with S32K144EVB</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Build-the-example-on-S32DS-with-S32K144EVB/m-p/1689661#M10597</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/220453"&gt;@Kapila&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you share your project so I can try to replicate your issue?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R.&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jul 2023 18:20:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Build-the-example-on-S32DS-with-S32K144EVB/m-p/1689661#M10597</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-07-20T18:20:18Z</dc:date>
    </item>
  </channel>
</rss>