<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design Studio中的主题 Re: Error : Failed to execute MI command:</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Error-Failed-to-execute-MI-command/m-p/1687786#M10568</link>
    <description>I have updated to ARM 2.2 and all is well</description>
    <pubDate>Thu, 13 Jul 2023 17:56:53 GMT</pubDate>
    <dc:creator>PaulSMagna</dc:creator>
    <dc:date>2023-07-13T17:56:53Z</dc:date>
    <item>
      <title>Error : Failed to execute MI command:</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Error-Failed-to-execute-MI-command/m-p/1498839#M8869</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;This is Kihoon Kim from Seoul National University of Science and Technology.&lt;/P&gt;&lt;P&gt;I have a question about S32 error.&lt;/P&gt;&lt;P&gt;How to solve this error??&lt;/P&gt;&lt;P&gt;Now I'm using S32 for Power Architecture, and MPC 5777 Development Board.&lt;/P&gt;&lt;P&gt;Error message is mentioned below.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Error in final launch sequence&lt;BR /&gt;Failed to execute MI command:&lt;BR /&gt;-exec-run&lt;BR /&gt;Error message from debugger back end:&lt;BR /&gt;Error creating process C:/Users/kihoon/Dropbox/[3]°úÁ¦/[0]Çö´ëÀÚµ¿Â÷ Single stage 11kW OBC/[3]MPC5777C/Workspace/Hyundai_NXP_220713/SNU_CMU_mpc5777c/Debug_FLASH/SNU_CMU_mpc5777c.elf, (error 193).&lt;BR /&gt;Error creating process C:/Users/kihoon/Dropbox/[3]°úÁ¦/[0]Çö´ëÀÚµ¿Â÷ Single stage 11kW OBC/[3]MPC5777C/Workspace/Hyundai_NXP_220713/SNU_CMU_mpc5777c/Debug_FLASH/SNU_CMU_mpc5777c.elf, (error 193).&lt;/P&gt;</description>
      <pubDate>Mon, 01 Aug 2022 13:11:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Error-Failed-to-execute-MI-command/m-p/1498839#M8869</guid>
      <dc:creator>kihoon</dc:creator>
      <dc:date>2022-08-01T13:11:25Z</dc:date>
    </item>
    <item>
      <title>Re: Error : Failed to execute MI command:</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Error-Failed-to-execute-MI-command/m-p/1551181#M9387</link>
      <description>&lt;P&gt;Hi kihoon,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you please visit the following link and try the suggestion? Please removing spaces in your path.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://stackoverflow.com/questions/1106930/cygwin-gdb-gives-error-193-when-trying-to-start-program" target="_blank"&gt;https://stackoverflow.com/questions/1106930/cygwin-gdb-gives-error-193-when-trying-to-start-program&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Nov 2022 15:43:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Error-Failed-to-execute-MI-command/m-p/1551181#M9387</guid>
      <dc:creator>juan_see</dc:creator>
      <dc:date>2022-11-09T15:43:06Z</dc:date>
    </item>
    <item>
      <title>Re: Error : Failed to execute MI command:</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Error-Failed-to-execute-MI-command/m-p/1583399#M9653</link>
      <description>&lt;P&gt;I am getting this same error . no space in the path&amp;nbsp;&lt;/P&gt;&lt;P&gt;Error in final launch sequence:&lt;/P&gt;&lt;P&gt;Failed to execute MI command:&lt;BR /&gt;-exec-run&lt;BR /&gt;Error message from debugger back end:&lt;BR /&gt;Error creating process C:\Work\NXP\flexcan_encrypted_s32k148\Debug_FLASH\flexcan_encrypted_s32k148.elf, (error 193).&lt;BR /&gt;Failed to execute MI command:&lt;BR /&gt;-exec-run&lt;BR /&gt;Error message from debugger back end:&lt;BR /&gt;Error creating process C:\Work\NXP\flexcan_encrypted_s32k148\Debug_FLASH\flexcan_encrypted_s32k148.elf, (error 193).&lt;BR /&gt;Error creating process C:\Work\NXP\flexcan_encrypted_s32k148\Debug_FLASH\flexcan_encrypted_s32k148.elf, (error 193).&lt;/P&gt;&lt;P&gt;I have checked the permissions on the folder and I have full&amp;nbsp;access/write access for the folder system ..&amp;nbsp;&lt;/P&gt;&lt;P&gt;any thoughts. is there another folder it must write as well somewhere. that perhaps or which I do not have permissions.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 16 Jan 2023 18:16:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Error-Failed-to-execute-MI-command/m-p/1583399#M9653</guid>
      <dc:creator>PaulSMagna</dc:creator>
      <dc:date>2023-01-16T18:16:53Z</dc:date>
    </item>
    <item>
      <title>Re: Error : Failed to execute MI command:</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Error-Failed-to-execute-MI-command/m-p/1583410#M9654</link>
      <description>&lt;P&gt;Hi Paul,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Where did you install your S32 Design Studio IDE? Could you please provide the full path?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 16 Jan 2023 18:39:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Error-Failed-to-execute-MI-command/m-p/1583410#M9654</guid>
      <dc:creator>juan_see</dc:creator>
      <dc:date>2023-01-16T18:39:39Z</dc:date>
    </item>
    <item>
      <title>Re: Error : Failed to execute MI command:</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Error-Failed-to-execute-MI-command/m-p/1583430#M9655</link>
      <description>&lt;P&gt;Hi Juan&lt;/P&gt;&lt;P&gt;it is at&amp;nbsp;&lt;/P&gt;&lt;P&gt;C:\NXP\S32DS.3.4\eclipse&lt;/P&gt;&lt;P&gt;thanks for the assistance.&lt;/P&gt;&lt;P&gt;paul&lt;/P&gt;</description>
      <pubDate>Mon, 16 Jan 2023 19:57:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Error-Failed-to-execute-MI-command/m-p/1583430#M9655</guid>
      <dc:creator>PaulSMagna</dc:creator>
      <dc:date>2023-01-16T19:57:34Z</dc:date>
    </item>
    <item>
      <title>Re: Error : Failed to execute MI command:</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Error-Failed-to-execute-MI-command/m-p/1583444#M9656</link>
      <description>&lt;P&gt;Hi Paul,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you please try creating a blank application project for the S32K148? Does the issue also occurs there?&lt;/P&gt;</description>
      <pubDate>Mon, 16 Jan 2023 21:10:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Error-Failed-to-execute-MI-command/m-p/1583444#M9656</guid>
      <dc:creator>juan_see</dc:creator>
      <dc:date>2023-01-16T21:10:41Z</dc:date>
    </item>
    <item>
      <title>Re: Error : Failed to execute MI command:</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Error-Failed-to-execute-MI-command/m-p/1687786#M10568</link>
      <description>I have updated to ARM 2.2 and all is well</description>
      <pubDate>Thu, 13 Jul 2023 17:56:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Error-Failed-to-execute-MI-command/m-p/1687786#M10568</guid>
      <dc:creator>PaulSMagna</dc:creator>
      <dc:date>2023-07-13T17:56:53Z</dc:date>
    </item>
  </channel>
</rss>