<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックS32G274A - HUGE blob file</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32G274A-HUGE-blob-file/m-p/1682006#M10488</link>
    <description>&lt;P&gt;working on S32DS 3.5 , RTD 4.0.1 on the GOLDBOX (RDB2)&lt;/P&gt;&lt;P&gt;Starting from NXP example project Dio_ToggleLed_S32G274A_M7, the project runs perfect&lt;/P&gt;&lt;P&gt;followed the steps in :&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Use-IVT-Tool-To-Create-A-Blob-Image-S32G274A/ta-p/1125675" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Use-IVT-Tool-To-Create-A-Blob-Image-S32G274A/ta-p/1125675&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Built and created the bin file,&amp;nbsp;also created the DCD file&lt;/P&gt;&lt;P&gt;when exporting blob file, its 875MB !!!&lt;/P&gt;&lt;P&gt;Of coarse can't be written to flashed and the flash tool says its too large&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="oferbaharguardknox_0-1688557833434.png" style="width: 708px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/230903iA575ED577CC16872/image-dimensions/708x363?v=v2" width="708" height="363" role="button" title="oferbaharguardknox_0-1688557833434.png" alt="oferbaharguardknox_0-1688557833434.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;oferbaharguardknox_0-1688557833434.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;in the IVT tool everything looks perfect&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="oferbaharguardknox_1-1688557909832.png" style="width: 731px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/230904iE24A44D3FAC26EAD/image-dimensions/731x413?v=v2" width="731" height="413" role="button" title="oferbaharguardknox_1-1688557909832.png" alt="oferbaharguardknox_1-1688557909832.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;oferbaharguardknox_1-1688557909832.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;the size of the image looks OK, all else as well&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is wrong here?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Why is the blob file so large?&lt;/P&gt;</description>
    <pubDate>Wed, 05 Jul 2023 11:53:59 GMT</pubDate>
    <dc:creator>ofer-bahar-guardknox</dc:creator>
    <dc:date>2023-07-05T11:53:59Z</dc:date>
    <item>
      <title>S32G274A - HUGE blob file</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32G274A-HUGE-blob-file/m-p/1682006#M10488</link>
      <description>&lt;P&gt;working on S32DS 3.5 , RTD 4.0.1 on the GOLDBOX (RDB2)&lt;/P&gt;&lt;P&gt;Starting from NXP example project Dio_ToggleLed_S32G274A_M7, the project runs perfect&lt;/P&gt;&lt;P&gt;followed the steps in :&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Use-IVT-Tool-To-Create-A-Blob-Image-S32G274A/ta-p/1125675" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Use-IVT-Tool-To-Create-A-Blob-Image-S32G274A/ta-p/1125675&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Built and created the bin file,&amp;nbsp;also created the DCD file&lt;/P&gt;&lt;P&gt;when exporting blob file, its 875MB !!!&lt;/P&gt;&lt;P&gt;Of coarse can't be written to flashed and the flash tool says its too large&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="oferbaharguardknox_0-1688557833434.png" style="width: 708px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/230903iA575ED577CC16872/image-dimensions/708x363?v=v2" width="708" height="363" role="button" title="oferbaharguardknox_0-1688557833434.png" alt="oferbaharguardknox_0-1688557833434.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;oferbaharguardknox_0-1688557833434.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;in the IVT tool everything looks perfect&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="oferbaharguardknox_1-1688557909832.png" style="width: 731px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/230904iE24A44D3FAC26EAD/image-dimensions/731x413?v=v2" width="731" height="413" role="button" title="oferbaharguardknox_1-1688557909832.png" alt="oferbaharguardknox_1-1688557909832.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;oferbaharguardknox_1-1688557909832.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;the size of the image looks OK, all else as well&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is wrong here?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Why is the blob file so large?&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jul 2023 11:53:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32G274A-HUGE-blob-file/m-p/1682006#M10488</guid>
      <dc:creator>ofer-bahar-guardknox</dc:creator>
      <dc:date>2023-07-05T11:53:59Z</dc:date>
    </item>
    <item>
      <title>Re: S32G274A - HUGE blob file</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32G274A-HUGE-blob-file/m-p/1682021#M10489</link>
      <description>&lt;P&gt;The problem is that in the Application bootloader section, &lt;STRONG&gt;before&lt;/STRONG&gt; exporting blob file, the image file should be selected as the one from the Generated image file (aka the full application image file) =&amp;gt; &lt;STRONG&gt;VERY CONFUSING&lt;/STRONG&gt;&amp;nbsp;, and un associative&lt;/P&gt;&lt;P&gt;(instead of put it in the UI in a place that the user can understand that it should be selected)&lt;/P&gt;&lt;P&gt;&amp;nbsp;Anyway when selecting the 'generated image file' - everything is OK and the FLASH is written OK&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jul 2023 12:19:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32G274A-HUGE-blob-file/m-p/1682021#M10489</guid>
      <dc:creator>ofer-bahar-guardknox</dc:creator>
      <dc:date>2023-07-05T12:19:08Z</dc:date>
    </item>
  </channel>
</rss>