<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32DS S32G VS_HEADLESS in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-S32G-VS-HEADLESS/m-p/1679831#M10455</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;As for the general idea of the Functional Groups, the following information is provided inside the Help Contents of S32DS:&lt;/P&gt;
&lt;P&gt;"&lt;SPAN&gt;These &lt;/SPAN&gt;&lt;SPAN class="resultofText"&gt;groups&lt;/SPAN&gt;&lt;SPAN&gt; represent &lt;/SPAN&gt;&lt;SPAN class="resultofText"&gt;function&lt;/SPAN&gt;&lt;SPAN&gt;s which will be generated into source code. Use the dropdown menu to switch between &lt;/SPAN&gt;&lt;SPAN class="resultofText"&gt;functional&lt;/SPAN&gt; &lt;SPAN class="resultofText"&gt;groups&lt;/SPAN&gt;&lt;SPAN&gt; and configure them.&lt;/SPAN&gt;"&lt;/P&gt;
&lt;P&gt;As for the specific of the headless functional groups, the following is told from the internal team:&lt;/P&gt;
&lt;P&gt;"&lt;SPAN&gt;LLCE headless mode also provides a method to load a configuration set on LLCE boot, without host intervention. This removes the dependency on having the host ready and sending the configuration data via the driver. In turn, this reduces LLCE startup time when the host application is slow to start, allowing LLCE to buffer incoming messages which can later be received by the host, or start routing.&lt;/SPAN&gt;"&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
    <pubDate>Fri, 30 Jun 2023 20:55:35 GMT</pubDate>
    <dc:creator>Daniel-Aguirre</dc:creator>
    <dc:date>2023-06-30T20:55:35Z</dc:date>
    <item>
      <title>S32DS S32G VS_HEADLESS</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-S32G-VS-HEADLESS/m-p/1679485#M10448</link>
      <description>&lt;P&gt;Working with the S32DS for SS32G2,&lt;/P&gt;&lt;P&gt;In the configuration tool on the top there is variable with drop down selection between&amp;nbsp;VS_0 and VS_Headless&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anyone explain these meaning of this variable and values please?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Fri, 30 Jun 2023 09:18:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-S32G-VS-HEADLESS/m-p/1679485#M10448</guid>
      <dc:creator>ofer-bahar-guardknox</dc:creator>
      <dc:date>2023-06-30T09:18:54Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS S32G VS_HEADLESS</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-S32G-VS-HEADLESS/m-p/1679831#M10455</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;As for the general idea of the Functional Groups, the following information is provided inside the Help Contents of S32DS:&lt;/P&gt;
&lt;P&gt;"&lt;SPAN&gt;These &lt;/SPAN&gt;&lt;SPAN class="resultofText"&gt;groups&lt;/SPAN&gt;&lt;SPAN&gt; represent &lt;/SPAN&gt;&lt;SPAN class="resultofText"&gt;function&lt;/SPAN&gt;&lt;SPAN&gt;s which will be generated into source code. Use the dropdown menu to switch between &lt;/SPAN&gt;&lt;SPAN class="resultofText"&gt;functional&lt;/SPAN&gt; &lt;SPAN class="resultofText"&gt;groups&lt;/SPAN&gt;&lt;SPAN&gt; and configure them.&lt;/SPAN&gt;"&lt;/P&gt;
&lt;P&gt;As for the specific of the headless functional groups, the following is told from the internal team:&lt;/P&gt;
&lt;P&gt;"&lt;SPAN&gt;LLCE headless mode also provides a method to load a configuration set on LLCE boot, without host intervention. This removes the dependency on having the host ready and sending the configuration data via the driver. In turn, this reduces LLCE startup time when the host application is slow to start, allowing LLCE to buffer incoming messages which can later be received by the host, or start routing.&lt;/SPAN&gt;"&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Fri, 30 Jun 2023 20:55:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-S32G-VS-HEADLESS/m-p/1679831#M10455</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-06-30T20:55:35Z</dc:date>
    </item>
  </channel>
</rss>