<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design Studio中的主题 external debugger</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/external-debugger/m-p/1679639#M10452</link>
    <description>&lt;P&gt;As the document says need an external probe to coonect MCU with the computer,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Would like to know the importance of open sda in the Evaluation board of (s32k3x8evb-q289)&lt;/P&gt;&lt;P&gt;Do I need an external debugger inorder to flash the code into the target processor.&lt;/P&gt;&lt;P&gt;Currently Iam connecting the received USB CABLE inorder to connect .(one end into the open sda and other into my pc).&lt;/P&gt;</description>
    <pubDate>Fri, 30 Jun 2023 12:41:59 GMT</pubDate>
    <dc:creator>Anjalipurushothaman</dc:creator>
    <dc:date>2023-06-30T12:41:59Z</dc:date>
    <item>
      <title>external debugger</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/external-debugger/m-p/1679639#M10452</link>
      <description>&lt;P&gt;As the document says need an external probe to coonect MCU with the computer,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Would like to know the importance of open sda in the Evaluation board of (s32k3x8evb-q289)&lt;/P&gt;&lt;P&gt;Do I need an external debugger inorder to flash the code into the target processor.&lt;/P&gt;&lt;P&gt;Currently Iam connecting the received USB CABLE inorder to connect .(one end into the open sda and other into my pc).&lt;/P&gt;</description>
      <pubDate>Fri, 30 Jun 2023 12:41:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/external-debugger/m-p/1679639#M10452</guid>
      <dc:creator>Anjalipurushothaman</dc:creator>
      <dc:date>2023-06-30T12:41:59Z</dc:date>
    </item>
    <item>
      <title>Re: external debugger</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/external-debugger/m-p/1680709#M10471</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/214201"&gt;@Anjalipurushothaman&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;OpenSDA provides a bridge between your computer (or other USB hosts) and the embedded target processor, which can be used for debugging, flash programming, and serial communication, all over a simple USB cable.&lt;/P&gt;
&lt;P&gt;If you are using an EVB it is not necessary to use an external debugger to&amp;nbsp;&lt;SPAN&gt;flash programming, unless you want it or required it.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;B.R.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;VaneB&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 03 Jul 2023 20:57:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/external-debugger/m-p/1680709#M10471</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-07-03T20:57:31Z</dc:date>
    </item>
  </channel>
</rss>