<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックBuild a project</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Build-a-project/m-p/1676141#M10399</link>
    <description>&lt;P&gt;While building a project , only one target option is enabled, which make to only debug the configration.&lt;/P&gt;&lt;P&gt;If I need to flash the program into target processor , which has to be selected . (PE Micro is not poping up in the Run configration window)&lt;/P&gt;&lt;P&gt;wheras while debigging , i can selecte PE Micro.&lt;/P&gt;&lt;P&gt;Since toolchain will be same for any target proessor, Hope anyone can provide solution to this.&lt;/P&gt;</description>
    <pubDate>Mon, 26 Jun 2023 15:53:08 GMT</pubDate>
    <dc:creator>Anjalipurushothaman</dc:creator>
    <dc:date>2023-06-26T15:53:08Z</dc:date>
    <item>
      <title>Build a project</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Build-a-project/m-p/1676141#M10399</link>
      <description>&lt;P&gt;While building a project , only one target option is enabled, which make to only debug the configration.&lt;/P&gt;&lt;P&gt;If I need to flash the program into target processor , which has to be selected . (PE Micro is not poping up in the Run configration window)&lt;/P&gt;&lt;P&gt;wheras while debigging , i can selecte PE Micro.&lt;/P&gt;&lt;P&gt;Since toolchain will be same for any target proessor, Hope anyone can provide solution to this.&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jun 2023 15:53:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Build-a-project/m-p/1676141#M10399</guid>
      <dc:creator>Anjalipurushothaman</dc:creator>
      <dc:date>2023-06-26T15:53:08Z</dc:date>
    </item>
    <item>
      <title>Re: Build a project</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Build-a-project/m-p/1678032#M10423</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/214201"&gt;@Anjalipurushothaman&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please correct me if I am wrong.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;What you are trying to do is flash your micro with your debugger, but you do not see the "release" option, you only see "debug"? Am I correct?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R.&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jun 2023 18:22:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Build-a-project/m-p/1678032#M10423</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-06-28T18:22:45Z</dc:date>
    </item>
    <item>
      <title>Re: Build a project</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Build-a-project/m-p/1678588#M10432</link>
      <description>&lt;P&gt;Yes, That is correct&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jun 2023 09:15:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Build-a-project/m-p/1678588#M10432</guid>
      <dc:creator>Anjalipurushothaman</dc:creator>
      <dc:date>2023-06-29T09:15:36Z</dc:date>
    </item>
  </channel>
</rss>