<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design Studio中的主题 Re: Changing LIN Frame ID</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Changing-LIN-Frame-ID/m-p/1672150#M10349</link>
    <description>&lt;P&gt;Also in 'Variables', if the frame ID is 0x1A, LIN status is LIN_TX_OK. Whereas, if the frame ID is anything other than 0x1A, LIN status is LIN_OPERATIONAL, which does not transmit the header frame at all. How do I change LIN status from LIN_OPERATIONAL to LIN_TX_OK?&lt;/P&gt;</description>
    <pubDate>Mon, 19 Jun 2023 18:53:46 GMT</pubDate>
    <dc:creator>cw20</dc:creator>
    <dc:date>2023-06-19T18:53:46Z</dc:date>
    <item>
      <title>Changing LIN Frame ID</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Changing-LIN-Frame-ID/m-p/1672069#M10348</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="cw20_0-1687186761670.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/228361i0FBFD1C8EF2675AB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="cw20_0-1687186761670.png" alt="cw20_0-1687186761670.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I have a S32K344 board and I am using the LIN Master Frame example. I want to be able to change the frame ID (0x1A) and have it run properly. When I try measuring in CANoe, only signals with the frame ID 0x1A are shown but I want to have signals with other IDs shown and constantly updating. How do I change it so that the frame ID can continually update?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="cw20_1-1687187017521.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/228364i5F6E89A443DC3008/image-size/medium?v=v2&amp;amp;px=400" role="button" title="cw20_1-1687187017521.png" alt="cw20_1-1687187017521.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 19 Jun 2023 15:03:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Changing-LIN-Frame-ID/m-p/1672069#M10348</guid>
      <dc:creator>cw20</dc:creator>
      <dc:date>2023-06-19T15:03:50Z</dc:date>
    </item>
    <item>
      <title>Re: Changing LIN Frame ID</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Changing-LIN-Frame-ID/m-p/1672150#M10349</link>
      <description>&lt;P&gt;Also in 'Variables', if the frame ID is 0x1A, LIN status is LIN_TX_OK. Whereas, if the frame ID is anything other than 0x1A, LIN status is LIN_OPERATIONAL, which does not transmit the header frame at all. How do I change LIN status from LIN_OPERATIONAL to LIN_TX_OK?&lt;/P&gt;</description>
      <pubDate>Mon, 19 Jun 2023 18:53:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Changing-LIN-Frame-ID/m-p/1672150#M10349</guid>
      <dc:creator>cw20</dc:creator>
      <dc:date>2023-06-19T18:53:46Z</dc:date>
    </item>
    <item>
      <title>Re: Changing LIN Frame ID</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Changing-LIN-Frame-ID/m-p/1672673#M10353</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;PID is used in LIn_PduType variable, so use valid PID value. Driver is checking whether PID is valid with correct parity bits..&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Tue, 20 Jun 2023 10:50:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Changing-LIN-Frame-ID/m-p/1672673#M10353</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-06-20T10:50:13Z</dc:date>
    </item>
  </channel>
</rss>