<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design Studio中的主题 How to set pin function</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-set-pin-function/m-p/1666075#M10296</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Here's the thing, I need to use FlexioI2C.&lt;/P&gt;&lt;P&gt;And before my pow-on sequence is finished, I want the two Flexio pins to keep Hi-Z.&lt;/P&gt;&lt;P&gt;After the pow-on sequence is done, set the two pins as FlexioI2C.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do I configure it?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've only found this API&amp;nbsp;&lt;EM&gt;Siul2_Port_Ip_SetPinDirection&lt;/EM&gt;, but it's just used to set pin direction, how do I set pin function in this case?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jetty&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 08 Jun 2023 09:40:07 GMT</pubDate>
    <dc:creator>jetty1012</dc:creator>
    <dc:date>2023-06-08T09:40:07Z</dc:date>
    <item>
      <title>How to set pin function</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-set-pin-function/m-p/1666075#M10296</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Here's the thing, I need to use FlexioI2C.&lt;/P&gt;&lt;P&gt;And before my pow-on sequence is finished, I want the two Flexio pins to keep Hi-Z.&lt;/P&gt;&lt;P&gt;After the pow-on sequence is done, set the two pins as FlexioI2C.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do I configure it?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've only found this API&amp;nbsp;&lt;EM&gt;Siul2_Port_Ip_SetPinDirection&lt;/EM&gt;, but it's just used to set pin direction, how do I set pin function in this case?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jetty&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jun 2023 09:40:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/How-to-set-pin-function/m-p/1666075#M10296</guid>
      <dc:creator>jetty1012</dc:creator>
      <dc:date>2023-06-08T09:40:07Z</dc:date>
    </item>
    <item>
      <title>Re: How to set pin function</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-set-pin-function/m-p/1666781#M10305</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Jetty,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;It is recommended to refer to the initialization of I2c_IP_FLEXIO_Transfer_S32K312 example in S32K3 RTD.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;/P&gt;</description>
      <pubDate>Fri, 09 Jun 2023 08:27:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/How-to-set-pin-function/m-p/1666781#M10305</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-06-09T08:27:12Z</dc:date>
    </item>
  </channel>
</rss>