<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: enabling S32K146 floating point instructions in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/enabling-S32K146-floating-point-instructions/m-p/1662863#M10264</link>
    <description>&lt;P&gt;The only option is fpv4-sp-d16, forcibly selected. Presumably this is the same as fpv4-sp&lt;/P&gt;</description>
    <pubDate>Fri, 02 Jun 2023 20:16:27 GMT</pubDate>
    <dc:creator>KelvinSmith</dc:creator>
    <dc:date>2023-06-02T20:16:27Z</dc:date>
    <item>
      <title>enabling S32K146 floating point instructions</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/enabling-S32K146-floating-point-instructions/m-p/1662208#M10254</link>
      <description>&lt;P&gt;The S32K146 processor includes a floating point unit, but if I go into the project properties and under 'target processor', I set 'Float ABI' to 'FP instructions (hard)', I get errors during the link stage like these:&lt;/P&gt;&lt;P&gt;c:/nxp/s32ds.3.4/s32ds/build_tools/gcc_b1620/gcc-6.3-arm32-eabi/bin/../lib/gcc/arm-none-eabi/6.3.1/../../../../arm-none-eabi/bin/real-ld.exe: error: libuavcanV1_demo.elf uses VFP register arguments, ./Project_Settings/Startup_Code/system_S32K146.o does not&lt;BR /&gt;c:/nxp/s32ds.3.4/s32ds/build_tools/gcc_b1620/gcc-6.3-arm32-eabi/bin/../lib/gcc/arm-none-eabi/6.3.1/../../../../arm-none-eabi/bin/real-ld.exe: failed to merge target specific data of file ./Project_Settings/Startup_Code/system_S32K146.o&lt;/P&gt;&lt;P&gt;These errors repeat for every source file, even if they do not use floating point instructions.&lt;/P&gt;</description>
      <pubDate>Thu, 01 Jun 2023 22:20:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/enabling-S32K146-floating-point-instructions/m-p/1662208#M10254</guid>
      <dc:creator>KelvinSmith</dc:creator>
      <dc:date>2023-06-01T22:20:12Z</dc:date>
    </item>
    <item>
      <title>Re: enabling S32K146 floating point instructions</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/enabling-S32K146-floating-point-instructions/m-p/1662653#M10258</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;this typically happen if you are linking external library which is compiled with soft FP. It is possible share your project?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 02 Jun 2023 12:02:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/enabling-S32K146-floating-point-instructions/m-p/1662653#M10258</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2023-06-02T12:02:55Z</dc:date>
    </item>
    <item>
      <title>Re: enabling S32K146 floating point instructions</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/enabling-S32K146-floating-point-instructions/m-p/1662661#M10260</link>
      <description>&lt;P&gt;Do you have chosen right FPU type (FPv4-SP)?&lt;/P&gt;</description>
      <pubDate>Fri, 02 Jun 2023 12:11:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/enabling-S32K146-floating-point-instructions/m-p/1662661#M10260</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2023-06-02T12:11:30Z</dc:date>
    </item>
    <item>
      <title>Re: enabling S32K146 floating point instructions</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/enabling-S32K146-floating-point-instructions/m-p/1662863#M10264</link>
      <description>&lt;P&gt;The only option is fpv4-sp-d16, forcibly selected. Presumably this is the same as fpv4-sp&lt;/P&gt;</description>
      <pubDate>Fri, 02 Jun 2023 20:16:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/enabling-S32K146-floating-point-instructions/m-p/1662863#M10264</guid>
      <dc:creator>KelvinSmith</dc:creator>
      <dc:date>2023-06-02T20:16:27Z</dc:date>
    </item>
    <item>
      <title>Re: enabling S32K146 floating point instructions</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/enabling-S32K146-floating-point-instructions/m-p/1662866#M10265</link>
      <description>&lt;P&gt;I solved this by doing a clean on the project. That caused a bunch of new errors. So I deleted the project from the workspace and readded it. Then I built it again and presto it worked! What a lot of nonesense. But at least it is possible.&lt;/P&gt;</description>
      <pubDate>Fri, 02 Jun 2023 20:24:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/enabling-S32K146-floating-point-instructions/m-p/1662866#M10265</guid>
      <dc:creator>KelvinSmith</dc:creator>
      <dc:date>2023-06-02T20:24:01Z</dc:date>
    </item>
  </channel>
</rss>