<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Failure in installing S32G support in S32DS 3.5.2 Linux version in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Failure-in-installing-S32G-support-in-S32DS-3-5-2-Linux-version/m-p/1661909#M10248</link>
    <description>&lt;P&gt;I found that using the offline package of the same version of the S32G update site solved the problem. So you can investigate why the online installation failed.&lt;/P&gt;</description>
    <pubDate>Thu, 01 Jun 2023 13:07:55 GMT</pubDate>
    <dc:creator>AdrianGancev</dc:creator>
    <dc:date>2023-06-01T13:07:55Z</dc:date>
    <item>
      <title>Failure in installing S32G support in S32DS 3.5.2 Linux version</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Failure-in-installing-S32G-support-in-S32DS-3-5-2-Linux-version/m-p/1661892#M10247</link>
      <description>&lt;P&gt;I need to install S32DS with S32G support.&lt;/P&gt;
&lt;P&gt;So I installed the S32DS.3.5_b220726_linux.x86_64.bin&lt;/P&gt;
&lt;P&gt;Here the contents of the installation so far:&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;Package: GDB Client for ARM Embedded Processors 9.2 Build 1701; Version: 1701; Build id: 202012011653
Package: S32 Design Studio Platform package; Version: 3.5.2; Build id: 202302262111
Package: NXP GCC for Arm Embedded Processors v9.2 build 1649; Version: 1649; Build id: 202005201157
Package: GNU ARM PEMicro Interface Debugging Support; Version: 5.1.7; Build id: 202112141853
Package: S32 Design Studio Platform Tools package; Version: 3.5.2; Build id: 202302262111
Package: NXP GCC for Arm Embedded Processors Build 1620; Version: 1620; Build id: 202005201521
&lt;/LI-CODE&gt;
&lt;P&gt;When installing the S32G development package version 3.5.2, there is a failure as depicted below. How to solve this?&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="AdrianGancev_2-1685623021109.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/225872i3EC94D7551B71D3B/image-size/large?v=v2&amp;amp;px=999" role="button" title="AdrianGancev_2-1685623021109.png" alt="AdrianGancev_2-1685623021109.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Cheers.&lt;/P&gt;</description>
      <pubDate>Thu, 01 Jun 2023 12:37:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Failure-in-installing-S32G-support-in-S32DS-3-5-2-Linux-version/m-p/1661892#M10247</guid>
      <dc:creator>AdrianGancev</dc:creator>
      <dc:date>2023-06-01T12:37:33Z</dc:date>
    </item>
    <item>
      <title>Re: Failure in installing S32G support in S32DS 3.5.2 Linux version</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Failure-in-installing-S32G-support-in-S32DS-3-5-2-Linux-version/m-p/1661909#M10248</link>
      <description>&lt;P&gt;I found that using the offline package of the same version of the S32G update site solved the problem. So you can investigate why the online installation failed.&lt;/P&gt;</description>
      <pubDate>Thu, 01 Jun 2023 13:07:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Failure-in-installing-S32G-support-in-S32DS-3-5-2-Linux-version/m-p/1661909#M10248</guid>
      <dc:creator>AdrianGancev</dc:creator>
      <dc:date>2023-06-01T13:07:55Z</dc:date>
    </item>
  </channel>
</rss>