<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: S32ds studio version 3.4</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32ds-studio-version-3-4/m-p/1657967#M10209</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;From the Release Notes of the RTD of S32K358 and S32K388, it can be seen that it is developed based on S32 Design Studio 3.5. So if you need to develop S32K358\S32K388 , please use S32DS v3.5 instead of v3.4.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Fri, 26 May 2023 00:40:45 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2023-05-26T00:40:45Z</dc:date>
    <item>
      <title>S32ds studio version 3.4</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32ds-studio-version-3-4/m-p/1657841#M10208</link>
      <description>&lt;P&gt;&lt;SPAN&gt;will the S32ds studio version 3.4 support family S32K388 OR S32K358?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 25 May 2023 16:42:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32ds-studio-version-3-4/m-p/1657841#M10208</guid>
      <dc:creator>Anjalipurushothaman</dc:creator>
      <dc:date>2023-05-25T16:42:46Z</dc:date>
    </item>
    <item>
      <title>Re: S32ds studio version 3.4</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32ds-studio-version-3-4/m-p/1657967#M10209</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;From the Release Notes of the RTD of S32K358 and S32K388, it can be seen that it is developed based on S32 Design Studio 3.5. So if you need to develop S32K358\S32K388 , please use S32DS v3.5 instead of v3.4.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 26 May 2023 00:40:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32ds-studio-version-3-4/m-p/1657967#M10209</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-05-26T00:40:45Z</dc:date>
    </item>
  </channel>
</rss>